<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: Schematic for MHT1008N reference circuit?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Schematic-for-MHT1008N-reference-circuit/m-p/1049180#M9272</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DXF file for MHT1008N 2450 MHz design is provided on the device product page:&lt;BR /&gt;&lt;A href="https://www.nxp.com/products/rf/rf-power/rf-cooking/2450-mhz-rf-cooking/2450-mhz-12-5-w-cw-28-v-rf-ldmos-transistor-for-consumer-and-commercial-cooking:MHT1008N?tab=Design_Tools_Tab" target="test_blank"&gt;https://www.nxp.com/products/rf/rf-power/rf-cooking/2450-mhz-rf-cooking/2450-mhz-12-5-w-cw-28-v-rf-ldmos-transistor-for-consumer-and-commercial-cooking:MHT1008N?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Load pull contours are available in the datasheet pages 5 and 6. You can start designing matching and bias networks using these recommended impedance values. You can optimize your design for either maximum P1dB, P3dB power or maximum efficiency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have no any dedicated length of transmission lines since the actual layout would depend on substrate and your application requirements: frequency bandwidth, dimensional constrains...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP 2450 MHz design provides input matching consisting of two TL segments and a capacitor. Output matching consist of three TL segments and a capacitor. Primary purpose of this layout is to provide optimal performance in wider frequency range 2400..2500MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a narrowband design (single operating frequency), the matching circuit coud be simplier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel&lt;BR /&gt;TIC&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Apr 2020 09:24:21 GMT</pubDate>
    <dc:creator>LPP</dc:creator>
    <dc:date>2020-04-06T09:24:21Z</dc:date>
    <item>
      <title>Schematic for MHT1008N reference circuit?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Schematic-for-MHT1008N-reference-circuit/m-p/1049179#M9271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP Team!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to design an RF amplifier using your&amp;nbsp;MHT1008N.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, since I want to do the simulation on ADS,&amp;nbsp; is there any reference where I could see and analyze the schematic circuit of the&amp;nbsp;MHT1008, as in the attached, 2450MHz reference design? As I would also want to know if there is any dedicated length of transmission lines at RFin and RFout, or even at other pin terminal if any.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2020 14:18:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Schematic-for-MHT1008N-reference-circuit/m-p/1049179#M9271</guid>
      <dc:creator>mrazld_hamdan</dc:creator>
      <dc:date>2020-04-02T14:18:59Z</dc:date>
    </item>
    <item>
      <title>Re: Schematic for MHT1008N reference circuit?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Schematic-for-MHT1008N-reference-circuit/m-p/1049180#M9272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DXF file for MHT1008N 2450 MHz design is provided on the device product page:&lt;BR /&gt;&lt;A href="https://www.nxp.com/products/rf/rf-power/rf-cooking/2450-mhz-rf-cooking/2450-mhz-12-5-w-cw-28-v-rf-ldmos-transistor-for-consumer-and-commercial-cooking:MHT1008N?tab=Design_Tools_Tab" target="test_blank"&gt;https://www.nxp.com/products/rf/rf-power/rf-cooking/2450-mhz-rf-cooking/2450-mhz-12-5-w-cw-28-v-rf-ldmos-transistor-for-consumer-and-commercial-cooking:MHT1008N?tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Load pull contours are available in the datasheet pages 5 and 6. You can start designing matching and bias networks using these recommended impedance values. You can optimize your design for either maximum P1dB, P3dB power or maximum efficiency.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have no any dedicated length of transmission lines since the actual layout would depend on substrate and your application requirements: frequency bandwidth, dimensional constrains...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP 2450 MHz design provides input matching consisting of two TL segments and a capacitor. Output matching consist of three TL segments and a capacitor. Primary purpose of this layout is to provide optimal performance in wider frequency range 2400..2500MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For a narrowband design (single operating frequency), the matching circuit coud be simplier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel&lt;BR /&gt;TIC&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Apr 2020 09:24:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Schematic-for-MHT1008N-reference-circuit/m-p/1049180#M9272</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2020-04-06T09:24:21Z</dc:date>
    </item>
  </channel>
</rss>