<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: QN9021 failed to run BLE example  project</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/QN9021-failed-to-run-BLE-example-project/m-p/1008796#M8565</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;The example is&amp;nbsp; QN902x_SDK_1.4.0\Projects\BLE\prj_bass.&lt;/P&gt;&lt;P&gt;I use the jlink commad in PRJROOT\src\link\iar\qn9020_flash.mac to&amp;nbsp;get that the chip is “Device: QN9020 B3”.&lt;/P&gt;&lt;P&gt;After&amp;nbsp;using the macro CFG_QN9020_B2, it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;qn9020_flash.mac:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;execUserReset()&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;{&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __var chip_id;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;chip_id = __readMemory32(0x40000088, "Memory");&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;if(chip_id == 0x2801) // QN9020 B0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B0";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B0();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else if(chip_id == 0x2901) // QN9020 B1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B1";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B1();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else if(chip_id == 0x2A01) // QN9020 B2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B2";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B2();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else if(chip_id == 0x2B01) // QN9020 B3&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B3";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B2();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else if(chip_id == 0x2C01) // QN9020 B4&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B4";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B4();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Error: unknown device ID: ", chip_id;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;}&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Nov 2019 06:20:18 GMT</pubDate>
    <dc:creator>229856331</dc:creator>
    <dc:date>2019-11-20T06:20:18Z</dc:date>
    <item>
      <title>QN9021 failed to run BLE example  project</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9021-failed-to-run-BLE-example-project/m-p/1008794#M8563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I run the prj_bass project, but it can not work.&lt;/P&gt;&lt;P&gt;I debug it with jlink, found that BLE stack APIs locate at the address around 0x01000000~0x0102000 (defined in&amp;nbsp; fw_func_addr.h), but the content of the chip&amp;nbsp;in the&amp;nbsp;range is all 0xFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SDK version 1.4.0&lt;/P&gt;&lt;P&gt;The marking letter of chip is&amp;nbsp; "9021&amp;nbsp; &amp;nbsp; 355Y5&amp;nbsp; &amp;nbsp;00UMF"&lt;/P&gt;&lt;P&gt;I use the macro QN_9020_B4&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 11:36:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9021-failed-to-run-BLE-example-project/m-p/1008794#M8563</guid>
      <dc:creator>229856331</dc:creator>
      <dc:date>2019-11-19T11:36:49Z</dc:date>
    </item>
    <item>
      <title>Re: QN9021 failed to run BLE example  project</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9021-failed-to-run-BLE-example-project/m-p/1008795#M8564</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the example that you are trying to run?&lt;/P&gt;&lt;P&gt;What are the lib that you have included?&lt;/P&gt;&lt;P&gt;Please look at the next AN&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN12288.pdf" title="https://www.nxp.com/docs/en/application-note/AN12288.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN12288.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is it your custom board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 17:57:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9021-failed-to-run-BLE-example-project/m-p/1008795#M8564</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2019-11-19T17:57:34Z</dc:date>
    </item>
    <item>
      <title>Re: QN9021 failed to run BLE example  project</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9021-failed-to-run-BLE-example-project/m-p/1008796#M8565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;The example is&amp;nbsp; QN902x_SDK_1.4.0\Projects\BLE\prj_bass.&lt;/P&gt;&lt;P&gt;I use the jlink commad in PRJROOT\src\link\iar\qn9020_flash.mac to&amp;nbsp;get that the chip is “Device: QN9020 B3”.&lt;/P&gt;&lt;P&gt;After&amp;nbsp;using the macro CFG_QN9020_B2, it works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;qn9020_flash.mac:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;execUserReset()&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;{&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __var chip_id;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;chip_id = __readMemory32(0x40000088, "Memory");&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;if(chip_id == 0x2801) // QN9020 B0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B0";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B0();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else if(chip_id == 0x2901) // QN9020 B1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B1";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B1();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else if(chip_id == 0x2A01) // QN9020 B2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B2";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B2();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else if(chip_id == 0x2B01) // QN9020 B3&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B3";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B2();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else if(chip_id == 0x2C01) // QN9020 B4&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Device: QN9020 B4";&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; cfg_fw_9020_B4();&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; else&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; {&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; __message "Error: unknown device ID: ", chip_id;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt; }&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;}&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Nov 2019 06:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9021-failed-to-run-BLE-example-project/m-p/1008796#M8565</guid>
      <dc:creator>229856331</dc:creator>
      <dc:date>2019-11-20T06:20:18Z</dc:date>
    </item>
  </channel>
</rss>