<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: How do I read/write to an ISO15693 tag using NXP NFC Cockpit?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/How-do-I-read-write-to-an-ISO15693-tag-using-NXP-NFC-Cockpit/m-p/974652#M8130</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the image, I assume you are working with CLRC663 eval board.&amp;nbsp;Regarding the Tag, did you make sure that the Tag's block you are trying to read is not password protected or require authentication?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Jul 2019 20:18:19 GMT</pubDate>
    <dc:creator>IvanRuiz</dc:creator>
    <dc:date>2019-07-01T20:18:19Z</dc:date>
    <item>
      <title>How do I read/write to an ISO15693 tag using NXP NFC Cockpit?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/How-do-I-read-write-to-an-ISO15693-tag-using-NXP-NFC-Cockpit/m-p/974651#M8129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the NFC cockpit v4.8.0 to work with HF RFID tags using the ISO15693 protocol. I'm able to&amp;nbsp;send data to a ISO14443A tag I have and receive bytes back, but when I try to use my ISO 15693 tag, I'm not able to write data to this card (ERROR:RFProtocolType15693Service:Perform15693DataExchangeFailed) or read blocks (ERROR:RFProtocolType15693Service:PerformReadSingleBlockFailed). I'm able to get the tag's UID through the Inventory button but reading and writing always throws these errors. Any advice would be great!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/89841i51D768C5F01E973D/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_391.png" alt="pastedImage_391.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2019 23:27:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/How-do-I-read-write-to-an-ISO15693-tag-using-NXP-NFC-Cockpit/m-p/974651#M8129</guid>
      <dc:creator>alexpainter3</dc:creator>
      <dc:date>2019-06-26T23:27:31Z</dc:date>
    </item>
    <item>
      <title>Re: How do I read/write to an ISO15693 tag using NXP NFC Cockpit?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/How-do-I-read-write-to-an-ISO15693-tag-using-NXP-NFC-Cockpit/m-p/974652#M8130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the image, I assume you are working with CLRC663 eval board.&amp;nbsp;Regarding the Tag, did you make sure that the Tag's block you are trying to read is not password protected or require authentication?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Ivan.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jul 2019 20:18:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/How-do-I-read-write-to-an-ISO15693-tag-using-NXP-NFC-Cockpit/m-p/974652#M8130</guid>
      <dc:creator>IvanRuiz</dc:creator>
      <dc:date>2019-07-01T20:18:19Z</dc:date>
    </item>
  </channel>
</rss>