<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Qn908x HID Device Pairing in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960139#M7805</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Strange, I was trying with Bare Metal example code and its not working at all whatever I try to do.&lt;/P&gt;&lt;P&gt;So, I tried with FreeRTOS example code and made the same modifications i.e. only two Macros changed and it works flawlessly every time.&lt;BR /&gt;&lt;BR /&gt;Is there any different setup/steps wrt Bare Metal or any bug which is causing this?&lt;BR /&gt;&lt;BR /&gt;Can anyone provide any info on which is better to use BareMetal or FreeRTOS?&lt;BR /&gt;I don't have much knowledge on RTOS kind of stuff.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Aug 2019 05:08:29 GMT</pubDate>
    <dc:creator>ankur_rathi</dc:creator>
    <dc:date>2019-08-23T05:08:29Z</dc:date>
    <item>
      <title>Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960129#M7795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using QN908x dev board and SDK2.2.0_QN908XCDK and MCUExpresso IDE for development purpose.&lt;BR /&gt;&lt;BR /&gt;I loaded HID device (bare metal) example code and when I connect to my Android App (nRF Connect), its getting connected and when I try to connect it with System Bluetooth, it through an error "pairing Rejected", which is correct as Pairing and Bonding was disabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now, I have enabled Pairing and Bonding in "app_preinclude" header file:&lt;BR /&gt;/*! Enable/disable use of bonding capability */&lt;BR /&gt;#define gAppUseBonding_d&amp;nbsp;&amp;nbsp; 1&lt;/P&gt;&lt;P&gt;/*! Enable/disable use of pairing procedure */&lt;BR /&gt;#define gAppUsePairing_d&amp;nbsp;&amp;nbsp; 1&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;But, when I tried to connect it with system Bluetooth as well as Mobile Application, it through an error "Could not pair with NXP_HID because of incorrect pin or passkey.".&lt;BR /&gt;&lt;BR /&gt;It doesn't ask to Enter pairing pin.&lt;BR /&gt;I am using nRF Connect mobile application to check the BLE behavior.&lt;BR /&gt;&lt;BR /&gt;I want Pairing and Bonding to be enabled. So, do you have any example code for Pairing and Bonding and also do OOB pairing is supported in QN908x.&lt;BR /&gt;&lt;BR /&gt;While going through forum, I just saw that Enabling in "app_preinclude" header file has solved pairing problem but I was not able to pair. Is there any extra setting/modification need to be done to make pairing possible?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jun 2019 13:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960129#M7795</guid>
      <dc:creator>ankur_rathi</dc:creator>
      <dc:date>2019-06-07T13:27:57Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960130#M7796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you pressing the button 1 to start advertising and getting everything working ? I was able to make it work just changing those two defines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, which IDE are you using and SDK versions ? I would recommend you to use the latest version of both, also when importing the project please be sure to use the UART instead of the semi hosting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check as well the &lt;EM style="color: #0000ff; "&gt;Bluetooth® Low Energy Demo Applications User’s Guide&lt;/EM&gt;, I believe this might be useful for you if you are just getting started working with this device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jun 2019 16:47:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960130#M7796</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-06-07T16:47:38Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960131#M7797</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry Estephania for late response.&lt;BR /&gt;I have modified those two Macros before only but my Mobile device doesn't ask for Pairing pin. It directly through an error. I am using Redmi Note 7 Pro.&lt;BR /&gt;&lt;BR /&gt;But strange, it works on One Plus 6T consistently.&lt;BR /&gt;I tried Restarting my phone and Turning ON/OFF Bluetooth also, then also popup for pairing pin is not getting populated.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 10:07:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960131#M7797</guid>
      <dc:creator>ankur_rathi</dc:creator>
      <dc:date>2019-06-11T10:07:59Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960132#M7798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have the location enables as well in your device ?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 16:08:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960132#M7798</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-06-11T16:08:41Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960133#M7799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, location is enabled on the device.&lt;BR /&gt;Does OOB is also supported on QN908x?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 05:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960133#M7799</guid>
      <dc:creator>ankur_rathi</dc:creator>
      <dc:date>2019-06-13T05:55:19Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960134#M7800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an example for the KW41Z that you can use as a base and there is one example for the &lt;A href="https://www.nxp.com/docs/en/application-note/AN12319.pdf"&gt;QN9080-001-ML17&lt;/A&gt;, those uses an NTAG I2C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 14:05:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960134#M7800</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-06-13T14:05:14Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960135#M7801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I will go through those example code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Thu, 13 Jun, 2019, 7:35 PM estephania_martinez, &amp;lt;admin@community.nxp.com&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 14:33:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960135#M7801</guid>
      <dc:creator>ankur_rathi</dc:creator>
      <dc:date>2019-06-13T14:33:27Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960136#M7802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hope that helps&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Jun 2019 15:47:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960136#M7802</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-06-13T15:47:43Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960137#M7803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MCUXpresso v11.0.0 to build QN908x (HID device example code).&lt;BR /&gt;QN908x SDK v2.2.0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using HID device Bare Metal example code.&lt;BR /&gt;I want to enable "Pairing" in this example code, so in "app_preinclude" header file, I am modified following macro to:&lt;/P&gt;&lt;P&gt;#define gAppUseBonding_d&amp;nbsp;&amp;nbsp; 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*! Enable/disable use of bonding capability */&lt;BR /&gt;#define gAppUsePairing_d&amp;nbsp;&amp;nbsp; 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*! Enable/disable use of pairing procedure */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I build the project successfully without any error and then loaded onto QN9080DK-V1.3. &lt;BR /&gt;I am able to see the "NXP_HID" device onto mobile app but when I try to connect, it through an error "Could not pair with NXP_HID device because of incorrect Pin", but strange it has not asked for Pairing Pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;While debugging, I am able to see setting of Pairing Pin API gets called as well as Pairing Complete event get triggered but I am not able to successfully Pair the device with Mobile.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pairing setting (app_config.c):&lt;BR /&gt;/* SMP Data */&lt;BR /&gt;gapPairingParameters_t gPairingParameters = {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .withBonding = TRUE,&amp;nbsp;&amp;nbsp; &amp;nbsp;//gAppUseBonding_d,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .securityModeAndLevel = gSecurityMode_1_Level_4_c,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .maxEncryptionKeySize = mcEncryptionKeySize_c,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .localIoCapabilities = gIoDisplayOnly_c,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .oobAvailable = FALSE,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .centralKeys = (gapSmpKeyFlags_t) (gLtk_c | gIrk_c),&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .peripheralKeys = (gapSmpKeyFlags_t) (gLtk_c | gIrk_c),&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .leSecureConnectionSupported = TRUE,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .useKeypressNotifications = FALSE,&lt;BR /&gt;};&lt;BR /&gt;&lt;BR /&gt;Attached the screenshot while debugging, it goes to HardFault Handler after BLE_Init() function call after trying to connect multiple times&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88768iA22607545DCE6986/image-size/large?v=v2&amp;amp;px=999" title="PairingLog.png" alt="PairingLog.png" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;Do please let me know if something I am doing wrong or following some wrong procedure to enable pairing.&lt;BR /&gt;&lt;BR /&gt;Is there any document explaining steps to Enable and setting Pairing.&lt;/P&gt;&lt;P&gt;I have already gone through BLE developer document.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Aug 2019 06:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960137#M7803</guid>
      <dc:creator>ankur_rathi</dc:creator>
      <dc:date>2019-08-21T06:57:45Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960138#M7804</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone faced this kind of issue?&lt;/P&gt;&lt;P&gt;Need urgent help on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone from NXP help/respond on this ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2019 04:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960138#M7804</guid>
      <dc:creator>ankur_rathi</dc:creator>
      <dc:date>2019-08-23T04:04:40Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960139#M7805</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Strange, I was trying with Bare Metal example code and its not working at all whatever I try to do.&lt;/P&gt;&lt;P&gt;So, I tried with FreeRTOS example code and made the same modifications i.e. only two Macros changed and it works flawlessly every time.&lt;BR /&gt;&lt;BR /&gt;Is there any different setup/steps wrt Bare Metal or any bug which is causing this?&lt;BR /&gt;&lt;BR /&gt;Can anyone provide any info on which is better to use BareMetal or FreeRTOS?&lt;BR /&gt;I don't have much knowledge on RTOS kind of stuff.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2019 05:08:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960139#M7805</guid>
      <dc:creator>ankur_rathi</dc:creator>
      <dc:date>2019-08-23T05:08:29Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960140#M7806</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;Hi&amp;nbsp;&lt;SPAN&gt;Estephania,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;&lt;/P&gt;&lt;P style="color: #51626f; background-color: #ffffff; border: 0px;"&gt;i&amp;nbsp; have a problem about Pairing and bonding,&lt;/P&gt;&lt;P style="border: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="border: 0px;"&gt;while the pairing and bonding and encryption are working fine, but cannot access to the encryption&amp;nbsp; required Characteristic value and description.&lt;/P&gt;&lt;P style="border: 0px;"&gt;you can have a check of my issue,&lt;/P&gt;&lt;P style="border: 0px;"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/511014?commentID=1195965#comment-1195965" style="color: #3d9ce7; background-color: transparent; border: 0px; font-weight: inherit; padding: 1px 0px 1px calc(12px + 0.35ex);"&gt;https://community.nxp.com/message/1195965?commentID=1195965#comment-1195965&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P style="border: 0px;"&gt;&lt;/P&gt;&lt;P style="border: 0px;"&gt;i have reported this issue, but seems no one is looking at this one...&lt;/P&gt;&lt;P style="border: 0px;"&gt;&lt;/P&gt;&lt;P style="border: 0px;"&gt;Regards,&lt;/P&gt;&lt;P style="border: 0px;"&gt;Ziv&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 03:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960140#M7806</guid>
      <dc:creator>zhi_wang</dc:creator>
      <dc:date>2019-08-26T03:43:16Z</dc:date>
    </item>
    <item>
      <title>Re: Qn908x HID Device Pairing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960141#M7807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;With new SDK (SDK_SDK_2.2.1_QN908XCDK), Bare Metal example code is working fine.&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;The new SDK can be downloaded from the link:&lt;/P&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/license?hash=21a9800cfb7c901e52a996ac70522d3d&amp;amp;hash_download=1" target="test_blank"&gt;https://mcuxpresso.nxp.com/en/license?hash=21a9800cfb7c901e52a996ac70522d3d&amp;amp;hash_download=1&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Nov 2019 11:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qn908x-HID-Device-Pairing/m-p/960141#M7807</guid>
      <dc:creator>ankur_rathi</dc:creator>
      <dc:date>2019-11-05T11:05:40Z</dc:date>
    </item>
  </channel>
</rss>