<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic which sdk support ZPS_vSetOverrideLocalMacAddress in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/which-sdk-support-ZPS-vSetOverrideLocalMacAddress/m-p/939575#M7355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;i find function&amp;lt; ZPS_vSetOverrideLocalMacAddress function &amp;gt;&amp;nbsp; at JN-UG-3048, but cannot find it in sdk JN-SW-4170.&lt;/P&gt;&lt;P&gt;i want modify macAddress to simulate a lot nodes by one JN5169. i will change the mac address and try to join the network to test the max nodes my network support. i am using JN-AN-1229 to do the work.&lt;/P&gt;&lt;P&gt;so,&lt;/P&gt;&lt;P&gt;1. how can i use the fun&amp;nbsp;ZPS_vSetOverrideLocalMacAddress, which sdk i should use.&lt;/P&gt;&lt;P&gt;2. how can i simulate a lot nodes by one 5169&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Aug 2019 15:47:10 GMT</pubDate>
    <dc:creator>xubovey</dc:creator>
    <dc:date>2019-08-01T15:47:10Z</dc:date>
    <item>
      <title>which sdk support ZPS_vSetOverrideLocalMacAddress</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/which-sdk-support-ZPS-vSetOverrideLocalMacAddress/m-p/939575#M7355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;i find function&amp;lt; ZPS_vSetOverrideLocalMacAddress function &amp;gt;&amp;nbsp; at JN-UG-3048, but cannot find it in sdk JN-SW-4170.&lt;/P&gt;&lt;P&gt;i want modify macAddress to simulate a lot nodes by one JN5169. i will change the mac address and try to join the network to test the max nodes my network support. i am using JN-AN-1229 to do the work.&lt;/P&gt;&lt;P&gt;so,&lt;/P&gt;&lt;P&gt;1. how can i use the fun&amp;nbsp;ZPS_vSetOverrideLocalMacAddress, which sdk i should use.&lt;/P&gt;&lt;P&gt;2. how can i simulate a lot nodes by one 5169&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Aug 2019 15:47:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/which-sdk-support-ZPS-vSetOverrideLocalMacAddress/m-p/939575#M7355</guid>
      <dc:creator>xubovey</dc:creator>
      <dc:date>2019-08-01T15:47:10Z</dc:date>
    </item>
    <item>
      <title>Re: which sdk support ZPS_vSetOverrideLocalMacAddress</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/which-sdk-support-ZPS-vSetOverrideLocalMacAddress/m-p/939576#M7356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xu,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This address is stored locally in the index sector of Flash memory&lt;/P&gt;&lt;P&gt;The mac address is configured before the&amp;nbsp;ZPS_eAplAfInit. However, the API is using by the OTA Cluster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Caution: If required, this function must be called before the ZigBee PRO stack is initialized.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Aug 2019 20:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/which-sdk-support-ZPS-vSetOverrideLocalMacAddress/m-p/939576#M7356</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2019-08-02T20:17:08Z</dc:date>
    </item>
  </channel>
</rss>