<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: QN9080 BLE overflow problem in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/QN9080-BLE-overflow-problem/m-p/939193#M7354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The API adds to the queue in the controller, if it returns a &lt;EM&gt;&lt;SPAN style="color: #0000ff;"&gt;gBleOverflow_c&lt;/SPAN&gt; &lt;/EM&gt;it means that the queue it's full and you need to wait until you can send a new message, I'll need to investigate further on this. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By any chance, did you modify something else? When you mention a custom device, are you referring to custom profile or are you referring to a custom board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And just to confirm, in your test it starts working correctly and sending the data and after some time it stops? Or It never sends the data ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 Sep 2019 01:55:25 GMT</pubDate>
    <dc:creator>stephanie_m</dc:creator>
    <dc:date>2019-09-05T01:55:25Z</dc:date>
    <item>
      <title>QN9080 BLE overflow problem</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9080-BLE-overflow-problem/m-p/939192#M7353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm trying to solve the BLE overflow problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My project is to send data from client custom device using QN9080-M17 to QN9080-DK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is that after a certain time, an overflow error appears and no data is sent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We use wireless_uart example form SDK_2.x_QN908XCDK and we send data using battery measurement timer callback function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our time interval is 20ms and we send data length of 60 bytes at same interval.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked the "gBleOverflow_c" error is the return value of BLE API functions...so I cannot solve this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I solve this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2019 13:41:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9080-BLE-overflow-problem/m-p/939192#M7353</guid>
      <dc:creator>tpgurtpgur2</dc:creator>
      <dc:date>2019-09-03T13:41:14Z</dc:date>
    </item>
    <item>
      <title>Re: QN9080 BLE overflow problem</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9080-BLE-overflow-problem/m-p/939193#M7354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The API adds to the queue in the controller, if it returns a &lt;EM&gt;&lt;SPAN style="color: #0000ff;"&gt;gBleOverflow_c&lt;/SPAN&gt; &lt;/EM&gt;it means that the queue it's full and you need to wait until you can send a new message, I'll need to investigate further on this. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By any chance, did you modify something else? When you mention a custom device, are you referring to custom profile or are you referring to a custom board ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And just to confirm, in your test it starts working correctly and sending the data and after some time it stops? Or It never sends the data ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2019 01:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9080-BLE-overflow-problem/m-p/939193#M7354</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-09-05T01:55:25Z</dc:date>
    </item>
  </channel>
</rss>