<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Poll control Cluster</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Poll-control-Cluster/m-p/933332#M7250</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I would like to ask a question regarding to the poll control cluster.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After binding the poll control cluster 0x0020 of my End device which uses the &lt;SPAN&gt;JN5169&lt;/SPAN&gt;, the end device sends to the coordinator a check in command. However, the response i get from the coordinator is the following:&lt;/P&gt;&lt;P&gt;Status code:[0xC3] Unsupported Cluster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have programmed my coordinator with the&amp;nbsp;JN-AN-1216-Zigbee-3-0-IoT-ControlBridge and i am using the&amp;nbsp;ZGWUI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the&amp;nbsp;&lt;SPAN&gt;JN-AN-1216&lt;/SPAN&gt; coordinator support the poll control cluster? I could not find anything associate to poll control in the zcl_options.h file of&amp;nbsp;&lt;SPAN&gt;JN-AN-1216&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Aug 2019 11:57:42 GMT</pubDate>
    <dc:creator>kostas1</dc:creator>
    <dc:date>2019-08-16T11:57:42Z</dc:date>
    <item>
      <title>Poll control Cluster</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Poll-control-Cluster/m-p/933332#M7250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I would like to ask a question regarding to the poll control cluster.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After binding the poll control cluster 0x0020 of my End device which uses the &lt;SPAN&gt;JN5169&lt;/SPAN&gt;, the end device sends to the coordinator a check in command. However, the response i get from the coordinator is the following:&lt;/P&gt;&lt;P&gt;Status code:[0xC3] Unsupported Cluster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have programmed my coordinator with the&amp;nbsp;JN-AN-1216-Zigbee-3-0-IoT-ControlBridge and i am using the&amp;nbsp;ZGWUI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the&amp;nbsp;&lt;SPAN&gt;JN-AN-1216&lt;/SPAN&gt; coordinator support the poll control cluster? I could not find anything associate to poll control in the zcl_options.h file of&amp;nbsp;&lt;SPAN&gt;JN-AN-1216&lt;/SPAN&gt;&lt;SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Aug 2019 11:57:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Poll-control-Cluster/m-p/933332#M7250</guid>
      <dc:creator>kostas1</dc:creator>
      <dc:date>2019-08-16T11:57:42Z</dc:date>
    </item>
    <item>
      <title>Re: Poll control Cluster</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Poll-control-Cluster/m-p/933333#M7251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kostas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default, the JN-AN-1216 doesn't have the Poll Control Cluster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could add the Cluster following the chapter&amp;nbsp;20.10 Compile-Time Options&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/user-guide/JN-UG-3115.pdf"&gt;ZigBee Cluster Library (for ZigBee 3.0) User Guide&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, please look at the&amp;nbsp;&amp;nbsp;&lt;SPAN style="font-size: 15px;"&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-335075"&gt;ZigBee 3.0: Adding Clusters&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 15px;"&gt;Mario&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Aug 2019 22:18:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Poll-control-Cluster/m-p/933333#M7251</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2019-08-16T22:18:23Z</dc:date>
    </item>
    <item>
      <title>Re: Poll control Cluster</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Poll-control-Cluster/m-p/933334#M7252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mario,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to ask you a general question regarding to the poll control cluster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming that the poll control cluster is not bind to a parent and when the check in interval expires (for example after 1 hour) does the end device need to enter into&amp;nbsp;a fast polling mode for 7.68 seconds? or&amp;nbsp; does the End device should enter the 7.68 seconds fast polling time when its poll control cluster is bound?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards,&lt;BR /&gt;Kostas&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Aug 2019 15:50:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Poll-control-Cluster/m-p/933334#M7252</guid>
      <dc:creator>kostas1</dc:creator>
      <dc:date>2019-08-22T15:50:24Z</dc:date>
    </item>
    <item>
      <title>Re: Poll control Cluster</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Poll-control-Cluster/m-p/933335#M7253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kostas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It will depend on the values that you have previously set. Please look at the different scenarios, the Zigbee Cluster Libary Spec details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the Poll Control Server receives a Check-In Response from a client for which there is no binding (unbound),&lt;BR /&gt;it SHOULD respond with a Default Response with a status value indicating ACTION_DENIED.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If the Poll Control Server receives a Check-In Response from a client for which there is a binding (bound)&lt;BR /&gt;with an invalid fast poll interval, it SHOULD respond with a Default Response with status INVALID_&lt;BR /&gt;VALUE.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If the Poll Control Server receives a Check-In Response from a bound client after temporary fast poll mode is&lt;BR /&gt;completed it SHOULD respond with a Default Response with a status value indicating TIMEOUT.&lt;BR /&gt;In all of the above cases, the Server SHALL respond with a Default Response not equal to ZCL_SUCCESS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please look at the&amp;nbsp;3.16.5.3.1.2 Fast Poll Timeout&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Aug 2019 21:42:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Poll-control-Cluster/m-p/933335#M7253</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2019-08-23T21:42:16Z</dc:date>
    </item>
  </channel>
</rss>