<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Customize beacon fields in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931172#M7166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am able to achieve my task partially. I used&amp;nbsp;NVIC_SystemReset(), but this would reset the entire program. I am looking for reset functionality like pressing SW3 of frdm kw41z would do. (like a reflashing but erasing existing memory). Can you help me in this aspect?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Niranjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Sep 2019 04:51:29 GMT</pubDate>
    <dc:creator>trialaccount12</dc:creator>
    <dc:date>2019-09-12T04:51:29Z</dc:date>
    <item>
      <title>Customize beacon fields</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931166#M7160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;It is possible to customize the fields in beacons(I am working with kw41z). I looked into ibeacon and it has an array of 25 bytes. In my case, i want to send one more additional value from my program as a part of 25 bytes.&lt;/P&gt;&lt;P&gt;Is it possible to do that? I tried to modify the code base and all the functions are constant. They expect a static value whereas my new value is dynamic and it changes every second. Can you please tell me if my approach is possible?&amp;nbsp; Any alternatives would also be helpful.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Basically I should be able to witness UUID, Major value along with my dynamically generated value when I scan for the device in my mobile app.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Niranjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Aug 2019 23:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931166#M7160</guid>
      <dc:creator>trialaccount12</dc:creator>
      <dc:date>2019-08-30T23:32:49Z</dc:date>
    </item>
    <item>
      <title>Re: Customize beacon fields</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931167#M7161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if you are exactly looking for a beacon you can check this post &lt;A href="https://community.nxp.com/docs/DOC-329201"&gt;https://community.nxp.com/docs/DOC-329201&lt;/A&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Could you please check it and let me know if that it's helpful for you?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;BR /&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2019 19:40:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931167#M7161</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-09-02T19:40:11Z</dc:date>
    </item>
    <item>
      <title>Re: Customize beacon fields</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931168#M7162</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; Yes, I looked into the document. But the examples/demo applications in SDK shows the advertising fields like UUID,beacon identifier, company identifier are getting added to&amp;nbsp;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;adData1 as static values which remains unique. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;In my application, I want to add a dynamic value like acceleration of device(x or y or z) along with advertising packet. [That is the value has to be added in run time of application rather than during compile time]&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;Is it possible to add this functionality?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;Thanks and Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff;"&gt;Niranjan&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Sep 2019 19:35:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931168#M7162</guid>
      <dc:creator>trialaccount12</dc:creator>
      <dc:date>2019-09-03T19:35:27Z</dc:date>
    </item>
    <item>
      <title>Re: Customize beacon fields</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931169#M7163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How many bytes will you be needing in your packet? If you can provide more details about this I can investigate further on this. I believe it should be possible if the packet you want to send it's compliant with the advertisement packet structure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which version&amp;nbsp; of the SDK are you using ? Could you please help me confirm that you are using the latest one available in the SDK builder?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The process to follow will change in case you have a previous version of the examples&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Sep 2019 02:33:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931169#M7163</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-09-05T02:33:53Z</dc:date>
    </item>
    <item>
      <title>Re: Customize beacon fields</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931170#M7164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; Yes, I am able to figure it out and advertise customized packets now. Now I have two new questions&lt;/P&gt;&lt;P&gt;1. How would I restart the beacon advertising every second (beacon application fields A,B,C is getting changed in my project). Any documentation for this? please note that I am not having two tasks in my rtos code. Inside the single main_task I am executing all.&lt;/P&gt;&lt;P&gt;2. The FXOS8700Q is subjected to soft and hard iron magnetic effects(I read this in a community post). But I dont intend to calibrate the device every-time I switch it on. Is there any static offsets to be given? To be specific I want my device to function like an ecompass in android phone.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help.&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;P&gt;Niranjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Sep 2019 18:28:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931170#M7164</guid>
      <dc:creator>trialaccount12</dc:creator>
      <dc:date>2019-09-07T18:28:07Z</dc:date>
    </item>
    <item>
      <title>Re: Customize beacon fields</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931171#M7165</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;'Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is not a specific document to achieve what you are looking for. It won't be possible to do it in the main task, you will need to use a timer and either a task or function triggered to update the values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the e-compass, could you please check this post ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/350457"&gt;https://community.nxp.com/thread/350457&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Sep 2019 16:03:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931171#M7165</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-09-09T16:03:28Z</dc:date>
    </item>
    <item>
      <title>Re: Customize beacon fields</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931172#M7166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am able to achieve my task partially. I used&amp;nbsp;NVIC_SystemReset(), but this would reset the entire program. I am looking for reset functionality like pressing SW3 of frdm kw41z would do. (like a reflashing but erasing existing memory). Can you help me in this aspect?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Niranjan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 04:51:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931172#M7166</guid>
      <dc:creator>trialaccount12</dc:creator>
      <dc:date>2019-09-12T04:51:29Z</dc:date>
    </item>
    <item>
      <title>Re: Customize beacon fields</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931173#M7167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Due to my current load of work, and as this it's a different matter, could you please help me posting it in a different thread ? So we can have the information in a more organized way and also for this to be check not only by me but for other persons as well that might be able to help you &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Sep 2019 14:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Customize-beacon-fields/m-p/931173#M7167</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-09-12T14:59:25Z</dc:date>
    </item>
  </channel>
</rss>