<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: Is the KW01 sub-GHz SMAC inserting extra bytes into the packet?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Is-the-KW01-sub-GHz-SMAC-inserting-extra-bytes-into-the-packet/m-p/456231#M709</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brant,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, SMAC doesn´t insert extra bytes in the packet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please verify if this behavior is also reproduced with a &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;bit rate = 50000 bps, FSK modulation and packet mode?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Burgos.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Sep 2015 16:56:19 GMT</pubDate>
    <dc:creator>luisburgos</dc:creator>
    <dc:date>2015-09-22T16:56:19Z</dc:date>
    <item>
      <title>Is the KW01 sub-GHz SMAC inserting extra bytes into the packet?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Is-the-KW01-sub-GHz-SMAC-inserting-extra-bytes-into-the-packet/m-p/456230#M708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am transmitting from a simple loop program that I wrote. I am sending the same packet over and over again using the MRB-KW01 development board. I am receiving the packets using another MRB-KW01 that is running the SMAC graphical user interface (GUI) that came loaded on the rcvr board. The frequency is 915 MHz, bit rate = 4800 bps, OOK, continuous mode. I am sending a packet with a 3-byte preamble, a 4-byte sync word, and 8 bytes of payload. Each payload byte is 0x4F. I am monitoring the received packets with an o'scope on the data &amp;amp; clk outputs on j18, the bit error rate test port, of the rcvr MRB-KW01. I am seeing 4 extra bytes inserted into the packet&amp;nbsp; right after the adr byte and before the payload bytes. Also 2 bytes are inserted after the payload and before the CRC byes. Please see attached jpgs. Might anyone know why these mystery bytes (marked with ? marks) are there? Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Sep 2015 18:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Is-the-KW01-sub-GHz-SMAC-inserting-extra-bytes-into-the-packet/m-p/456230#M708</guid>
      <dc:creator>stronglikebool</dc:creator>
      <dc:date>2015-09-16T18:00:31Z</dc:date>
    </item>
    <item>
      <title>Re: Is the KW01 sub-GHz SMAC inserting extra bytes into the packet?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Is-the-KW01-sub-GHz-SMAC-inserting-extra-bytes-into-the-packet/m-p/456231#M709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Brant,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No, SMAC doesn´t insert extra bytes in the packet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please verify if this behavior is also reproduced with a &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;bit rate = 50000 bps, FSK modulation and packet mode?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Burgos.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Sep 2015 16:56:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Is-the-KW01-sub-GHz-SMAC-inserting-extra-bytes-into-the-packet/m-p/456231#M709</guid>
      <dc:creator>luisburgos</dc:creator>
      <dc:date>2015-09-22T16:56:19Z</dc:date>
    </item>
  </channel>
</rss>