<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NFC Reader Library Port to MDK Keil in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/NFC-Reader-Library-Port-to-MDK-Keil/m-p/899943#M6603</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm Eric.Now I have some questions about CLRC663:O&lt;/P&gt;&lt;P&gt;1. When I use OM26630 FDK to test NFC tag, the block data can be read and written.&amp;nbsp;But RF430FRL152H (NTAG from TI) tag was used, block data &lt;SPAN&gt;can not be read,even UID&amp;nbsp;&lt;/SPAN&gt;. When non-NXP card be used, how do I need to modify the program?&lt;/P&gt;&lt;P&gt;2. NXP NFC Reader Library currently only has MCUXpresso version. I port it to MDK and IAR, there were many errors, mainly in macro definition. Is there an engineering example of MDK Keil version?If not,How I can port it by muyself?&lt;/P&gt;&lt;P&gt;3. What is the exactly process of reading ISO15693 card by NFC Reader Library? Have external interrupts and timer interrupts been used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Apr 2019 08:01:49 GMT</pubDate>
    <dc:creator>eric_wanghao</dc:creator>
    <dc:date>2019-04-18T08:01:49Z</dc:date>
    <item>
      <title>NFC Reader Library Port to MDK Keil</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NFC-Reader-Library-Port-to-MDK-Keil/m-p/899943#M6603</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm Eric.Now I have some questions about CLRC663:O&lt;/P&gt;&lt;P&gt;1. When I use OM26630 FDK to test NFC tag, the block data can be read and written.&amp;nbsp;But RF430FRL152H (NTAG from TI) tag was used, block data &lt;SPAN&gt;can not be read,even UID&amp;nbsp;&lt;/SPAN&gt;. When non-NXP card be used, how do I need to modify the program?&lt;/P&gt;&lt;P&gt;2. NXP NFC Reader Library currently only has MCUXpresso version. I port it to MDK and IAR, there were many errors, mainly in macro definition. Is there an engineering example of MDK Keil version?If not,How I can port it by muyself?&lt;/P&gt;&lt;P&gt;3. What is the exactly process of reading ISO15693 card by NFC Reader Library? Have external interrupts and timer interrupts been used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Apr 2019 08:01:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NFC-Reader-Library-Port-to-MDK-Keil/m-p/899943#M6603</guid>
      <dc:creator>eric_wanghao</dc:creator>
      <dc:date>2019-04-18T08:01:49Z</dc:date>
    </item>
    <item>
      <title>Re: NFC Reader Library Port to MDK Keil</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NFC-Reader-Library-Port-to-MDK-Keil/m-p/899944#M6604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. As I know, RF430FRL152H is an ISO15693 tag, did you use the right example for this type of tag?&lt;/P&gt;&lt;P&gt;2.I think you may use LPCopen as a reference, which supports IAR and Keil, please refer to &lt;A class="link-titled" href="https://www.nxp.com/support/developer-resources/software-development-tools/lpc-developer-resources-/lpcopen-libraries-and-examples:LPC-OPEN-LIBRARIES?lang=en&amp;amp;lang_cd=en&amp;amp;" title="https://www.nxp.com/support/developer-resources/software-development-tools/lpc-developer-resources-/lpcopen-libraries-and-examples:LPC-OPEN-LIBRARIES?lang=en&amp;amp;lang_cd=en&amp;amp;"&gt;LPCOpen Libraries and Examples | NXP&lt;/A&gt; for details. BTW, what is the reason for IAR or Keil porting? MCUXpresso is a free IDE and easy to use...&lt;/P&gt;&lt;P&gt;3.We provide an example in the NFC reader library as shown below, you may use it as a starting point.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80224iB45359893AB869CE/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 08:47:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NFC-Reader-Library-Port-to-MDK-Keil/m-p/899944#M6604</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2019-04-23T08:47:12Z</dc:date>
    </item>
  </channel>
</rss>