<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックZigbee Cluster Library,Network Rejoining with Non Volatile Memory?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437776#M609</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good Morning,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on a dimmable lamp, i've used a beekit preset and it works but i have a problem with the network rejoin.&lt;/P&gt;&lt;P&gt;What i want to do is make it remember the previous network, in way that&amp;nbsp; when&amp;nbsp; power out the lamp, once the power is back, it automatically&amp;nbsp; rejoin into the network.&lt;/P&gt;&lt;P&gt;I've seen that the beekit preset have a section in the code dedicated to storage data in the&amp;nbsp; NVM, but i&amp;nbsp; don't know how to use it.&lt;/P&gt;&lt;P&gt;So want to know is which data I need to storage in the NVM and how i do it , to make a network rejoin?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The microcontroller i’m using is MC13237CHT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Manuel Báez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Oct 2015 14:04:16 GMT</pubDate>
    <dc:creator>manuelbaez</dc:creator>
    <dc:date>2015-10-28T14:04:16Z</dc:date>
    <item>
      <title>Zigbee Cluster Library,Network Rejoining with Non Volatile Memory?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437776#M609</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good Morning,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on a dimmable lamp, i've used a beekit preset and it works but i have a problem with the network rejoin.&lt;/P&gt;&lt;P&gt;What i want to do is make it remember the previous network, in way that&amp;nbsp; when&amp;nbsp; power out the lamp, once the power is back, it automatically&amp;nbsp; rejoin into the network.&lt;/P&gt;&lt;P&gt;I've seen that the beekit preset have a section in the code dedicated to storage data in the&amp;nbsp; NVM, but i&amp;nbsp; don't know how to use it.&lt;/P&gt;&lt;P&gt;So want to know is which data I need to storage in the NVM and how i do it , to make a network rejoin?.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The microcontroller i’m using is MC13237CHT.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Manuel Báez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Oct 2015 14:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437776#M609</guid>
      <dc:creator>manuelbaez</dc:creator>
      <dc:date>2015-10-28T14:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: Zigbee Cluster Library,Network Rejoining with Non Volatile Memory?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437777#M610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Manuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assuming you are using codebase 3.1.1, in the case of the Ha Dimmable Light demo application, with the default configuration, it should be enough to set the gNvStorageIncluded_d define to TRUE for an existing project, or check the option "Non-Volatile Memory" when creating the project in BeeKit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After a device joins a network the stack will automatically save all the required network information into NVM. At startup the Ha Dimmable Light demo application will check if the device was previously on a network and, if that is the case, use the NVM information to silently rejoin the network. This way the device should automatically resume normal operation once the power is back on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the demo application the code for rejoining the network with NVM is located at the end of the BeeAppInit() function in BeeApp.c, where the ZDO_Start() function is called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Cosmin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2015 14:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437777#M610</guid>
      <dc:creator>cosmingrumei</dc:creator>
      <dc:date>2015-10-29T14:04:54Z</dc:date>
    </item>
    <item>
      <title>Re: Zigbee Cluster Library,Network Rejoining with Non Volatile Memory?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437778#M611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cosmin, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for answering my question,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="line-height: 1.5;"&gt;I've tried that but the first time i restart the device, it just seems like it has successfully connected to the network but it doesn't, the second time it just do nothing. &lt;/SPAN&gt;I don't know i there is any way to know if the data saved is wrong or not, but if there is, i would like to know it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Manuel&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2015 19:23:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437778#M611</guid>
      <dc:creator>manuelbaez</dc:creator>
      <dc:date>2015-10-29T19:23:59Z</dc:date>
    </item>
    <item>
      <title>Re: Zigbee Cluster Library,Network Rejoining with Non Volatile Memory?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437779#M612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Manuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ran the Ha Dimmable LIght (Coordinator) and Switch (Router) demo applications and everything works Ok. Once the boards are programmed, start the commissioning process and then go to the run mode in both boards. If you don't know if the NVM module has devices stored please long press the SW2 to reset to factory defaults.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(From the ZigBee applications user's guide):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51930iAB8F99AECA38C6E0/image-size/large?v=v2&amp;amp;px=999" title="zaug.jpg" alt="zaug.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Once the demo is working, reset one MCU, since the initial mode is configuration you need to long press the SW1 to go to the run mode again, it should be working without repeating the commissioning process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if this works for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Nov 2015 17:22:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437779#M612</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2015-11-03T17:22:42Z</dc:date>
    </item>
    <item>
      <title>Re: Zigbee Cluster Library,Network Rejoining with Non Volatile Memory?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437780#M613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Earl,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried that and it gets connected to the network, but immediately gets stuck in identify mode for a few minutes and then just stops.&lt;/P&gt;&lt;P&gt;I think It just doesn't get into run mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Best regards,&lt;/P&gt;&lt;P style="font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif; color: #51626f;"&gt;Manuel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Nov 2015 21:21:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437780#M613</guid>
      <dc:creator>manuelbaez</dc:creator>
      <dc:date>2015-11-04T21:21:49Z</dc:date>
    </item>
    <item>
      <title>Re: Zigbee Cluster Library,Network Rejoining with Non Volatile Memory?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437781#M614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Manuel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is your switch a router or an end device? Please configure it as a router. Since the end device is sleepy, it would be useful to discard that the problem is related with the low power configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached my BeeKit configurations. I tested with the MC13234C MCU so you need to change it to the MC13237C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3315iA791E73C63BD260C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Nov 2015 16:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Zigbee-Cluster-Library-Network-Rejoining-with-Non-Volatile/m-p/437781#M614</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2015-11-06T16:34:26Z</dc:date>
    </item>
  </channel>
</rss>