<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Module with SN5169 or SN5179, 125 °C in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Module-with-SN5169-or-SN5179-125-C/m-p/868525#M6057</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;SN5169 or SN5179&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I would like to test a module with integrated antenna in an environment with 125 °C. All the modules I found are only specified up to 85 °C. Is it possible to order an amount of modules with the 125-degree-IC on it? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Jan 2019 12:57:22 GMT</pubDate>
    <dc:creator>juergen_schwage</dc:creator>
    <dc:date>2019-01-29T12:57:22Z</dc:date>
    <item>
      <title>Module with SN5169 or SN5179, 125 °C</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Module-with-SN5169-or-SN5179-125-C/m-p/868525#M6057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;SN5169 or SN5179&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I would like to test a module with integrated antenna in an environment with 125 °C. All the modules I found are only specified up to 85 °C. Is it possible to order an amount of modules with the 125-degree-IC on it? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 12:57:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Module-with-SN5169-or-SN5179-125-C/m-p/868525#M6057</guid>
      <dc:creator>juergen_schwage</dc:creator>
      <dc:date>2019-01-29T12:57:22Z</dc:date>
    </item>
    <item>
      <title>Re: Module with SN5169 or SN5179, 125 °C</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Module-with-SN5169-or-SN5179-125-C/m-p/868526#M6058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juergen,&lt;/P&gt;&lt;P&gt;Just to confirm, is the JN5169 that you are referring&amp;nbsp;for?&amp;nbsp;&lt;/P&gt;&lt;P&gt;The JN5169 Module&amp;nbsp;Temperature range: 40 C to +85 C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, we do not provide a module that supports 125 C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 17:54:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Module-with-SN5169-or-SN5179-125-C/m-p/868526#M6058</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2019-01-29T17:54:14Z</dc:date>
    </item>
    <item>
      <title>Re: Module with SN5169 or SN5179, 125 °C</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Module-with-SN5169-or-SN5179-125-C/m-p/868527#M6059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for this information. &lt;BR /&gt;Sorry for my typing error: This question concerns the ICs &lt;STRONG&gt;J&lt;/STRONG&gt;N5169 and &lt;STRONG&gt;J&lt;/STRONG&gt;N5179.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which is the best way to realise a board with one of these ICs? From the customers point of view, I think the best way is to take the NXP-Designs for modules with integrated antenne, produce a PCB, and populate it with the 125-degree-version of the SoC. Does NXP provide the schematics and PCB-Designs of the modules to customers?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 20:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Module-with-SN5169-or-SN5179-125-C/m-p/868527#M6059</guid>
      <dc:creator>juergen_schwage</dc:creator>
      <dc:date>2019-01-29T20:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: Module with SN5169 or SN5179, 125 °C</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Module-with-SN5169-or-SN5179-125-C/m-p/868528#M6060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Juergen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend the JN5169 device, the IC supports 125 grades, but the JN516X module supports 85-degree.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Does NXP provide the schematics and PCB-Designs of the modules to customers?&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/wireless/proprietary-ieee-802.15.4-based/support-resources-for-jn516x-mcus:SUPPORT-RESOURCES-JN516X-MCUS"&gt;Support Resources for JN516x MCUs&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;JN-RD-6038&amp;nbsp;and the JN-RD-6036&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN class="" data-dtmaction="Social Share Email Click"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2019 21:34:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Module-with-SN5169-or-SN5179-125-C/m-p/868528#M6060</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2019-01-29T21:34:15Z</dc:date>
    </item>
  </channel>
</rss>