<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: [MKW41Z] CCA on GENFSK</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860190#M5905</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please, any news about this? It's a very urgent task for us.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Mar 2019 16:02:15 GMT</pubDate>
    <dc:creator>domenico_virgil</dc:creator>
    <dc:date>2019-03-21T16:02:15Z</dc:date>
    <item>
      <title>[MKW41Z] CCA on GENFSK</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860189#M5904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;we need to perform a CCA using GENFSK.&lt;/P&gt;&lt;P&gt;From the datasheet we saw that the &lt;EM&gt;CCA treshold&lt;/EM&gt; is supported only in the ZLL, but we want to put a treshold in software to compare with ED value.&lt;/P&gt;&lt;P&gt;In the documentation of the Receiver Digital Module in MKW41Z Reference Manual (page 1673), is reported that the Digital Module can return the ED value from the &lt;EM&gt;rx_cca_ed_lqi&lt;/EM&gt; which, in turn, uses the &lt;EM&gt;w/rssi&lt;/EM&gt; signal from &lt;EM&gt;rx_agc&lt;/EM&gt; Module.&lt;/P&gt;&lt;P&gt;So we supposed, following the manual, that we can use &lt;EM&gt;XcvrFskGetInstantRssi&lt;/EM&gt; test function provided in MCUXPRESSO_SDK v 2.2.0 to perform an RX WarmUp, read the &lt;EM&gt;XCVR CCA_ED_LQI_STAT_0&lt;/EM&gt; register and get the ED value, but this approach doesn't work.&lt;/P&gt;&lt;P&gt;The table 45-20 (page 1686 - Reference Manual) shows the two signals which needs to be configured to raise &lt;EM&gt;CCA1/ED&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;meas. state &lt;/EM&gt;&lt;EM&gt;(wideband &lt;/EM&gt;&lt;EM&gt;mode). &lt;/EM&gt;The signal &lt;EM&gt;cca1_ed_trig&lt;/EM&gt; should be triggered on RX WarmUp, the second one, &lt;EM&gt;sfd_aa_match,&lt;/EM&gt; has no references in the Reference Manual.&lt;/P&gt;&lt;P&gt;So the questions are:&lt;/P&gt;&lt;P&gt;1) It's possible to use &lt;EM&gt;RSSI/CCA1/LQI&lt;/EM&gt; module in direct manner using the Receiver Digital Module and it's registers, without using the ZLL Module registers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) If not, is there a way to software compute the ED, starting from the &lt;EM&gt;istant RSSI&lt;/EM&gt; value?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We think that once computed the ED, we can address in our firmware a CCA threshold value and design a CA strategy to avoid collisions.&lt;/P&gt;&lt;P&gt;Have you any hint which can put us on the right path?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Domenico Virgilio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2019 10:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860189#M5904</guid>
      <dc:creator>domenico_virgil</dc:creator>
      <dc:date>2019-03-15T10:46:55Z</dc:date>
    </item>
    <item>
      <title>Re: [MKW41Z] CCA on GENFSK</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860190#M5905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please, any news about this? It's a very urgent task for us.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 16:02:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860190#M5905</guid>
      <dc:creator>domenico_virgil</dc:creator>
      <dc:date>2019-03-21T16:02:15Z</dc:date>
    </item>
    <item>
      <title>Re: [MKW41Z] CCA on GENFSK</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860191#M5906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will need to investigate in further detail if this it's possible in the way you want to, as I'm not sure how it can be implemented when using the GFSK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll need some time to check this out.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the inconveniences this might cause you.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;BR /&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Mar 2019 21:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860191#M5906</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-03-21T21:03:09Z</dc:date>
    </item>
    <item>
      <title>Re: [MKW41Z] CCA on GENFSK</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860192#M5907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Estephania,&lt;/P&gt;&lt;P&gt;thank you for the answer.&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;I hope that what I want to do is possible.&lt;/P&gt;&lt;P&gt;Just a question: since the &lt;EM&gt;RSSI / CCA1 / LQI&lt;/EM&gt; module is located in the RX Digital, it would be possible to use it bypassing the various Link Layers and directly using the RX Digital module, without going through the GENFSK, if the GENFSK does not support this functionality?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Domenico Virgilio&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Mar 2019 15:57:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860192#M5907</guid>
      <dc:creator>domenico_virgil</dc:creator>
      <dc:date>2019-03-26T15:57:12Z</dc:date>
    </item>
    <item>
      <title>Re: [MKW41Z] CCA on GENFSK</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860193#M5908</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, I was not able to locate any further information regarding the topic, but I do not believe it is possible to bypass the different link layers as it would appear that when setting the GFSK you can't use it due to the radio settings, nonetheless, you can try it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Sorry for the inconveniences this might cause you, but all the information that you have it's the one available.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&amp;nbsp;&lt;BR /&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Mar 2019 21:16:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MKW41Z-CCA-on-GENFSK/m-p/860193#M5908</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-03-27T21:16:28Z</dc:date>
    </item>
  </channel>
</rss>