<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックFLEXIO frdmkw36</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/FLEXIO-frdmkw36/m-p/846374#M5685</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;I work on project on&amp;nbsp;frdmkw36 that depend's 2 UART interface, so i need to implement an other Software UART because the FRDMKW36 provide only one UART inerface.&lt;/P&gt;&lt;P&gt;I need to implement the second interface with the FLEXIO API that i didn't see it in the SDK.&lt;/P&gt;&lt;P&gt;i want to confirm that the FLEXIO API is available or not in the&amp;nbsp;&lt;SPAN&gt;FRDMKW36&amp;nbsp; SDK.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Nov 2018 10:47:34 GMT</pubDate>
    <dc:creator>hayouniaymen</dc:creator>
    <dc:date>2018-11-16T10:47:34Z</dc:date>
    <item>
      <title>FLEXIO frdmkw36</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FLEXIO-frdmkw36/m-p/846374#M5685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello community,&lt;/P&gt;&lt;P&gt;I work on project on&amp;nbsp;frdmkw36 that depend's 2 UART interface, so i need to implement an other Software UART because the FRDMKW36 provide only one UART inerface.&lt;/P&gt;&lt;P&gt;I need to implement the second interface with the FLEXIO API that i didn't see it in the SDK.&lt;/P&gt;&lt;P&gt;i want to confirm that the FLEXIO API is available or not in the&amp;nbsp;&lt;SPAN&gt;FRDMKW36&amp;nbsp; SDK.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Nov 2018 10:47:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FLEXIO-frdmkw36/m-p/846374#M5685</guid>
      <dc:creator>hayouniaymen</dc:creator>
      <dc:date>2018-11-16T10:47:34Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXIO frdmkw36</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FLEXIO-frdmkw36/m-p/846375#M5686</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the inconvenience this might cause you, but the KW36 does not have a FlexIo module. You can check the &lt;A href="https://www.nxp.com/docs/en/reference-manual/MKW36A512RM.pdf"&gt;reference manual&lt;/A&gt;. Nonetheless, if you check the&amp;nbsp;Table 2-1. Feature Summary&amp;nbsp;on page 69 you might find that there are two LPUART modules for KW36 and one LPUART module for KW35 as well as the rest of available communication interfaces.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76360i3E3D20EB86E15E68/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Nov 2018 17:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FLEXIO-frdmkw36/m-p/846375#M5686</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2018-11-16T17:38:25Z</dc:date>
    </item>
  </channel>
</rss>