<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: beacon package in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/beacon-package/m-p/838423#M5576</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Remember The time Delta is the time interval between 2 captured packets, which is calculated based on the elapsed time from the previous packet regardless of its source network or channel. are the same device 0xDBB3 and the one that is sending the beacon request?&lt;/P&gt;&lt;P&gt;What is the application note that you are working on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Sep 2018 20:21:14 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2018-09-10T20:21:14Z</dc:date>
    <item>
      <title>beacon package</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/beacon-package/m-p/838422#M5575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hardware:JN5169&lt;/P&gt;&lt;P&gt;software:zigbee 3.0&amp;nbsp; --- end device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The end device has been added the network built by coordinator. The end device will poll 250&amp;nbsp;milliseconds once. Sometime, the following phenonmena are as follows when I remove&amp;nbsp;&lt;SPAN&gt;coordinator(poweroff).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67694iF8DF53BF302474A8/image-size/large?v=v2&amp;amp;px=999" title="zigbee_7.png" alt="zigbee_7.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;bag tool:Ubiqua Protocol Analyzer&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The last beacon request is too long to come. This will result in a large amount of electricity consumption.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;How can I control the exception?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Aug 2018 12:44:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/beacon-package/m-p/838422#M5575</guid>
      <dc:creator>zherlei</dc:creator>
      <dc:date>2018-08-29T12:44:13Z</dc:date>
    </item>
    <item>
      <title>Re: beacon package</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/beacon-package/m-p/838423#M5576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Remember The time Delta is the time interval between 2 captured packets, which is calculated based on the elapsed time from the previous packet regardless of its source network or channel. are the same device 0xDBB3 and the one that is sending the beacon request?&lt;/P&gt;&lt;P&gt;What is the application note that you are working on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2018 20:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/beacon-package/m-p/838423#M5576</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2018-09-10T20:21:14Z</dc:date>
    </item>
  </channel>
</rss>