<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: Can not enter the callback function when I use UART0</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Can-not-enter-the-callback-function-when-I-use-UART0/m-p/836109#M5538</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gao Lei,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please try to call&amp;nbsp;OS_ISR(&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;APP_myisrUart&lt;/SPAN&gt;)?&lt;/P&gt;&lt;P&gt;Also, you have to add the interrupt source,Uart in this case in the .oscfgdiag file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Nov 2018 22:28:42 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2018-11-21T22:28:42Z</dc:date>
    <item>
      <title>Can not enter the callback function when I use UART0</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Can-not-enter-the-callback-function-when-I-use-UART0/m-p/836107#M5536</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;I am working on the &lt;/SPAN&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;JN-AN-1189.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff; border: 0px; font-size: 14px;"&gt;PRIVATE void vUart_Init(void)&lt;BR /&gt;{&lt;BR /&gt; vAHI_UartEnable(E_AHI_UART_0);&lt;BR /&gt; vAHI_UartReset(E_AHI_UART_0, TRUE, TRUE);&lt;BR /&gt; vAHI_UartReset(E_AHI_UART_0, FALSE, FALSE);&lt;BR /&gt; vAHI_UartSetBaudRate(E_AHI_UART_0, E_AHI_UART_RATE_115200);&lt;BR /&gt; vAHI_UartSetRTSCTS(E_AHI_UART_0, FALSE);&lt;BR /&gt; vAHI_UartSetControl(E_AHI_UART_0, FALSE, FALSE, E_AHI_UART_WORD_LEN_8, TRUE, FALSE); /* [I SP001222_P1 279] */&lt;BR /&gt; vAHI_Uart0RegisterCallback ( APP_myisrUart );&lt;BR /&gt; vAHI_UartSetInterrupt(E_AHI_UART_0, FALSE, TRUE, TRUE, TRUE, E_AHI_UART_FIFO_LEVEL_1);&lt;BR /&gt;}&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PUBLIC void APP_myisrUart(uint32 u32Device, uint32 u32ItemBitmap)&lt;BR /&gt;{&lt;BR /&gt; unsigned int irq = ((*((volatile uint32 *)(UART_START_ADR + 0x08))) &amp;gt;&amp;gt; 1) &amp;amp; 0x0007;&lt;BR /&gt; uint8 u8Byte;&lt;BR /&gt; vAHI_UartWriteData(E_AHI_UART_0, 0x33);&lt;BR /&gt; vAHI_UartWriteData(E_AHI_UART_0, 0x33);&lt;BR /&gt; if (irq &amp;amp; E_AHI_UART_INT_RXDATA)&lt;BR /&gt; {&lt;BR /&gt; u8Byte = u8AHI_UartReadData(E_AHI_UART_0);&lt;BR /&gt; vAHI_UartWriteData(E_AHI_UART_0, u8Byte);&lt;BR /&gt; //if(ZQ_bQueueSend(&amp;amp;APP_msgSerialRx, &amp;amp;u8Byte) == FALSE)&lt;BR /&gt; //{&lt;BR /&gt; // /* Failed to send the message to queue */&lt;BR /&gt; //}&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;if (irq &amp;amp; E_AHI_UART_INT_TX)&lt;BR /&gt; {&lt;BR /&gt; /*if(ZQ_bQueueReceive(&amp;amp;APP_msgSerialTx, &amp;amp;u8Byte) == TRUE)&lt;BR /&gt; {&lt;BR /&gt; vAHI_UartWriteData(E_AHI_UART_0, u8Byte);&lt;BR /&gt; decrement activity counter for dequeued data&lt;BR /&gt; }&lt;BR /&gt; else&lt;BR /&gt; {&lt;BR /&gt; disable tx interrupt as nothing to send&lt;BR /&gt; UART_vSetTxInterrupt(FALSE);&lt;BR /&gt; }*/&lt;BR /&gt; }&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note:&amp;nbsp;I have seen suggestions in&lt;A _jive_internal="true" data-containerid="11235" data-containertype="14" data-content-finding="Community" data-objectid="462011" data-objecttype="1" href="https://community.nxp.com/thread/462011" style="color: #3d9ce7; background-color: #ffffff; border: 0px; padding: 1px 0px 1px calc(12px + 0.35ex);"&gt;JN5168 UART vAHI_Uart0RegisterCallback() Using&lt;/A&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&amp;nbsp;，but it has no effect.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;The send function can be used normally, but&amp;nbsp;the callback function of&amp;nbsp;&lt;SPAN style="color: #3d3d3d;"&gt;APP_myisrUart()&amp;nbsp;has no effect。&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;can you help me to solve it?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;Thank you !&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Sep 2018 07:39:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Can-not-enter-the-callback-function-when-I-use-UART0/m-p/836107#M5536</guid>
      <dc:creator>2433841893</dc:creator>
      <dc:date>2018-09-18T07:39:21Z</dc:date>
    </item>
    <item>
      <title>Re: Can not enter the callback function when I use UART0</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Can-not-enter-the-callback-function-when-I-use-UART0/m-p/836108#M5537</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Is there anyone, this problem has been bothering me for a few days, can you help me analyze it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 07:38:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Can-not-enter-the-callback-function-when-I-use-UART0/m-p/836108#M5537</guid>
      <dc:creator>2433841893</dc:creator>
      <dc:date>2018-09-25T07:38:26Z</dc:date>
    </item>
    <item>
      <title>Re: Can not enter the callback function when I use UART0</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Can-not-enter-the-callback-function-when-I-use-UART0/m-p/836109#M5538</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gao Lei,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please try to call&amp;nbsp;OS_ISR(&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;APP_myisrUart&lt;/SPAN&gt;)?&lt;/P&gt;&lt;P&gt;Also, you have to add the interrupt source,Uart in this case in the .oscfgdiag file&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 22:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Can-not-enter-the-callback-function-when-I-use-UART0/m-p/836109#M5538</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2018-11-21T22:28:42Z</dc:date>
    </item>
  </channel>
</rss>