<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Replace with the same type function, an error happen in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Replace-with-the-same-type-function-an-error-happen/m-p/799370#M5100</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As we see in the picture: when I try to change the&amp;nbsp;function "....AsInitiator" and rebuilt the projet , an error happen .These two functions ,&lt;SPAN&gt;"....AsInitiator" and "....AsTarget" ,&amp;nbsp;&lt;/SPAN&gt;should be the same type and on the same header file, why is there an error that can't find the object? Undefined Symbol ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Sep 2018 08:21:30 GMT</pubDate>
    <dc:creator>964884134</dc:creator>
    <dc:date>2018-09-26T08:21:30Z</dc:date>
    <item>
      <title>Replace with the same type function, an error happen</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Replace-with-the-same-type-function-an-error-happen/m-p/799370#M5100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As we see in the picture: when I try to change the&amp;nbsp;function "....AsInitiator" and rebuilt the projet , an error happen .These two functions ,&lt;SPAN&gt;"....AsInitiator" and "....AsTarget" ,&amp;nbsp;&lt;/SPAN&gt;should be the same type and on the same header file, why is there an error that can't find the object? Undefined Symbol ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Sep 2018 08:21:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Replace-with-the-same-type-function-an-error-happen/m-p/799370#M5100</guid>
      <dc:creator>964884134</dc:creator>
      <dc:date>2018-09-26T08:21:30Z</dc:date>
    </item>
    <item>
      <title>Re: Replace with the same type function, an error happen</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Replace-with-the-same-type-function-an-error-happen/m-p/799371#M5101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="margin-bottom: .0001pt;"&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Could you please share with me the release version of the SDK you are using? I just downloaded the latest one and the latest AN1217, just changed that line just as you have it and everything builds correctly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73618iAC958A1E98125C7B/image-size/large?v=v2&amp;amp;px=999" title="target build.png" alt="target build.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;&lt;BR /&gt;Did you modify something else?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Regards,&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Estephania&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Oct 2018 19:03:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Replace-with-the-same-type-function-an-error-happen/m-p/799371#M5101</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2018-10-01T19:03:13Z</dc:date>
    </item>
  </channel>
</rss>