<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: Thread low power end device examples can't thr join?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Thread-low-power-end-device-examples-can-t-thr-join/m-p/794976#M5036</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Based on shell log ( Thread version - 1.1.1.18), seems to be the same problem with the one from this topic :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/479584"&gt;Thread low power end device examples can't thr join?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A new release including the fix for low power devices will be available at the end of July.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ovidiu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jul 2018 14:34:01 GMT</pubDate>
    <dc:creator>ovidiu_usturoi</dc:creator>
    <dc:date>2018-07-17T14:34:01Z</dc:date>
    <item>
      <title>Thread low power end device examples can't thr join?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Thread-low-power-end-device-examples-can-t-thr-join/m-p/794973#M5033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="vertical-align: inherit;"&gt;&lt;SPAN style="vertical-align: inherit;"&gt;我导入低功耗终端设备示例（FRDM-KW41Z），并将THREAD_USE_SHELL更改为1，这是文件./source/config.h中的宏定义。&lt;/SPAN&gt;&lt;SPAN style="vertical-align: inherit;"&gt;然后，我输入命令'thr join'到shell，但它打印'join failed'。&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65152i37132A10091523CA/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="vertical-align: inherit;"&gt;当我使用ED示例时，我成功加入。&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="vertical-align: inherit;"&gt;&lt;SPAN style="vertical-align: inherit;"&gt;因此，我用嗅探器观察。&lt;/SPAN&gt;&lt;SPAN style="vertical-align: inherit;"&gt;我发现两个例子的加入请求已经达成一致并且交换了密钥。&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="vertical-align: inherit;"&gt;为什么？&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jul 2018 07:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Thread-low-power-end-device-examples-can-t-thr-join/m-p/794973#M5033</guid>
      <dc:creator>yaoxingshan</dc:creator>
      <dc:date>2018-07-10T07:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: Thread low power end device examples can't thr join?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Thread-low-power-end-device-examples-can-t-thr-join/m-p/794974#M5034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which release and IDE are you using? Did you make any other change in the example?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By any chance, could you please reply in English?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Jul 2018 17:32:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Thread-low-power-end-device-examples-can-t-thr-join/m-p/794974#M5034</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2018-07-16T17:32:27Z</dc:date>
    </item>
    <item>
      <title>Re: Thread low power end device examples can't thr join?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Thread-low-power-end-device-examples-can-t-thr-join/m-p/794975#M5035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use&amp;nbsp;MCUXpresso IDE v10.1.1_606 and import the example(thread_low_power_end_device).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I changed the macro definition THREAD_USE_SHELL in the file config.h to 1.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Then I type the command ‘thr join’ in the shell, but it prints out ‘join failed’.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I uploaded two sniffing messages, one was successfully added and the other was added by the example.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 03:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Thread-low-power-end-device-examples-can-t-thr-join/m-p/794975#M5035</guid>
      <dc:creator>yaoxingshan</dc:creator>
      <dc:date>2018-07-17T03:28:00Z</dc:date>
    </item>
    <item>
      <title>Re: Thread low power end device examples can't thr join?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Thread-low-power-end-device-examples-can-t-thr-join/m-p/794976#M5036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Based on shell log ( Thread version - 1.1.1.18), seems to be the same problem with the one from this topic :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/479584"&gt;Thread low power end device examples can't thr join?&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;A new release including the fix for low power devices will be available at the end of July.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ovidiu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 14:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Thread-low-power-end-device-examples-can-t-thr-join/m-p/794976#M5036</guid>
      <dc:creator>ovidiu_usturoi</dc:creator>
      <dc:date>2018-07-17T14:34:01Z</dc:date>
    </item>
  </channel>
</rss>