<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: Dhcp internet connection problem via ethernet</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Dhcp-internet-connection-problem-via-ethernet/m-p/788544#M4940</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What part are you using ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 31 Jul 2018 17:33:55 GMT</pubDate>
    <dc:creator>stephanie_m</dc:creator>
    <dc:date>2018-07-31T17:33:55Z</dc:date>
    <item>
      <title>Dhcp internet connection problem via ethernet</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Dhcp-internet-connection-problem-via-ethernet/m-p/788543#M4939</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I boot, I have got below results&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Configuring network interfaces... fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready&lt;BR /&gt;eth0: adding address fe80::204:9fff:fe04:a712&lt;BR /&gt;eth0: waiting for carrier&lt;BR /&gt;fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx&lt;BR /&gt;IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready&lt;BR /&gt;eth0: carrier acquired&lt;BR /&gt;DUID 00:01:00:01:22:ec:83:f3:00:04:9f:04:a7:12&lt;BR /&gt;eth0: IAID 9f:04:a7:12&lt;BR /&gt;eth0: probing address 192.168.0.10/24&lt;BR /&gt;eth0: soliciting an IPv6 router&lt;BR /&gt;eth0: using static address 192.168.0.10/24&lt;BR /&gt;eth0: adding route to 192.168.0.0/24&lt;BR /&gt;eth0: adding default route via 192.168.0.1&lt;BR /&gt;forked to background, child pid 403&lt;BR /&gt;done.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Even I change dhcpcd.conf or interface ip configuration, it always goes to 192.168.0.1 default route.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone suggest me what do I have to do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 14:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Dhcp-internet-connection-problem-via-ethernet/m-p/788543#M4939</guid>
      <dc:creator>hkhunkim</dc:creator>
      <dc:date>2018-07-26T14:47:00Z</dc:date>
    </item>
    <item>
      <title>Re: Dhcp internet connection problem via ethernet</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Dhcp-internet-connection-problem-via-ethernet/m-p/788544#M4940</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What part are you using ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 17:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Dhcp-internet-connection-problem-via-ethernet/m-p/788544#M4940</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2018-07-31T17:33:55Z</dc:date>
    </item>
  </channel>
</rss>