<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: QN9021 cannot run application in RAM</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/QN9021-cannot-run-application-in-RAM/m-p/770280#M4700</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Leaf Lee,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a problem with newer versions of IAR. Some project options are not correctly imported but you can manually add them to your project as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Right click on your project &amp;gt; Options.&lt;/LI&gt;&lt;LI&gt;Debugger &amp;gt; Download.&lt;/LI&gt;&lt;LI&gt;Check&amp;nbsp;&lt;EM&gt;Override default .board file&lt;/EM&gt; and add "$TOOLKIT_DIR$\config\flashloader\NXP\FlashQN9020.board".&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11705iDC7884AA098D06DC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if this solves your issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 27 Apr 2018 00:31:01 GMT</pubDate>
    <dc:creator>gerardo_rodriguez</dc:creator>
    <dc:date>2018-04-27T00:31:01Z</dc:date>
    <item>
      <title>QN9021 cannot run application in RAM</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9021-cannot-run-application-in-RAM/m-p/770279#M4699</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am new to QN902x and BLE 4.0/4.1/4.2, now I develop a project of QN9021 on IAR ARM 8.11.3. &amp;nbsp;After I start debug by clicking the sub menu of "Project/Download and Debug". QN9021 doesn't run my application, just is stuck on the PC of 0x01002574 or 0x01002576, which is a ROM address, the content is 4 byte of 0xffffffff. And I think 0xffffffff should not be a instruction/instructions of CPU.&lt;/P&gt;&lt;P&gt;Is my application not downloaded into the chip of QN9021 by Jlink when clicking dubug? Either due to IAR setting, or hardware problem? &amp;nbsp;Any suggestions will be appreciated!&lt;/P&gt;&lt;P&gt;The IAR debug snapshot is attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Apr 2018 10:35:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9021-cannot-run-application-in-RAM/m-p/770279#M4699</guid>
      <dc:creator>leaflee</dc:creator>
      <dc:date>2018-04-26T10:35:35Z</dc:date>
    </item>
    <item>
      <title>Re: QN9021 cannot run application in RAM</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9021-cannot-run-application-in-RAM/m-p/770280#M4700</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Leaf Lee,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a problem with newer versions of IAR. Some project options are not correctly imported but you can manually add them to your project as below:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Right click on your project &amp;gt; Options.&lt;/LI&gt;&lt;LI&gt;Debugger &amp;gt; Download.&lt;/LI&gt;&lt;LI&gt;Check&amp;nbsp;&lt;EM&gt;Override default .board file&lt;/EM&gt; and add "$TOOLKIT_DIR$\config\flashloader\NXP\FlashQN9020.board".&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/11705iDC7884AA098D06DC/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if this solves your issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Apr 2018 00:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9021-cannot-run-application-in-RAM/m-p/770280#M4700</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2018-04-27T00:31:01Z</dc:date>
    </item>
    <item>
      <title>Re: QN9021 cannot run application in RAM</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9021-cannot-run-application-in-RAM/m-p/770281#M4701</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Gerardo,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Many thanks for your suggestion! &amp;nbsp;It is so helpful, it can solve some IAR debug problems. Besides that, my developing board had some HW problem, which contributed debug problem as well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 May 2018 01:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9021-cannot-run-application-in-RAM/m-p/770281#M4701</guid>
      <dc:creator>leaflee</dc:creator>
      <dc:date>2018-05-04T01:37:54Z</dc:date>
    </item>
  </channel>
</rss>