<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Look for a BlueTooth device -&amp;gt; CDC (SPP serial)</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764974#M4610</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is Nxp has a microcontroller solution with a code exemple which can do the&amp;nbsp; following function:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bluetooth device working on USB (Host or Device) CDC SPP serial client?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My aim is to have a serial link (Rx/Tx) like an RS232 but by Bluetooth way.&lt;/P&gt;&lt;P&gt;Then we can imagine two exactly small board which are connected between them (by air..) and as output has Rx line and Tx Line.&lt;/P&gt;&lt;P&gt;-All bytes sent on Tx line in a side will be received on the Rx line on the other side and reverse.&lt;/P&gt;&lt;P&gt;-We can also imagine have this small board on only one side, on in the other side it is a computer or a smartphone will emulate a serial port via the Bluetooth connection.&lt;/P&gt;&lt;P&gt;-And to have an evoluate device, we can imagine replace the serial Rx/Tx line by an USB port (in Host or device) in CDC mode...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then is Nxp has this kind of microcontroler to do this with a code exemple? (Better if there are a demo board...)&lt;/P&gt;&lt;P&gt;In other word, I would realize this kind of device:&lt;/P&gt;&lt;P&gt;&lt;A href="http://arpci.fr/adaptateur-bluetooth-usb/3404-adaptateur-bluetooth-usb-pour-le-remplacement-du-port-serie-bluetoot-3701007155195.html"&gt;http://arpci.fr/adaptateur-bluetooth-usb/3404-adaptateur-bluetooth-usb-pour-le-remplacement-du-port-serie-bluetoot-3701007155195.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Mar 2018 07:15:44 GMT</pubDate>
    <dc:creator>arnogir</dc:creator>
    <dc:date>2018-03-16T07:15:44Z</dc:date>
    <item>
      <title>Look for a BlueTooth device -&gt; CDC (SPP serial)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764974#M4610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is Nxp has a microcontroller solution with a code exemple which can do the&amp;nbsp; following function:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bluetooth device working on USB (Host or Device) CDC SPP serial client?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My aim is to have a serial link (Rx/Tx) like an RS232 but by Bluetooth way.&lt;/P&gt;&lt;P&gt;Then we can imagine two exactly small board which are connected between them (by air..) and as output has Rx line and Tx Line.&lt;/P&gt;&lt;P&gt;-All bytes sent on Tx line in a side will be received on the Rx line on the other side and reverse.&lt;/P&gt;&lt;P&gt;-We can also imagine have this small board on only one side, on in the other side it is a computer or a smartphone will emulate a serial port via the Bluetooth connection.&lt;/P&gt;&lt;P&gt;-And to have an evoluate device, we can imagine replace the serial Rx/Tx line by an USB port (in Host or device) in CDC mode...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then is Nxp has this kind of microcontroler to do this with a code exemple? (Better if there are a demo board...)&lt;/P&gt;&lt;P&gt;In other word, I would realize this kind of device:&lt;/P&gt;&lt;P&gt;&lt;A href="http://arpci.fr/adaptateur-bluetooth-usb/3404-adaptateur-bluetooth-usb-pour-le-remplacement-du-port-serie-bluetoot-3701007155195.html"&gt;http://arpci.fr/adaptateur-bluetooth-usb/3404-adaptateur-bluetooth-usb-pour-le-remplacement-du-port-serie-bluetoot-3701007155195.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 07:15:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764974#M4610</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2018-03-16T07:15:44Z</dc:date>
    </item>
    <item>
      <title>Re: Look for a BlueTooth device -&gt; CDC (SPP serial)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764975#M4611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Arnaud&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you can combine two demo project in QN908x to do this:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;C:\SDK\SDK_2.2_QN908XCDK\boards\qn908xcdk\wireless_examples\bluetooth\wireless_uart&lt;/P&gt;&lt;P&gt;2. C:\SDK\SDK_2.2_QN908XCDK\boards\qn908xcdk\usb_examples\usb_device_cdc_vcom&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please Contact local distributor&amp;nbsp;for demo&amp;nbsp;board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Mar 2018 02:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764975#M4611</guid>
      <dc:creator>neoxiong</dc:creator>
      <dc:date>2018-03-18T02:55:19Z</dc:date>
    </item>
    <item>
      <title>Re: Look for a BlueTooth device -&gt; CDC (SPP serial)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764976#M4612</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On which micro controler these demonstration are designed? Is it based on HCS08?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Mar 2018 07:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764976#M4612</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2018-03-19T07:00:31Z</dc:date>
    </item>
    <item>
      <title>Re: Look for a BlueTooth device -&gt; CDC (SPP serial)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764977#M4613</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Arnaud,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Serial Port Profile (SPP) is only supported in Bluetooth Classic, but a similar functionality can be achieved with the Wireless UART profile in Bluetooth Low Energy as Neo Xiong suggested.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition to the &lt;A href="https://www.nxp.com/products/wireless-connectivity/bluetooth-low-energy-ble/qn908x-ultra-low-power-ble-system-on-chip-solution:QN9080"&gt;QN908x&lt;/A&gt;, you can see more BLE devices in the&amp;nbsp;&lt;A href="https://www.nxp.com/products/wireless-connectivity/bluetooth-low-energy-ble:BLUETOOTH-LOW-ENERGY-BLE"&gt;Bluetooth Low Energy&lt;/A&gt;&amp;nbsp;product page.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Mar 2018 18:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764977#M4613</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2018-03-21T18:20:59Z</dc:date>
    </item>
    <item>
      <title>Re: Look for a BlueTooth device -&gt; CDC (SPP serial)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764978#M4614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I'm interested by Kinetis Chip (Because we know these family, we already designed system on K60 and K70 with MQX, then we have all tool...)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is some similar exemple for the K32, K35 etc...?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Mar 2018 07:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764978#M4614</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2018-03-22T07:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: Look for a BlueTooth device -&gt; CDC (SPP serial)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764979#M4615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arnaud,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are already familiar with Kinetis, I recommend you check out the &lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/kinetis-cortex-m-mcus/w-serieswireless-conn.m0-plus-m4:KINETIS_W_SERIES"&gt;Kinetis W series&lt;/A&gt;, specifically the &lt;A href="https://www.nxp.com/products/wireless-connectivity/zigbee/kinetis-kw41z-2.4-ghz-dual-mode-ble-and-802.15.4-wireless-radio-microcontroller-mcu-based-on-arm-cortex-m0-plus-core:KW41Z"&gt;KW41Z Family&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The BLE Wireless UART example is also available for these devices and can be found in the KW41 SDK. You can download the SDK from the &lt;A href="https://mcuxpresso.nxp.com/en/select"&gt;MCUXpresso SDK builder&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Mar 2018 17:54:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Look-for-a-BlueTooth-device-gt-CDC-SPP-serial/m-p/764979#M4615</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2018-03-23T17:54:45Z</dc:date>
    </item>
  </channel>
</rss>