<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LLWU ISR triggered from LLS3 without flags set in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/LLWU-ISR-triggered-from-LLS3-without-flags-set/m-p/759839#M4504</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a project built on the 802.15.4 MAC sensor FreeRTOS example for a KW41Z from the MCUXpresso SDK 2.2.0. I am noticing that occasionally the processor will wake from LLS3 almost immediately after going to sleep. I was able to trap the LLWU_ISR when this happens and all LLWU flags are 0 so I do not know what is trigger the wake and ISR.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the code I removed any pin sources and in this mode, only the LPTMR is a LLWU source. If I look at the LLWU registers at the start of the LLWU interrupt, all registers are 0 except LLWU-&amp;gt;ME is equal to 1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas what would cause this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Jan 2018 15:30:17 GMT</pubDate>
    <dc:creator>nick002025</dc:creator>
    <dc:date>2018-01-26T15:30:17Z</dc:date>
    <item>
      <title>LLWU ISR triggered from LLS3 without flags set</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/LLWU-ISR-triggered-from-LLS3-without-flags-set/m-p/759839#M4504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a project built on the 802.15.4 MAC sensor FreeRTOS example for a KW41Z from the MCUXpresso SDK 2.2.0. I am noticing that occasionally the processor will wake from LLS3 almost immediately after going to sleep. I was able to trap the LLWU_ISR when this happens and all LLWU flags are 0 so I do not know what is trigger the wake and ISR.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the code I removed any pin sources and in this mode, only the LPTMR is a LLWU source. If I look at the LLWU registers at the start of the LLWU interrupt, all registers are 0 except LLWU-&amp;gt;ME is equal to 1.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas what would cause this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jan 2018 15:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/LLWU-ISR-triggered-from-LLS3-without-flags-set/m-p/759839#M4504</guid>
      <dc:creator>nick002025</dc:creator>
      <dc:date>2018-01-26T15:30:17Z</dc:date>
    </item>
    <item>
      <title>Re: LLWU ISR triggered from LLS3 without flags set</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/LLWU-ISR-triggered-from-LLS3-without-flags-set/m-p/759840#M4505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;Nick McKendree,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I will try to reproduce this on my side so I can further investigate about this behavior. I'm suspecting that the device is not&amp;nbsp;entering LLS mode correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you share more information about&amp;nbsp;your project?&lt;/P&gt;&lt;P&gt;-Example application that you are using&lt;/P&gt;&lt;P&gt;-Code modifications made&lt;/P&gt;&lt;P&gt;-Steps to reproduce the problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Feb 2018 17:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/LLWU-ISR-triggered-from-LLS3-without-flags-set/m-p/759840#M4505</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2018-02-07T17:46:03Z</dc:date>
    </item>
  </channel>
</rss>