<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: QN908x Proprietary Radio Send Packet</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/QN908x-Proprietary-Radio-Send-Packet/m-p/750523#M4295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lukas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;A href="https://mcuxpresso.nxp.com/en/select"&gt;latest QN9080 SDK&lt;/A&gt; has an example for Generic FSK located at&amp;nbsp;&amp;lt;SDK&amp;gt;\boards\qn908xcdk\wireless_examples\genfsk\. You can use this application as a base for developing an application with a propietary protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Feb 2018 22:50:27 GMT</pubDate>
    <dc:creator>gerardo_rodriguez</dc:creator>
    <dc:date>2018-02-07T22:50:27Z</dc:date>
    <item>
      <title>QN908x Proprietary Radio Send Packet</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN908x-Proprietary-Radio-Send-Packet/m-p/750522#M4294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to send a packet in proprietary mode using the Q9080. I&amp;nbsp;tried implementing the&amp;nbsp;program flow chart for TX as described in the user manual (chapter 33.8.2&amp;nbsp;TX and RX flow).&lt;/P&gt;&lt;P&gt;I don't quite understand how output data can be send to the radio peripherals TX_BUF.&lt;/P&gt;&lt;P&gt;In the user manual it says that DMA requests are directly connected to the peripherals (12.5.1.1 DMA requests).&amp;nbsp;For DMA channel 10 we have a prop TX request input. However, reading through the radio chapter I was not able to find out where this prop TX request is made. I only found that there is a&amp;nbsp;TX request flag. Setting it to 1 did not seem to trigger a&amp;nbsp;&lt;SPAN&gt;prop TX DMA request.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Unfortunately there is no example in the SDK I looked at which shows how to configure the radio peripheral for use with proprietary&amp;nbsp;mode.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware&lt;BR /&gt;QN9080 DK-V1.2 R20161129&lt;/P&gt;&lt;P&gt;SDK&lt;/P&gt;&lt;P&gt;SDK_2.2_QN908xCDK_Beta&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Nov 2017 09:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN908x-Proprietary-Radio-Send-Packet/m-p/750522#M4294</guid>
      <dc:creator>lukaswidmer</dc:creator>
      <dc:date>2017-11-30T09:58:56Z</dc:date>
    </item>
    <item>
      <title>Re: QN908x Proprietary Radio Send Packet</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN908x-Proprietary-Radio-Send-Packet/m-p/750523#M4295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lukas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The &lt;A href="https://mcuxpresso.nxp.com/en/select"&gt;latest QN9080 SDK&lt;/A&gt; has an example for Generic FSK located at&amp;nbsp;&amp;lt;SDK&amp;gt;\boards\qn908xcdk\wireless_examples\genfsk\. You can use this application as a base for developing an application with a propietary protocol.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Feb 2018 22:50:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN908x-Proprietary-Radio-Send-Packet/m-p/750523#M4295</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2018-02-07T22:50:27Z</dc:date>
    </item>
  </channel>
</rss>