<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックHow can drivers and Framework middleware be used while programming in the same project to avoid hardware resource access conflicts?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/How-can-drivers-and-Framework-middleware-be-used-while/m-p/742455#M4182</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Wireless UART(freeRTOS) is a BLE demo application in the SDK_2.2_FRDM-KW41Z, this demo use the FreeRTOS, Framework&amp;nbsp; middleware and BLE protocol components, these will use KW41Z of hardware resources, such as TPM timer, PIT timer, etc.I need to add the high speed ADC control during normal BLE and serial communication in this demo, and I need to directly operate the PIT and TPM timer in KW41Z through drivers (the timer in TimersManager is too slow).&lt;/P&gt;&lt;P&gt;My question is how do I avoid the PIT and TPM timers used in drivers that don't conflict with the middleware TimersManager and bluetooth protocol?Are there any middleware instructions?How can drivers and Framework middleware be used while programming in the same project to avoid hardware resource access conflicts?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 21 Jan 2018 06:28:17 GMT</pubDate>
    <dc:creator>bjemt</dc:creator>
    <dc:date>2018-01-21T06:28:17Z</dc:date>
    <item>
      <title>How can drivers and Framework middleware be used while programming in the same project to avoid hardware resource access conflicts?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/How-can-drivers-and-Framework-middleware-be-used-while/m-p/742455#M4182</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Wireless UART(freeRTOS) is a BLE demo application in the SDK_2.2_FRDM-KW41Z, this demo use the FreeRTOS, Framework&amp;nbsp; middleware and BLE protocol components, these will use KW41Z of hardware resources, such as TPM timer, PIT timer, etc.I need to add the high speed ADC control during normal BLE and serial communication in this demo, and I need to directly operate the PIT and TPM timer in KW41Z through drivers (the timer in TimersManager is too slow).&lt;/P&gt;&lt;P&gt;My question is how do I avoid the PIT and TPM timers used in drivers that don't conflict with the middleware TimersManager and bluetooth protocol?Are there any middleware instructions?How can drivers and Framework middleware be used while programming in the same project to avoid hardware resource access conflicts?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 21 Jan 2018 06:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/How-can-drivers-and-Framework-middleware-be-used-while/m-p/742455#M4182</guid>
      <dc:creator>bjemt</dc:creator>
      <dc:date>2018-01-21T06:28:17Z</dc:date>
    </item>
    <item>
      <title>Re: How can drivers and Framework middleware be used while programming in the same project to avoid hardware resource access conflicts?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/How-can-drivers-and-Framework-middleware-be-used-while/m-p/742456#M4183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although I knew that FreeRTOS and these middleware were designed to be independent of hardware, but the program had to run on a hardware platform.FreeRTOS and these middleware have the user interface for developers, there is also a hardware interface to the hardware. How should I view these hardware interface definitions in SDK_2.2_FRDM-KW41Z？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jan 2018 07:10:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/How-can-drivers-and-Framework-middleware-be-used-while/m-p/742456#M4183</guid>
      <dc:creator>bjemt</dc:creator>
      <dc:date>2018-01-22T07:10:43Z</dc:date>
    </item>
    <item>
      <title>Re: How can drivers and Framework middleware be used while programming in the same project to avoid hardware resource access conflicts?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/How-can-drivers-and-Framework-middleware-be-used-while/m-p/742457#M4184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello limin Jia,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As long as you don't use the same timer instance as the framework you should have no problems. For example, the BLE wireless UART uses the TPM1, indicated by&amp;nbsp;&lt;EM&gt;gStackTimerInstance_c&amp;nbsp;&lt;/EM&gt;defined in &lt;EM&gt;board.h&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PIT timer is not used unless the timestamp service is used (gTimestamp_Enabled_d).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Feb 2018 00:23:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/How-can-drivers-and-Framework-middleware-be-used-while/m-p/742457#M4184</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2018-02-07T00:23:42Z</dc:date>
    </item>
  </channel>
</rss>