<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic JN5179 in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5179/m-p/705859#M3610</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;To put the module into UART programming mode, tie MISO to 0 V while releasing&lt;BR /&gt;RESET. This causes the device to read zeros back from the Flash memory during&lt;BR /&gt;initialization and, as a result, to enter programming mode. If you are using the module in&lt;BR /&gt;conjunction with a serial interface then the signal PGM is available to put the device into&lt;BR /&gt;programming mode. To allow this signal to operate correctly from the Flash programming&lt;BR /&gt;software.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;What is the signal PGM?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 16 Sep 2017 12:00:47 GMT</pubDate>
    <dc:creator>wupengfei</dc:creator>
    <dc:date>2017-09-16T12:00:47Z</dc:date>
    <item>
      <title>JN5179</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5179/m-p/705859#M3610</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class=""&gt;To put the module into UART programming mode, tie MISO to 0 V while releasing&lt;BR /&gt;RESET. This causes the device to read zeros back from the Flash memory during&lt;BR /&gt;initialization and, as a result, to enter programming mode. If you are using the module in&lt;BR /&gt;conjunction with a serial interface then the signal PGM is available to put the device into&lt;BR /&gt;programming mode. To allow this signal to operate correctly from the Flash programming&lt;BR /&gt;software.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;What is the signal PGM?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 16 Sep 2017 12:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5179/m-p/705859#M3610</guid>
      <dc:creator>wupengfei</dc:creator>
      <dc:date>2017-09-16T12:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: JN5179</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5179/m-p/705860#M3611</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/wupengfei"&gt;wupengfei&lt;/A&gt;‌&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I believe that's is the way to enter programming mode&amp;nbsp;&lt;BR /&gt;&lt;A href="https://community.nxp.com/thread/460072"&gt;https://community.nxp.com/thread/460072&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Sep 2017 08:45:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5179/m-p/705860#M3611</guid>
      <dc:creator>davidashraf</dc:creator>
      <dc:date>2017-09-22T08:45:07Z</dc:date>
    </item>
  </channel>
</rss>