<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックInverted-F antenna design</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Inverted-F-antenna-design/m-p/701084#M3519</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was checking the MC1320xRFCUG document and saw that the SMA port is attached to the open side of the inverted-F antenna. Since the antenna design needs very careful steps, two questions arise:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Was that done intentionally? I mean is it claimed&amp;nbsp;that the open side of the antenna is free to be used?&lt;/P&gt;&lt;P&gt;- Is it also OK to place the SMA to the close side of the antenna (ground side)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 17 Aug 2017 19:02:43 GMT</pubDate>
    <dc:creator>yavuzyaman</dc:creator>
    <dc:date>2017-08-17T19:02:43Z</dc:date>
    <item>
      <title>Inverted-F antenna design</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Inverted-F-antenna-design/m-p/701084#M3519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was checking the MC1320xRFCUG document and saw that the SMA port is attached to the open side of the inverted-F antenna. Since the antenna design needs very careful steps, two questions arise:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Was that done intentionally? I mean is it claimed&amp;nbsp;that the open side of the antenna is free to be used?&lt;/P&gt;&lt;P&gt;- Is it also OK to place the SMA to the close side of the antenna (ground side)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Aug 2017 19:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Inverted-F-antenna-design/m-p/701084#M3519</guid>
      <dc:creator>yavuzyaman</dc:creator>
      <dc:date>2017-08-17T19:02:43Z</dc:date>
    </item>
    <item>
      <title>Re: Inverted-F antenna design</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Inverted-F-antenna-design/m-p/701085#M3520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MC1320x is not recommended for new designs. You can check out our &lt;A href="http://www.nxp.com/products/microcontrollers-and-processors/more-processors/application-specific-mcus-mpus/ieee-802.15.4-wireless-mcus:IEEE-802.15.4"&gt;IEEE®&amp;nbsp;802.15.4-based Wireless MCUs - 2.4 GHz Solutions&lt;/A&gt;&amp;nbsp;for a list of our latest products.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About your question on the SMA connector, yes, it is ok to place it like that. Note that there is a 0 ohm resistor to select the inverted F-antenna or the SMA connector. You can use that design as reference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more information on the antennas and RF circuit, you can refer to:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN2731.pdf?&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;Compact Integrated Antennas&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="http://www.nxp.com/docs/en/reference-manual/ZHDCRM.pdf?&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;Freescale IEEE 802.15.4 / ZigBee&amp;nbsp;Package and Hardware Layout&amp;nbsp;Considerations&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN5377.pdf"&gt;Hardware Design Considerations for MKW41Z/31Z/21Z BLE and IEEE 802.15.4 Devices&lt;/A&gt;&lt;/LI&gt;&lt;LI&gt;&lt;A href="http://www.nxp.com/docs/en/application-note/AN4957.pdf"&gt;Hardware Design Considerations for MKW2x IEEE 802.15.4 Devices&lt;/A&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Aug 2017 22:23:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Inverted-F-antenna-design/m-p/701085#M3520</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2017-08-21T22:23:25Z</dc:date>
    </item>
  </channel>
</rss>