<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: NXP jennet IP LAN/WAN</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/NXP-jennet-IP-LAN-WAN/m-p/695806#M3419</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LAN in a JenNet-IP system connects together the WPANs of the system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The LAN may also provide a connection to a WAN, such as the Internet (and this WAN may provide connections to other JenNet-IP systems consisting of a LAN and associated WPANs. So,Messages are sent between the wireless nodes of a JenNet-IP system as IPv6 packets which are compressed and embedded in IEEE 802.15.4 frames.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: As you know, the support for the JenNet-IP stack is limited.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Sep 2017 21:41:28 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2017-09-11T21:41:28Z</dc:date>
    <item>
      <title>NXP jennet IP LAN/WAN</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NXP-jennet-IP-LAN-WAN/m-p/695805#M3418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Support Team&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;STRONG&gt;ZigbeeNodeControlBridge/Source/ZigbeeNodeControlBridge in JN5168 as&lt;/STRONG&gt; Control Bridge connected to&lt;STRONG&gt;linux based PC&amp;nbsp;&lt;/STRONG&gt; via UART serial port&lt;/P&gt;&lt;P&gt;/*******************************************************************************************************************/&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Below things will be running in linux based PC&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;ZigbeeNodeControlBridge/Source/Host/zigbee-jip-daemon/JIP/Build &amp;nbsp; =&amp;gt; &lt;STRONG&gt;zigbee daemon &amp;nbsp;will be running in one terminal&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Host/ZigbeeNodeControlBridge/Source/Host/libJIP/Build &amp;nbsp;&lt;STRONG&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; =&amp;gt; jip will be running in another terminal window&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;/********************************************************************************************************************/&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;i &amp;nbsp;am able to run daemon and connect to Available ZIGBEE nodes and get data and notification,&amp;nbsp;&lt;/P&gt;&lt;P&gt;consider another PC connected to Gateway via LAN&lt;/P&gt;&lt;P&gt;As per jennet ip documents i will be able to control or read / write data to ZIGBEE node from another PC connected to gateway via LAN&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this scenerio i tried running &amp;nbsp;zigbee_daemon in GATEWAY PC&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; jip client will be running in Another PC where i want to do the read/write (./JIP -6 "GATEWAY_PC_IPV6") , will i be able to do this way ??&lt;/P&gt;&lt;P&gt;please provide some information that clarifies above scenario...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Sep 2017 13:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NXP-jennet-IP-LAN-WAN/m-p/695805#M3418</guid>
      <dc:creator>prasanthv</dc:creator>
      <dc:date>2017-09-06T13:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: NXP jennet IP LAN/WAN</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NXP-jennet-IP-LAN-WAN/m-p/695806#M3419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The LAN in a JenNet-IP system connects together the WPANs of the system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;The LAN may also provide a connection to a WAN, such as the Internet (and this WAN may provide connections to other JenNet-IP systems consisting of a LAN and associated WPANs. So,Messages are sent between the wireless nodes of a JenNet-IP system as IPv6 packets which are compressed and embedded in IEEE 802.15.4 frames.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: As you know, the support for the JenNet-IP stack is limited.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Sep 2017 21:41:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NXP-jennet-IP-LAN-WAN/m-p/695806#M3419</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2017-09-11T21:41:28Z</dc:date>
    </item>
  </channel>
</rss>