<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックMKW22 Internal reference voltage</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/MKW22-Internal-reference-voltage/m-p/389369#M334</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have this question.&lt;/P&gt;&lt;P&gt;In the MKW2xDxxx reference manual, says that there is a internal reference voltaje of 1.22V that can be used as reference for analog peripheral, with the ADCx_SC2 register we can select the reference in the bits REFSEL. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;EM&gt;01 Alternate reference pair, that is, VALTH and V ALTL. This pair may be additional external pins or internal sources depending on the MCU configuration. See the chip configuration information for details specific to this MCU.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;But in the datasheet of the MKW22 I do not see any reference to it... (perhaps I am missing something?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I am working with a custom board that uses the KW22D512 and we were couting into use this internal reference voltaje for the ADC, is there a way to use connecting it internally?, we do not have available neither the VrefH and VrefL in the custom board. (or at less in this revision).&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Apr 2015 02:15:39 GMT</pubDate>
    <dc:creator>luisluna</dc:creator>
    <dc:date>2015-04-09T02:15:39Z</dc:date>
    <item>
      <title>MKW22 Internal reference voltage</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MKW22-Internal-reference-voltage/m-p/389369#M334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have this question.&lt;/P&gt;&lt;P&gt;In the MKW2xDxxx reference manual, says that there is a internal reference voltaje of 1.22V that can be used as reference for analog peripheral, with the ADCx_SC2 register we can select the reference in the bits REFSEL. &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;EM&gt;01 Alternate reference pair, that is, VALTH and V ALTL. This pair may be additional external pins or internal sources depending on the MCU configuration. See the chip configuration information for details specific to this MCU.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;But in the datasheet of the MKW22 I do not see any reference to it... (perhaps I am missing something?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I am working with a custom board that uses the KW22D512 and we were couting into use this internal reference voltaje for the ADC, is there a way to use connecting it internally?, we do not have available neither the VrefH and VrefL in the custom board. (or at less in this revision).&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2015 02:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MKW22-Internal-reference-voltage/m-p/389369#M334</guid>
      <dc:creator>luisluna</dc:creator>
      <dc:date>2015-04-09T02:15:39Z</dc:date>
    </item>
    <item>
      <title>Re: MKW22 Internal reference voltage</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MKW22-Internal-reference-voltage/m-p/389370#M335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Dear Luis,&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;It seems the VREFOUT and therefore the internal reference voltage mentioned (VALTH, VALTL) are not available in KW2x package at all. This should be removed from Reference Manual shortly.&amp;nbsp; Sorry for the inconvenience this might have caused.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;AngelC&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Apr 2015 20:53:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MKW22-Internal-reference-voltage/m-p/389370#M335</guid>
      <dc:creator>AngelC</dc:creator>
      <dc:date>2015-04-16T20:53:59Z</dc:date>
    </item>
  </channel>
</rss>