<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Temperature sensor/collector example on FRDM-KW41ZJ not working in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Temperature-sensor-collector-example-on-FRDM-KW41ZJ-not-working/m-p/686857#M3233</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;BR /&gt;I'm trying to run the temperature sensor/collector example provided by NXP on 2 FRDM-KW41ZJ boards. However, when I tried to flash and debug the examples using MCUXpresso, both programs just pause at the breakpoints at OSA_init() function, after resuming,&amp;nbsp;LED3 is not on as described. Additionally, when SW4 is pressed, nothing happens. On the debugger there is also no indication of any error.&lt;BR /&gt;I then tried to run these examples using KDS. With KDS, both programs showed 'No source available for "0x0"' after resuming from&amp;nbsp;&lt;SPAN&gt;OSA_init() function.&lt;BR /&gt;I tried running other examples from the FRDM board and they all seem to work fine except these two. Any help would be very appreciated.&lt;BR /&gt;&lt;BR /&gt;Kind regards,&lt;BR /&gt;Khanh Huynh&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Jul 2017 16:18:58 GMT</pubDate>
    <dc:creator>khanh_huynh</dc:creator>
    <dc:date>2017-07-06T16:18:58Z</dc:date>
    <item>
      <title>Temperature sensor/collector example on FRDM-KW41ZJ not working</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Temperature-sensor-collector-example-on-FRDM-KW41ZJ-not-working/m-p/686857#M3233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;BR /&gt;I'm trying to run the temperature sensor/collector example provided by NXP on 2 FRDM-KW41ZJ boards. However, when I tried to flash and debug the examples using MCUXpresso, both programs just pause at the breakpoints at OSA_init() function, after resuming,&amp;nbsp;LED3 is not on as described. Additionally, when SW4 is pressed, nothing happens. On the debugger there is also no indication of any error.&lt;BR /&gt;I then tried to run these examples using KDS. With KDS, both programs showed 'No source available for "0x0"' after resuming from&amp;nbsp;&lt;SPAN&gt;OSA_init() function.&lt;BR /&gt;I tried running other examples from the FRDM board and they all seem to work fine except these two. Any help would be very appreciated.&lt;BR /&gt;&lt;BR /&gt;Kind regards,&lt;BR /&gt;Khanh Huynh&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jul 2017 16:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Temperature-sensor-collector-example-on-FRDM-KW41ZJ-not-working/m-p/686857#M3233</guid>
      <dc:creator>khanh_huynh</dc:creator>
      <dc:date>2017-07-06T16:18:58Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature sensor/collector example on FRDM-KW41ZJ not working</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Temperature-sensor-collector-example-on-FRDM-KW41ZJ-not-working/m-p/686858#M3234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;BR /&gt;Not sure about MCUXpresso, but according to what you describe in KSD, the issue might be that you have low power mode enabled. That way after flashing the debugger disconnects. And also LEDs are not used in this mode. My suggestion is to disable&amp;nbsp;cPWR_UsePowerDownMode in app_preinclude.h and test if it is any different.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 12:21:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Temperature-sensor-collector-example-on-FRDM-KW41ZJ-not-working/m-p/686858#M3234</guid>
      <dc:creator>danielkresta</dc:creator>
      <dc:date>2017-07-07T12:21:43Z</dc:date>
    </item>
    <item>
      <title>Re: Temperature sensor/collector example on FRDM-KW41ZJ not working</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Temperature-sensor-collector-example-on-FRDM-KW41ZJ-not-working/m-p/686859#M3235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Daniel.&lt;BR /&gt;I tried disabling&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;cPWR_UsePowerDownMode in both programs and now they are working!&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Khanh&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Jul 2017 13:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Temperature-sensor-collector-example-on-FRDM-KW41ZJ-not-working/m-p/686859#M3235</guid>
      <dc:creator>khanh_huynh</dc:creator>
      <dc:date>2017-07-07T13:56:45Z</dc:date>
    </item>
  </channel>
</rss>