<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Listen to more than one udp socket in Thread Network with KW41Z in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Listen-to-more-than-one-udp-socket-in-Thread-Network-with-KW41Z/m-p/686263#M3223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;im using the FREEDOM-KW41Z with the frdmkw41z_wireless_examples_thread_router_eligible_device_freertos Example and UDP Sockets, which are enabled with the&amp;nbsp;SOCK_DEMO macro . My Question is, how can I listen to more than one udp-Socket-Port at the same time? I need this to install a unicast and multicast part. If I'm right, i just can open different ports on the site of the Sender, but can not configure on the Receiver site, to which ports he should listen to? I'm very thankfull for Suggestions how to install this functionality. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has no one an Idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Jul 2017 07:12:47 GMT</pubDate>
    <dc:creator>steffenjahnkepa</dc:creator>
    <dc:date>2017-07-28T07:12:47Z</dc:date>
    <item>
      <title>Listen to more than one udp socket in Thread Network with KW41Z</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Listen-to-more-than-one-udp-socket-in-Thread-Network-with-KW41Z/m-p/686263#M3223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;im using the FREEDOM-KW41Z with the frdmkw41z_wireless_examples_thread_router_eligible_device_freertos Example and UDP Sockets, which are enabled with the&amp;nbsp;SOCK_DEMO macro . My Question is, how can I listen to more than one udp-Socket-Port at the same time? I need this to install a unicast and multicast part. If I'm right, i just can open different ports on the site of the Sender, but can not configure on the Receiver site, to which ports he should listen to? I'm very thankfull for Suggestions how to install this functionality. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has no one an Idea?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2017 07:12:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Listen-to-more-than-one-udp-socket-in-Thread-Network-with-KW41Z/m-p/686263#M3223</guid>
      <dc:creator>steffenjahnkepa</dc:creator>
      <dc:date>2017-07-28T07:12:47Z</dc:date>
    </item>
    <item>
      <title>Re: Listen to more than one udp socket in Thread Network with KW41Z</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Listen-to-more-than-one-udp-socket-in-Thread-Network-with-KW41Z/m-p/686264#M3224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to hear more than one UDP port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By default the demo will create and bind a socket to the port 1234 you will need to create and bind to another port (available in the range) as it is done with the first one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To do so you will need to open the app_socket_utils.c file and add the next modifications&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="comment token"&gt;/* Server sockets */&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; int32_t mSockfd &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;static&lt;/SPAN&gt; int32_t mSockfdNewCustom &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;SPAN style="color: windowtext; font-size: 9.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt; &lt;SPAN class="comment token"&gt;/* Socket storage information used for RX */&lt;/SPAN&gt;
sockaddrIn6_t mSsRx &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
sockaddrIn6_t mSsRxNewCustom &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;SPAN style="color: windowtext; font-size: 9.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="comment token"&gt;////////////////First socket/////////////////&lt;/SPAN&gt;
 &lt;SPAN class="comment token"&gt;/* Create a socket for global IP address */&lt;/SPAN&gt;
 &lt;SPAN class="comment token"&gt;/* Set local information */&lt;/SPAN&gt;
mSsRx&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sin6_family &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; AF_INET6&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
mSsRx&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sin6_port &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; UDP_PORT&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;IP_AddrCopy&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;mSsRx&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sin6_addr&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;in6addr_any&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Create socket */&lt;/SPAN&gt;
mSockfd &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;socket&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;mSsRx&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sin6_family&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; SOCK_DGRAM&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; IPPROTO_UDP&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="comment token"&gt;/* Bind socket to local information */&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;bind&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;mSockfd&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;sockaddrStorage_t&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;mSsRx&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;sockaddrStorage_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

 &lt;SPAN class="comment token"&gt;////////////////Second socket///////////////// &lt;/SPAN&gt;
 mSsRxNewCustom&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sin6_family &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; AF_INET6&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 mSsRxNewCustom&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sin6_port &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;8080&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//Choose a port in the correct range&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;IP_AddrCopy&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;mSsRxNewCustom&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sin6_addr&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;in6addr_any&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="comment token"&gt;/* Create socket */&lt;/SPAN&gt;
 mSockfdNewCustom &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;socket&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;mSsRxNewCustom&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;sin6_family&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; SOCK_DGRAM&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; IPPROTO_UDP&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
 &lt;SPAN class="comment token"&gt;/* Bind socket to local information */&lt;/SPAN&gt;
 &lt;SPAN class="token function"&gt;bind&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;mSockfdNewCustom&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;sockaddrStorage_t&lt;SPAN class="operator token"&gt;*&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;mSsRxNewCustom&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;sockaddrStorage_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="font-size: 9.0pt;"&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Also you will need to check the following functions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;void APP_InitUserSockets&lt;/LI&gt;&lt;LI&gt;static void APP_InitSocketServer&lt;SPAN style="font-size: 9.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Estephania&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 04:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Listen-to-more-than-one-udp-socket-in-Thread-Network-with-KW41Z/m-p/686264#M3224</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2017-08-09T04:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: Listen to more than one udp socket in Thread Network with KW41Z</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Listen-to-more-than-one-udp-socket-in-Thread-Network-with-KW41Z/m-p/686265#M3225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Estephania,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot! This works fine!&lt;/P&gt;&lt;P&gt;After your Explanation i wonder why i didn't try that before. :smileywink:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Steffen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Aug 2017 13:42:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Listen-to-more-than-one-udp-socket-in-Thread-Network-with-KW41Z/m-p/686265#M3225</guid>
      <dc:creator>steffenjahnkepa</dc:creator>
      <dc:date>2017-08-09T13:42:39Z</dc:date>
    </item>
  </channel>
</rss>