<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 MC33814</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/MC33814/m-p/676854#M3069</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;SPAN style="color: #000000; font-size: medium; font-family: 新細明體;"&gt;I&amp;nbsp;would like to&amp;nbsp;check if the inputs on the MC33814 can be connected directly to the outputs from a 3.3v MCU without using a level shifter? We are using a 5V buffer at the moment because we do not want to risk it.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Jul 2017 06:41:36 GMT</pubDate>
    <dc:creator>berniecheah</dc:creator>
    <dc:date>2017-07-20T06:41:36Z</dc:date>
    <item>
      <title>MC33814</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MC33814/m-p/676854#M3069</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="margin: 0cm 0cm 0pt;"&gt;&lt;SPAN style="color: #000000; font-size: medium; font-family: 新細明體;"&gt;I&amp;nbsp;would like to&amp;nbsp;check if the inputs on the MC33814 can be connected directly to the outputs from a 3.3v MCU without using a level shifter? We are using a 5V buffer at the moment because we do not want to risk it.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 06:41:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MC33814/m-p/676854#M3069</guid>
      <dc:creator>berniecheah</dc:creator>
      <dc:date>2017-07-20T06:41:36Z</dc:date>
    </item>
    <item>
      <title>Re: MC33814</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MC33814/m-p/676855#M3070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I’m afraid that it is not possible to connect the inputs on the MC33814 can be connected directly to the outputs from a 3.3v MCU without using a level shifter, the reason is that the Digital interface input of the MC33814 is dependent from VCC voltage and VCC voltage should be 5V. Using a level shifter is the best solution for this case. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Jul 2017 21:22:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MC33814/m-p/676855#M3070</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2017-07-25T21:22:13Z</dc:date>
    </item>
  </channel>
</rss>