<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic UART usage in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/UART-usage/m-p/674003#M3019</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to communicate with another uC using UART. My application is based on thread_router_bluetooth_wireless_uart_hybrid example. Should I use SerialManager or FSCI module from Wireless Connectivity Framework? Any example?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Jun 2017 11:33:01 GMT</pubDate>
    <dc:creator>lukaszgesieniec</dc:creator>
    <dc:date>2017-06-26T11:33:01Z</dc:date>
    <item>
      <title>UART usage</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/UART-usage/m-p/674003#M3019</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to communicate with another uC using UART. My application is based on thread_router_bluetooth_wireless_uart_hybrid example. Should I use SerialManager or FSCI module from Wireless Connectivity Framework? Any example?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 11:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/UART-usage/m-p/674003#M3019</guid>
      <dc:creator>lukaszgesieniec</dc:creator>
      <dc:date>2017-06-26T11:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: UART usage</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/UART-usage/m-p/674004#M3020</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lukasz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The serial manager is used for communication to the upper layers in the stack. For most thread examples, the serial manager is user by the shell interface and communicates through UART to the OpenSDA MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the KW41 only has one UART, you would need to disable the serial manager to have access to the UART. Once disabled, you can use the SDK drivers for the UART module. There are examples for this driver located in &lt;EM&gt;&amp;lt;SDK installation&amp;gt;\boards\frdmkw41z\driver_examples\lpuart\.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FSCI is a serial protocol used to control the Connectivity stack through serial commands.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jul 2017 19:59:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/UART-usage/m-p/674004#M3020</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2017-07-14T19:59:57Z</dc:date>
    </item>
  </channel>
</rss>