<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックAbout Z3.0 Join the network:</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/About-Z3-0-Join-the-network/m-p/673262#M3001</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;BR /&gt;&lt;SPAN&gt;I have two devices, a coordinator, an end node, can be successful, but when I re-programmed the node again (the EEPROM erase), the node can not join the coordinator, the coordinator must also erase&lt;/SPAN&gt; &lt;SPAN class=""&gt;Once the EEPROM, the terminal node can join the coordinator again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Know why?&lt;/SPAN&gt; &lt;SPAN class=""&gt;Help me think about it&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;If a MAC address of 01 equipment to join a coordinator,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;And then erase the EEPROM with the MAC address 01 device&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;MAC address of 01 this device to join the coordinator again, the network can not be successful.&lt;/SPAN&gt; &lt;SPAN&gt;The&lt;/SPAN&gt; &lt;SPAN&gt;The&lt;/SPAN&gt; &lt;SPAN class=""&gt;Why is this the case?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 26 Jun 2017 07:34:21 GMT</pubDate>
    <dc:creator>liuxiang</dc:creator>
    <dc:date>2017-06-26T07:34:21Z</dc:date>
    <item>
      <title>About Z3.0 Join the network:</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/About-Z3-0-Join-the-network/m-p/673262#M3001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="" lang="en"&gt;&lt;BR /&gt;&lt;SPAN&gt;I have two devices, a coordinator, an end node, can be successful, but when I re-programmed the node again (the EEPROM erase), the node can not join the coordinator, the coordinator must also erase&lt;/SPAN&gt; &lt;SPAN class=""&gt;Once the EEPROM, the terminal node can join the coordinator again.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;Know why?&lt;/SPAN&gt; &lt;SPAN class=""&gt;Help me think about it&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;If a MAC address of 01 equipment to join a coordinator,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;And then erase the EEPROM with the MAC address 01 device&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;MAC address of 01 this device to join the coordinator again, the network can not be successful.&lt;/SPAN&gt; &lt;SPAN&gt;The&lt;/SPAN&gt; &lt;SPAN&gt;The&lt;/SPAN&gt; &lt;SPAN class=""&gt;Why is this the case?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jun 2017 07:34:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/About-Z3-0-Join-the-network/m-p/673262#M3001</guid>
      <dc:creator>liuxiang</dc:creator>
      <dc:date>2017-06-26T07:34:21Z</dc:date>
    </item>
  </channel>
</rss>