<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328535#M3</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AngelCI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for the reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried this with multiple setups. There has been from 2 to 15 devices on the network. The number of devices does not seem affect to the timing of the problem. It occurs always after running for 4 hours 45 minutes.&lt;BR /&gt;Device are battery powered thermostat and they are polling (sending Data requests ) the coordinator for every 2 seconds. I haven't try changing the polling time, but I doubt it will have any significance. If it would be related to the quantify of message, I would assume that also number of devices would matter, don't you think?&lt;/P&gt;&lt;P&gt;During this blackout coordinator does not respond any messages, though it will transmit messages if it has any. For example Link status messages and commands sent through ZTC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;Teemu Avellan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 Dec 2014 08:25:49 GMT</pubDate>
    <dc:creator>teemuavellan</dc:creator>
    <dc:date>2014-12-12T08:25:49Z</dc:date>
    <item>
      <title>Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328533#M1</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have run into problems when I upgraded your HA coordinator's firmware to use Codebase 3.1.1. It causes the coordinator to go "deaf" for about 5 minutes in every 4 hour and 45 minutes.&lt;/P&gt;&lt;P&gt;It's very strange problem because it will occur exactly on clock every time. It does either not hear messages sent to it or ignores them completely during blackout. I used sniffer to see that messages are sent but there's no MAC-ACK. Ztc interface "normally" during blackout, and the chip give responses to commands, also it will send messages e.g link status.&lt;/P&gt;&lt;P&gt;This is not an application caused problem because I tested this also "vanilla" build, creating a sample coordinator with HA combined interface -template from Beekit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This problem does not occur with older 3.0.11 codebase.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Teemu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Dec 2014 14:28:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328533#M1</guid>
      <dc:creator>teemuavellan</dc:creator>
      <dc:date>2014-12-05T14:28:13Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328534#M2</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Dear Teemu,&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Please provide further details about the application itself and how to trigger the problem. In other words:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;How many devices are on the network? &lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;How often are messages sent to coordinator? &lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;Is coordinator sending any response back? &lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="color: #1f497d;"&gt;Also, if you modify the transmission’s period, is the problem appearing at a different time or exactly the same?&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;This will help us to have a better context of the problem and find a possible root cause. I will be looking forward to your reply. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;AngelC&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Dec 2014 19:19:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328534#M2</guid>
      <dc:creator>AngelC</dc:creator>
      <dc:date>2014-12-11T19:19:25Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328535#M3</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi AngelCI,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for the reply!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried this with multiple setups. There has been from 2 to 15 devices on the network. The number of devices does not seem affect to the timing of the problem. It occurs always after running for 4 hours 45 minutes.&lt;BR /&gt;Device are battery powered thermostat and they are polling (sending Data requests ) the coordinator for every 2 seconds. I haven't try changing the polling time, but I doubt it will have any significance. If it would be related to the quantify of message, I would assume that also number of devices would matter, don't you think?&lt;/P&gt;&lt;P&gt;During this blackout coordinator does not respond any messages, though it will transmit messages if it has any. For example Link status messages and commands sent through ZTC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;Teemu Avellan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Dec 2014 08:25:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328535#M3</guid>
      <dc:creator>teemuavellan</dc:creator>
      <dc:date>2014-12-12T08:25:49Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328536#M4</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I tried with only one thermostat on the network and changed polling time to 1 second. No change, still the coordinator stop listening after 4:45. Here's a sniffer capture log of the situation:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48341i7CC08978115FEF9C/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Br,&lt;/P&gt;&lt;P&gt;Teemu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2014 08:07:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328536#M4</guid>
      <dc:creator>teemuavellan</dc:creator>
      <dc:date>2014-12-16T08:07:43Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328537#M5</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, any progress on this case?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Br,&lt;/P&gt;&lt;P&gt;Teemu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 09:21:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328537#M5</guid>
      <dc:creator>teemuavellan</dc:creator>
      <dc:date>2015-01-07T09:21:33Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328538#M6</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to reproduce the problem that &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/teemuavellan"&gt;teemuavellan&lt;/A&gt; found. I sent results to SW team including memory dumps, sniffer LOGs, source code, and other deeper analysis. &lt;/P&gt;&lt;P&gt;I will report the outcome as soon as I get a resolution from SW team. Thank you in advance for your patience. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 23:36:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328538#M6</guid>
      <dc:creator>AlanCollins</dc:creator>
      <dc:date>2015-01-07T23:36:30Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328539#M7</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is great news. Thank you, Alan!&lt;/P&gt;&lt;P&gt;Looking forward for the resolution.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Br, Teemu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jan 2015 10:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328539#M7</guid>
      <dc:creator>teemuavellan</dc:creator>
      <dc:date>2015-01-08T10:38:57Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328540#M8</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alan,&lt;/P&gt;&lt;P&gt;any news on this? I know these things are hard to estimate, but could I get some kind of time frame when this could be solved?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Teemu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 13:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328540#M8</guid>
      <dc:creator>teemuavellan</dc:creator>
      <dc:date>2015-01-29T13:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328541#M9</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/teemuavellan"&gt;teemuavellan&lt;/A&gt;, As you know MC1322x is on "end of life", so all support related to this part is very limited today. Please be patience about a resolution. &lt;/P&gt;&lt;P&gt;In the meantime, if you want to investigate further, I suggest to use the following tips &amp;amp; tricks to isolate a the root cause: &lt;A href="https://community.nxp.com/message/482428"&gt;MC1322x: How to get memory dumps to analyze at failure state... and other tips &amp;amp;amp; tricks&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Feb 2015 17:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328541#M9</guid>
      <dc:creator>AlanCollins</dc:creator>
      <dc:date>2015-02-18T17:18:24Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with updating from ARM7 Beestack Codebase  3.0.11 to 3.1.1 on MC13224V</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328542#M10</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alan, thanks for nice guide for memory dumps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed that the sniffer software also suffers from the same problem. It could go unnoticed because it doesn't go "deaf" like HA coordinator sw does. But I noticed that the timestamp received with frames resets after this 4:45 time period. I was using MC1322x_Sniffer_Firmware_MC2.1_V1.0.2 firmware. &lt;BR /&gt;Also this showed more accurate representation that how long time this period takes. It was 4 hours 46 minutes 10-20 seconds, at least according to the sniffer timestamps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information will be helpful for you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Br,&lt;/P&gt;&lt;P&gt;Teemu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2015 11:32:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Problem-with-updating-from-ARM7-Beestack-Codebase-3-0-11-to-3-1/m-p/328542#M10</guid>
      <dc:creator>teemuavellan</dc:creator>
      <dc:date>2015-03-12T11:32:41Z</dc:date>
    </item>
  </channel>
</rss>