<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to handle E_ZCL_ERR_ZTRANSMIT_FAIL status return? in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/How-to-handle-E-ZCL-ERR-ZTRANSMIT-FAIL-status-return/m-p/668938#M2872</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This authentication interval must be set on all potential parent nodes via the network parameter APS Security Timeout Period&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;10.7 Advanced Device Parameters&lt;/P&gt;&lt;P&gt;APS Inter-frame Delay&lt;/P&gt;&lt;P&gt;Number of milliseconds between APS data frames. Following transmission of each data block, the APS starts a timer. If there are more unacknowledged blocks to send in the current transmission window then, after a delay of apsInterframeDelay milliseconds the next block is passed to the NWK data service. Otherwise, the timer is set to apscAckWaitDuration seconds.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/documents/user_manual/JN-UG-3101.pdf?fsrch=1&amp;amp;sr=5&amp;amp;pageNum=1" title="http://cache.nxp.com/documents/user_manual/JN-UG-3101.pdf?fsrch=1&amp;amp;sr=5&amp;amp;pageNum=1"&gt;http://www.nxp.com/documents/user_manual/JN-UG-3101.pdf?fsrch=1&amp;amp;sr=5&amp;amp;pageNum=1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 May 2017 21:13:17 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2017-05-19T21:13:17Z</dc:date>
    <item>
      <title>How to handle E_ZCL_ERR_ZTRANSMIT_FAIL status return?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/How-to-handle-E-ZCL-ERR-ZTRANSMIT-FAIL-status-return/m-p/668937#M2871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an application running on my main processor that talks to the Zigbee firmware running on the ZigBee chip (in this case JN5169).&lt;/P&gt;&lt;P&gt;Whenever I send a command to a device that is offline, I stop when I receive the 0x8702 reply (APS Data Confirm Fail).&lt;/P&gt;&lt;P&gt;However, when I now try to send a new command (to the same or a different device), I receive a status message (0x8000) with error code 0x15 (E_ZCL_ERR_ZTRANSMIT_FAIL).&lt;/P&gt;&lt;P&gt;It now takes several seconds before I can send again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;How should I handle&amp;nbsp;E_ZCL_ERR_ZTRANSMIT_FAIL?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Is there a better solution to handle this issue than to wait until I can send again?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using using JN-AN-1223 with JN-SW-4168 v1470&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 May 2017 09:55:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/How-to-handle-E-ZCL-ERR-ZTRANSMIT-FAIL-status-return/m-p/668937#M2871</guid>
      <dc:creator>baskoevoets</dc:creator>
      <dc:date>2017-05-05T09:55:50Z</dc:date>
    </item>
    <item>
      <title>Re: How to handle E_ZCL_ERR_ZTRANSMIT_FAIL status return?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/How-to-handle-E-ZCL-ERR-ZTRANSMIT-FAIL-status-return/m-p/668938#M2872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This authentication interval must be set on all potential parent nodes via the network parameter APS Security Timeout Period&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;10.7 Advanced Device Parameters&lt;/P&gt;&lt;P&gt;APS Inter-frame Delay&lt;/P&gt;&lt;P&gt;Number of milliseconds between APS data frames. Following transmission of each data block, the APS starts a timer. If there are more unacknowledged blocks to send in the current transmission window then, after a delay of apsInterframeDelay milliseconds the next block is passed to the NWK data service. Otherwise, the timer is set to apscAckWaitDuration seconds.&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/documents/user_manual/JN-UG-3101.pdf?fsrch=1&amp;amp;sr=5&amp;amp;pageNum=1" title="http://cache.nxp.com/documents/user_manual/JN-UG-3101.pdf?fsrch=1&amp;amp;sr=5&amp;amp;pageNum=1"&gt;http://www.nxp.com/documents/user_manual/JN-UG-3101.pdf?fsrch=1&amp;amp;sr=5&amp;amp;pageNum=1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 May 2017 21:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/How-to-handle-E-ZCL-ERR-ZTRANSMIT-FAIL-status-return/m-p/668938#M2872</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2017-05-19T21:13:17Z</dc:date>
    </item>
  </channel>
</rss>