<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: JN5168 Receive frame from a device</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5168-Receive-frame-from-a-device/m-p/666562#M2813</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following Receive functions are provided in the MicroMAC API&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please check the&amp;nbsp;ZigBee Green Power User Guide? JN-UG-3095&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/documents/user_manual/JN-UG-3095.pdf?fsrch=1&amp;amp;sr=8&amp;amp;pageNum=1" title="http://cache.nxp.com/documents/user_manual/JN-UG-3095.pdf?fsrch=1&amp;amp;sr=8&amp;amp;pageNum=1"&gt;http://www.nxp.com/documents/user_manual/JN-UG-3095.pdf?fsrch=1&amp;amp;sr=8&amp;amp;pageNum=1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void vMMAC_StartMacReceive(tsMacFrame *psFrame,  teRxOption eOptions);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uPayload is a union containing the payload data as either a byte-array or word-array:&lt;/P&gt;&lt;P&gt; au8Byte[127] is the payload data as an array of bytes&lt;/P&gt;&lt;P&gt; au32Word[32] is the payload data as an array of words&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 May 2017 19:20:17 GMT</pubDate>
    <dc:creator>mario_castaneda</dc:creator>
    <dc:date>2017-05-09T19:20:17Z</dc:date>
    <item>
      <title>JN5168 Receive frame from a device</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5168-Receive-frame-from-a-device/m-p/666561#M2812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on the JN5168 , I have some problems. I want to know how I&amp;nbsp;can receive and store the Zigbee frame from a device&amp;nbsp;in a variable.&lt;/P&gt;&lt;P&gt;My device send frame with the format of zigbee green power.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you tell me what is the command to&amp;nbsp;do that and in which library i can find this command ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 08:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5168-Receive-frame-from-a-device/m-p/666561#M2812</guid>
      <dc:creator>bricesup</dc:creator>
      <dc:date>2017-05-04T08:27:33Z</dc:date>
    </item>
    <item>
      <title>Re: JN5168 Receive frame from a device</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5168-Receive-frame-from-a-device/m-p/666562#M2813</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following Receive functions are provided in the MicroMAC API&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please check the&amp;nbsp;ZigBee Green Power User Guide? JN-UG-3095&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="http://cache.nxp.com/documents/user_manual/JN-UG-3095.pdf?fsrch=1&amp;amp;sr=8&amp;amp;pageNum=1" title="http://cache.nxp.com/documents/user_manual/JN-UG-3095.pdf?fsrch=1&amp;amp;sr=8&amp;amp;pageNum=1"&gt;http://www.nxp.com/documents/user_manual/JN-UG-3095.pdf?fsrch=1&amp;amp;sr=8&amp;amp;pageNum=1&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void vMMAC_StartMacReceive(tsMacFrame *psFrame,  teRxOption eOptions);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uPayload is a union containing the payload data as either a byte-array or word-array:&lt;/P&gt;&lt;P&gt; au8Byte[127] is the payload data as an array of bytes&lt;/P&gt;&lt;P&gt; au32Word[32] is the payload data as an array of words&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 May 2017 19:20:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5168-Receive-frame-from-a-device/m-p/666562#M2813</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2017-05-09T19:20:17Z</dc:date>
    </item>
  </channel>
</rss>