<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックCommissioning of Thread devices</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Commissioning-of-Thread-devices/m-p/330355#M28</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thread uses a secure scheme of commissioning based on the proven DTLS open standard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Users can authorize devices onto a Thread network using smart phones, tablets, or laptops/PCs. Also, GUI rich devices within the network can be used to authorize other devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When a new device is about to be enrolled in a Thread network, a security session is established between the new device and the commissioning device to authenticate and to provide the required credentials.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A Thread device can still function without a link to the internet provided by a Border Router. It can communicate with any other Thread device in the network or within the extended in-premise network.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Nov 2014 11:09:09 GMT</pubDate>
    <dc:creator>mihaidragnea</dc:creator>
    <dc:date>2014-11-11T11:09:09Z</dc:date>
    <item>
      <title>Commissioning of Thread devices</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Commissioning-of-Thread-devices/m-p/330355#M28</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thread uses a secure scheme of commissioning based on the proven DTLS open standard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Users can authorize devices onto a Thread network using smart phones, tablets, or laptops/PCs. Also, GUI rich devices within the network can be used to authorize other devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When a new device is about to be enrolled in a Thread network, a security session is established between the new device and the commissioning device to authenticate and to provide the required credentials.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A Thread device can still function without a link to the internet provided by a Border Router. It can communicate with any other Thread device in the network or within the extended in-premise network.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Nov 2014 11:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Commissioning-of-Thread-devices/m-p/330355#M28</guid>
      <dc:creator>mihaidragnea</dc:creator>
      <dc:date>2014-11-11T11:09:09Z</dc:date>
    </item>
  </channel>
</rss>