<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: PC cannot recognize USB-kw24d512 USB dongle</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/PC-cannot-recognize-USB-kw24d512-USB-dongle/m-p/660793#M2690</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Gerardo Rodriguez Espinoza&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reply all the same.&lt;/P&gt;&lt;P&gt;It is a hardware issue because Jtag line is modify by wrong method.&lt;/P&gt;&lt;P&gt;Now it is OK and flash can be succeed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 12 May 2017 01:02:30 GMT</pubDate>
    <dc:creator>lunwang</dc:creator>
    <dc:date>2017-05-12T01:02:30Z</dc:date>
    <item>
      <title>PC cannot recognize USB-kw24d512 USB dongle</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PC-cannot-recognize-USB-kw24d512-USB-dongle/m-p/660791#M2688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My PC cannot recognize usb-kw24d512 as the virtual com port. there is the same problem when I change to other PC.&lt;/P&gt;&lt;P&gt;Several days ago ,I try to update the firmware through through j-link ,but USB dongle cannot contact with j-link and flash unsuccessfully.&lt;/P&gt;&lt;P&gt;After that, my PC can not recognize the USB dongle till now.&lt;/P&gt;&lt;P&gt;Please help to solve this problem. thanks.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;=====================================================================&lt;/P&gt;&lt;P&gt;J-link log:&lt;/P&gt;&lt;P&gt;Application log started&lt;BR /&gt;&amp;nbsp;- J-Flash V6.12j (J-Flash compiled Feb 15 2017 18:01:27)&lt;BR /&gt;&amp;nbsp;- JLinkARM.dll V6.12j (DLL compiled Feb 15 2017 18:01:10)&lt;BR /&gt;Reading flash device list [C:\Program Files (x86)\SEGGER\JLink_V612j\ETC\JFlash\Flash.csv] ...&lt;BR /&gt;&amp;nbsp;- List of flash devices read successfully (451 Devices)&lt;BR /&gt;Reading MCU device list ...&lt;BR /&gt;&amp;nbsp;- List of MCU devices read successfully (6341 Devices)&lt;BR /&gt;Opening project file [C:\Program Files (x86)\SEGGER\JLink_V612j\Samples\JFlash\ProjectFiles\Freescale\111.jflash] ...&lt;BR /&gt;&amp;nbsp;- Project opened successfully&lt;BR /&gt;Connecting ...&lt;BR /&gt;&amp;nbsp;- Connecting via USB to J-Link device 0&lt;BR /&gt;&amp;nbsp;- Target interface speed: 1000 kHz (Auto)&lt;BR /&gt;&amp;nbsp;- VTarget = 2.805V&lt;BR /&gt;&amp;nbsp;- ERROR: Failed to connect.&lt;BR /&gt;Could not establish a connection to target.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 May 2017 03:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PC-cannot-recognize-USB-kw24d512-USB-dongle/m-p/660791#M2688</guid>
      <dc:creator>lunwang</dc:creator>
      <dc:date>2017-05-03T03:56:35Z</dc:date>
    </item>
    <item>
      <title>Re: PC cannot recognize USB-kw24d512 USB dongle</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PC-cannot-recognize-USB-kw24d512-USB-dongle/m-p/660792#M2689</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi lun wang,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you trying to use the USB-KW24D512 as a sniffer? If so, please follow the next steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Locate the &lt;EM&gt;USB-KW24D512_802.15.4_Sniffer.bin&lt;/EM&gt; file included in the &lt;A href="http://www.nxp.com/assets/downloads/data/en/board-support-packages/USBKW24D512-BSP.zip"&gt;USB-KW24D512 Board Support Package&lt;/A&gt;.&lt;/LI&gt;&lt;LI&gt;Copy and paste this binary file in the JLink installation path (i.e. "C:\Program Files (x86)\SEGGER\JLink_V600").&lt;/LI&gt;&lt;LI&gt;Connect the Jlink debugger to the corresponding JTAG connector (J1) in the USB-KW24D512.&lt;/LI&gt;&lt;LI&gt;Go the JLink installation path, and then open the application "JLink.exe".&lt;/LI&gt;&lt;LI&gt;Call the next instructions:&lt;OL style="list-style-type: lower-alpha;"&gt;&lt;LI&gt;unlock kinetis&lt;/LI&gt;&lt;LI&gt;device mkw24d512xxx5&lt;/LI&gt;&lt;LI&gt;loadbin USB-KW24D512_802.15.4_Sniffer.bin 0&lt;/LI&gt;&lt;LI&gt;(select SWD and default speed)&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;LI&gt;Unplug and plug again the USB-KW24D512.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Gerardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 May 2017 23:20:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PC-cannot-recognize-USB-kw24d512-USB-dongle/m-p/660792#M2689</guid>
      <dc:creator>gerardo_rodriguez</dc:creator>
      <dc:date>2017-05-04T23:20:59Z</dc:date>
    </item>
    <item>
      <title>Re: PC cannot recognize USB-kw24d512 USB dongle</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PC-cannot-recognize-USB-kw24d512-USB-dongle/m-p/660793#M2690</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Gerardo Rodriguez Espinoza&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for reply all the same.&lt;/P&gt;&lt;P&gt;It is a hardware issue because Jtag line is modify by wrong method.&lt;/P&gt;&lt;P&gt;Now it is OK and flash can be succeed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 May 2017 01:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PC-cannot-recognize-USB-kw24d512-USB-dongle/m-p/660793#M2690</guid>
      <dc:creator>lunwang</dc:creator>
      <dc:date>2017-05-12T01:02:30Z</dc:date>
    </item>
  </channel>
</rss>