<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 FRDM KW41Z Some Sample Projects Failing to Compile</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Some-Sample-Projects-Failing-to-Compile/m-p/650453#M2443</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day,&lt;/P&gt;&lt;P&gt;I recently received a FRDM KW41Z board and some of the sample projects within KDS are not compiling.&amp;nbsp; In particular:&lt;/P&gt;&lt;P&gt;a. health_thermometer_frdmkw41z&lt;/P&gt;&lt;P&gt;b. wireless_uart_frdmKW41z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I look at the first one I get errors relating to the frame work files like the following:&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc: error: C:/Software/NXP/MKW41Z_ConnSw_1.0.2/middleware/wireless/framework_5.3.2/XCVR/&lt;STRONG&gt;MW41Z4&lt;/STRONG&gt;/fsl_xcvr_gfsk_bt_0p3_h_0p5_config.c: No such file or directory&lt;BR /&gt;arm-none-eabi-gcc: fatal error: no input files&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here you will note that a portion of the the path is incorrect.. i.e. it should be MKW41Z4 (i.e. the "k" is missing.&amp;nbsp; The other fsl_xcvr_gfsk_bt* files fail compilation with similar errors... different aspects of the path is missing, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The wireless_uart has similar errors where the path or even source file name is invalid.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I review the file's, etc within KDS's project explorer all the files are correctly found and can be opened.&amp;nbsp; It seems as if the compilation process is messing up and somehow corrupting some of the passing parameters to the arm compiler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone else had these type of issues and if so how were you able to correct them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 18 Feb 2017 22:45:21 GMT</pubDate>
    <dc:creator>samsaprunoff</dc:creator>
    <dc:date>2017-02-18T22:45:21Z</dc:date>
    <item>
      <title>FRDM KW41Z Some Sample Projects Failing to Compile</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Some-Sample-Projects-Failing-to-Compile/m-p/650453#M2443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day,&lt;/P&gt;&lt;P&gt;I recently received a FRDM KW41Z board and some of the sample projects within KDS are not compiling.&amp;nbsp; In particular:&lt;/P&gt;&lt;P&gt;a. health_thermometer_frdmkw41z&lt;/P&gt;&lt;P&gt;b. wireless_uart_frdmKW41z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I look at the first one I get errors relating to the frame work files like the following:&lt;/P&gt;&lt;P&gt;arm-none-eabi-gcc: error: C:/Software/NXP/MKW41Z_ConnSw_1.0.2/middleware/wireless/framework_5.3.2/XCVR/&lt;STRONG&gt;MW41Z4&lt;/STRONG&gt;/fsl_xcvr_gfsk_bt_0p3_h_0p5_config.c: No such file or directory&lt;BR /&gt;arm-none-eabi-gcc: fatal error: no input files&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here you will note that a portion of the the path is incorrect.. i.e. it should be MKW41Z4 (i.e. the "k" is missing.&amp;nbsp; The other fsl_xcvr_gfsk_bt* files fail compilation with similar errors... different aspects of the path is missing, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The wireless_uart has similar errors where the path or even source file name is invalid.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I review the file's, etc within KDS's project explorer all the files are correctly found and can be opened.&amp;nbsp; It seems as if the compilation process is messing up and somehow corrupting some of the passing parameters to the arm compiler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone else had these type of issues and if so how were you able to correct them?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Feb 2017 22:45:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Some-Sample-Projects-Failing-to-Compile/m-p/650453#M2443</guid>
      <dc:creator>samsaprunoff</dc:creator>
      <dc:date>2017-02-18T22:45:21Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM KW41Z Some Sample Projects Failing to Compile</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Some-Sample-Projects-Failing-to-Compile/m-p/650454#M2444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good day All,&lt;/P&gt;&lt;P&gt;You can ignore my previous question, as it would seem that I had an older version of KDS installed (3.0.0).&amp;nbsp; Once I realized this and used ver 3.2.0 the projects are compiling correctly.&lt;/P&gt;&lt;P&gt;My apologies for the distraction!&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 18 Feb 2017 23:02:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW41Z-Some-Sample-Projects-Failing-to-Compile/m-p/650454#M2444</guid>
      <dc:creator>samsaprunoff</dc:creator>
      <dc:date>2017-02-18T23:02:19Z</dc:date>
    </item>
  </channel>
</rss>