<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックKW41Z Socket communication with PC</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW41Z-Socket-communication-with-PC/m-p/646988#M2393</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have the USB-KW41Z and FRDM-KW41Z kits and I'm running the Thread network demo on them, with the USB being the border router. I've successfully remade some functions so that they fit my project but what I've been stuck on is transfering data (a temperature value to be exact) from my border router to my PC. I've been trying to do so through sockets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried using both the UDP and TCP protocol functions from&amp;nbsp;app_socket_utils.h, I've also attempted to do it on my own using only the functions provided in sockets.h and I've also used the shell demo for socket communications on one of the FRDM nodes in my network.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using TCP, my program causes a hard fault when it uses the connect() function. When using UDP, sendto() returns -1. Interestingly, sending data through sockets from my PC to the node works fine. Also, I can ping the nodes and the border router from my PC but can't ping my PC from the nodes, not sure if that's related.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also tried disabling the firewall and windows defender completely but that didn't help either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone who encountered the same problem? Any advice would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Apr 2017 15:37:59 GMT</pubDate>
    <dc:creator>davidpiskula</dc:creator>
    <dc:date>2017-04-03T15:37:59Z</dc:date>
    <item>
      <title>KW41Z Socket communication with PC</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW41Z-Socket-communication-with-PC/m-p/646988#M2393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have the USB-KW41Z and FRDM-KW41Z kits and I'm running the Thread network demo on them, with the USB being the border router. I've successfully remade some functions so that they fit my project but what I've been stuck on is transfering data (a temperature value to be exact) from my border router to my PC. I've been trying to do so through sockets.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried using both the UDP and TCP protocol functions from&amp;nbsp;app_socket_utils.h, I've also attempted to do it on my own using only the functions provided in sockets.h and I've also used the shell demo for socket communications on one of the FRDM nodes in my network.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using TCP, my program causes a hard fault when it uses the connect() function. When using UDP, sendto() returns -1. Interestingly, sending data through sockets from my PC to the node works fine. Also, I can ping the nodes and the border router from my PC but can't ping my PC from the nodes, not sure if that's related.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also tried disabling the firewall and windows defender completely but that didn't help either.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone who encountered the same problem? Any advice would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Apr 2017 15:37:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW41Z-Socket-communication-with-PC/m-p/646988#M2393</guid>
      <dc:creator>davidpiskula</dc:creator>
      <dc:date>2017-04-03T15:37:59Z</dc:date>
    </item>
    <item>
      <title>Re: KW41Z Socket communication with PC</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW41Z-Socket-communication-with-PC/m-p/646989#M2394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Please check the below link and let me know if this helps:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/446739"&gt;MKW41z NXP Thread stack socket decryption&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Soledad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Apr 2017 18:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW41Z-Socket-communication-with-PC/m-p/646989#M2394</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-04-07T18:57:45Z</dc:date>
    </item>
    <item>
      <title>Re: KW41Z Socket communication with PC</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW41Z-Socket-communication-with-PC/m-p/646990#M2395</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, thanks for the answer, I ended up trying it out on Ubuntu-mate and there are no problems with it there, so it's most likely a problem with Windows. I don't really need it to work on Windows either, I just had a different issue regarding my raspberry pi, so I was trying to develop everything on Windows at the time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would delete the question but I do not know how to do that, so I'll just mark it as resolved, if that's ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nevertheless, thank you for your answer and have a nice day,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 09 Apr 2017 13:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW41Z-Socket-communication-with-PC/m-p/646990#M2395</guid>
      <dc:creator>davidpiskula</dc:creator>
      <dc:date>2017-04-09T13:55:39Z</dc:date>
    </item>
    <item>
      <title>Re: KW41Z Socket communication with PC</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW41Z-Socket-communication-with-PC/m-p/646991#M2396</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know, it's been a while since you started this post, but I'm trying to do the same with the same Hardware and sockets on Linux. Could you maybe give me some Information how you proceed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;&amp;nbsp;&amp;nbsp;You flashed the FRDM-KW41Z for example as RouterEligableDevice?&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp; You flashed the USB-KW41Z (MKW41) as Border-Router?&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;&amp;nbsp;&amp;nbsp;You flashed the USB-KW41Z (K22F) with rndis_bridge application?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4.&amp;nbsp;&amp;nbsp; But what have you done on the linux site to communicate via sockets with the end device? You are adressing the THREAD Nodes with ipv6-addresses in your self written linux application? Or is there something existing on linux to do this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would be awesome if you could give me some Information! Thanks a lot!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regrads,&lt;/P&gt;&lt;P&gt;Steffen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 23 Sep 2017 09:26:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW41Z-Socket-communication-with-PC/m-p/646991#M2396</guid>
      <dc:creator>steffenjahnkepa</dc:creator>
      <dc:date>2017-09-23T09:26:47Z</dc:date>
    </item>
  </channel>
</rss>