<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックCustom Board Support BeeStack #else /* gTarget_UserDefined_d */ no MCU_MKW24D512</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Custom-Board-Support-BeeStack-else-gTarget-UserDefined-d-no-MCU/m-p/646317#M2378</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to figure out the beestack port configurations. I have a custom board so&amp;nbsp;&lt;STRONG&gt;gTarget_UserDefined_d should be 1&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;In this case the macros include some headers given the MCU defined however even though there are tons of boards only a few MCU's in the PortConfig.h. Is this because other MCUs are covered by the boards? What should I do where I have a custom board that I want to adjust the port control registers of?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And also what is the explanation of that the code was generated with&amp;nbsp;gTarget_UserDefined_d = 0 even though I selected custom target and MKW24D512 MCU during BeeKit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jan 2017 17:37:01 GMT</pubDate>
    <dc:creator>atillametetured</dc:creator>
    <dc:date>2017-01-25T17:37:01Z</dc:date>
    <item>
      <title>Custom Board Support BeeStack #else /* gTarget_UserDefined_d */ no MCU_MKW24D512</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Custom-Board-Support-BeeStack-else-gTarget-UserDefined-d-no-MCU/m-p/646317#M2378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to figure out the beestack port configurations. I have a custom board so&amp;nbsp;&lt;STRONG&gt;gTarget_UserDefined_d should be 1&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;In this case the macros include some headers given the MCU defined however even though there are tons of boards only a few MCU's in the PortConfig.h. Is this because other MCUs are covered by the boards? What should I do where I have a custom board that I want to adjust the port control registers of?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And also what is the explanation of that the code was generated with&amp;nbsp;gTarget_UserDefined_d = 0 even though I selected custom target and MKW24D512 MCU during BeeKit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Mete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jan 2017 17:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Custom-Board-Support-BeeStack-else-gTarget-UserDefined-d-no-MCU/m-p/646317#M2378</guid>
      <dc:creator>atillametetured</dc:creator>
      <dc:date>2017-01-25T17:37:01Z</dc:date>
    </item>
  </channel>
</rss>