<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックKW01 TPMS Receiver cannot work with FXTH870911 – 434Hz EVB.</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW01-TPMS-Receiver-cannot-work-with-FXTH870911-434Hz-EVB/m-p/645782#M2366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you someone please take a look at this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on TPMS evaluation system with NXP's emitter, FXTH870911 – 434Hz, and receiver, MRB-KW019030JA.&lt;/P&gt;&lt;P&gt;And deployed SW is "TPMS FXTH87 MKW01 CW10 Rev4 " for emitter and "MKW01_IAR7v4_Project_TPMS_Rev0.6" for receiver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For some reason, I purchased the MRB-KW019030JA instead of MRB-KW019032NA and made some change on receiver side so as to fit for 30MHz XTAL on MRB-KW01.&lt;BR /&gt;(changing is made on clock source for KW01, 30MHz from 2MHz and PLL configuration and some frequency constant for 30MHz)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, it's not working, means I cannot see the packet MSG on the hyperterminal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know what I missed or made some wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your information, I can see the RSSI value is changed on Radio Utility tool.&lt;BR /&gt;So, it looks like not totally working but some parameter or something else is missed or not matched.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/tpms sensor/tg-p"&gt;#tpms sensor&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Dec 2016 09:26:09 GMT</pubDate>
    <dc:creator>jylee</dc:creator>
    <dc:date>2016-12-28T09:26:09Z</dc:date>
    <item>
      <title>KW01 TPMS Receiver cannot work with FXTH870911 – 434Hz EVB.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW01-TPMS-Receiver-cannot-work-with-FXTH870911-434Hz-EVB/m-p/645782#M2366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you someone please take a look at this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on TPMS evaluation system with NXP's emitter, FXTH870911 – 434Hz, and receiver, MRB-KW019030JA.&lt;/P&gt;&lt;P&gt;And deployed SW is "TPMS FXTH87 MKW01 CW10 Rev4 " for emitter and "MKW01_IAR7v4_Project_TPMS_Rev0.6" for receiver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For some reason, I purchased the MRB-KW019030JA instead of MRB-KW019032NA and made some change on receiver side so as to fit for 30MHz XTAL on MRB-KW01.&lt;BR /&gt;(changing is made on clock source for KW01, 30MHz from 2MHz and PLL configuration and some frequency constant for 30MHz)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, it's not working, means I cannot see the packet MSG on the hyperterminal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know what I missed or made some wrong.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your information, I can see the RSSI value is changed on Radio Utility tool.&lt;BR /&gt;So, it looks like not totally working but some parameter or something else is missed or not matched.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/tag/tpms sensor/tg-p"&gt;#tpms sensor&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 09:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW01-TPMS-Receiver-cannot-work-with-FXTH870911-434Hz-EVB/m-p/645782#M2366</guid>
      <dc:creator>jylee</dc:creator>
      <dc:date>2016-12-28T09:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: KW01 TPMS Receiver cannot work with FXTH870911 – 434Hz EVB.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW01-TPMS-Receiver-cannot-work-with-FXTH870911-434Hz-EVB/m-p/645783#M2367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jaeyeol Lee&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the status of your issue? Could you explain more how you made this change on clock source for KW01?. Because FXOSC has changed to 30 Mhz, Fstep, &lt;STRONG&gt;Frf&lt;/STRONG&gt;,&amp;nbsp;&lt;STRONG&gt;Fdev&lt;/STRONG&gt; and &lt;STRONG&gt;BR&lt;/STRONG&gt; have changed too, so they need to be re-calculated and redefined. In the demo that you are using, you can find these values defined with gDefaultRfFreq_c, gDefaultFreqDv_c, gDefaultBitRate_c in ApplicationConf.h file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please take a look to section 3.2.1 of the application note &lt;A href="http://www.nxp.com/assets/documents/data/en/application-notes/AN5136.pdf"&gt;AN5136&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Here they explain how to calculate these values for 315 MHz, so for example, Frf= (315M)/Fstep and Fstep= 61.03515625 for a 32Mhz FXOSC, then Frf=5160960.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, you should check that your MCG config is correctly set in your device (like you mentioned, your PLL configuration and other values), you can find this configuration in Platform_Init in main.c.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information helps you&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2017 23:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW01-TPMS-Receiver-cannot-work-with-FXTH870911-434Hz-EVB/m-p/645783#M2367</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-01-11T23:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: KW01 TPMS Receiver cannot work with FXTH870911 – 434Hz EVB.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW01-TPMS-Receiver-cannot-work-with-FXTH870911-434Hz-EVB/m-p/645784#M2368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge Alcala,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your update.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually, A workaround was made a week ago and verified it works with TPMS Emitter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you mentioned below, the changes have been made on the constants and MCG configuration for PLL of KW01.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For your information, I attach the patch of this workaround, &amp;lt;&amp;lt;MRB-KW019030JA_Patch_03Jan2017.zip &amp;gt;&amp;gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have a time, please take a look at this patch and let me know if there is something missed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyhow, thank you for your attention and sorry for missing update you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tommy(Jae-yeol) Lee&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jan 2017 01:04:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW01-TPMS-Receiver-cannot-work-with-FXTH870911-434Hz-EVB/m-p/645784#M2368</guid>
      <dc:creator>jylee</dc:creator>
      <dc:date>2017-01-12T01:04:13Z</dc:date>
    </item>
  </channel>
</rss>