<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: Is it possible to add serial bootloader functionality to otap bootloader?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644983#M2362</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried flashing firmware via serial port with ./fsci_bootloader.py but it always breaks at 44.81% (-&amp;gt; gHandleBootError_d();) which resets the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea what is going wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional info: OTAP works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18590iC4A4D59F000591B4/image-size/large?v=v2&amp;amp;px=999" title="error.JPG" alt="error.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Mar 2017 15:34:28 GMT</pubDate>
    <dc:creator>joachimk</dc:creator>
    <dc:date>2017-03-23T15:34:28Z</dc:date>
    <item>
      <title>Is it possible to add serial bootloader functionality to otap bootloader?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644980#M2359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have created a wireless project which uses ble + thread in concurence.&lt;/P&gt;&lt;P&gt;We need to update the firmware over-the-air, so i have programmed otap bootloader into the device (kw41z).&lt;/P&gt;&lt;P&gt;But we also want to update the firmware via a serial connection.&lt;/P&gt;&lt;P&gt;Is it possible to do so? Is there any document about this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Mar 2017 13:19:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644980#M2359</guid>
      <dc:creator>joachimk</dc:creator>
      <dc:date>2017-03-13T13:19:46Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to add serial bootloader functionality to otap bootloader?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644981#M2360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joachim Keh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, basically you need two bootloaders; we provide with these two bootloaders in the connectivity software, you can find them in the path: {MKW41Z_ConnSw_1.0.2}\boards\frdmkw41z\wireless_examples\framework. Problem here is that they cannot coexist, because both of them are implemented to work as they were the only bootloader working. So if you want to use both of them, you need to combine this two bootloaders.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check section 3.21.Bootloader of the Connectivity Framework Reference Manual located in {MKW41Z_ConnSw_1.0.2}\docs\wireless\Common.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information helps you&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jorge Alcala&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Mar 2017 18:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644981#M2360</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2017-03-22T18:04:10Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to add serial bootloader functionality to otap bootloader?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644982#M2361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the document was really helpful! Thanks!&lt;/P&gt;&lt;P&gt;Is there any recommended Serial FlashTool for Windows?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 08:31:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644982#M2361</guid>
      <dc:creator>joachimk</dc:creator>
      <dc:date>2017-03-23T08:31:16Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to add serial bootloader functionality to otap bootloader?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644983#M2362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried flashing firmware via serial port with ./fsci_bootloader.py but it always breaks at 44.81% (-&amp;gt; gHandleBootError_d();) which resets the MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea what is going wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Additional info: OTAP works fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/18590iC4A4D59F000591B4/image-size/large?v=v2&amp;amp;px=999" title="error.JPG" alt="error.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Mar 2017 15:34:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644983#M2362</guid>
      <dc:creator>joachimk</dc:creator>
      <dc:date>2017-03-23T15:34:28Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to add serial bootloader functionality to otap bootloader?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644984#M2363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update / Solution:&lt;/P&gt;&lt;P&gt;-&amp;gt; Using .bin (raw binary) file instead of .srec file solves the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 10:58:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Is-it-possible-to-add-serial-bootloader-functionality-to-otap/m-p/644984#M2363</guid>
      <dc:creator>joachimk</dc:creator>
      <dc:date>2017-04-04T10:58:26Z</dc:date>
    </item>
  </channel>
</rss>