<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックUsing the KW2x series devices Low Power Preamble Search (LPPS) feature to save current.</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Using-the-KW2x-series-devices-Low-Power-Preamble-Search-LPPS/m-p/367548#M206</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MKW2x IEEE 802.15.4 series devices have a unique feature for that saves power during the receive sequence of the transceiver.&amp;nbsp; The feature is called Low Power Preamble Search (LPPS).&amp;nbsp; When the LPPS feature is enabled, the demodulator section of the receiver is duty cycled during part of the preamble search phase of packet reception.&amp;nbsp; During the LPPS phase of the preamble, the receiver looks for one symbol 0 match.&amp;nbsp; Once this criterion for LPPS is met the receiver goes into normal preamble search followed by packet processing.&amp;nbsp; The hardware sequence manager handles the timing and is not adjustable by the user.&amp;nbsp; During LPPS mode, the receiver current consumption is reduced approximately 4mA.&amp;nbsp; In addition, there is no added cost of using the LPPS feature since no extra components are required.&amp;nbsp; In fact, enabling LPPS mode all the time has little system design impact and the current savings is 20%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;LPPS Flow and timing diagram:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The following figures show the MKW2x LPPS flow diagram and timing associated with the feature.&amp;nbsp; Although not adjustable by the user, it figures show the hardware sequence of the feature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: center;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="LPPS - topic.PNG.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46409iEC89881372DA83ED/image-size/large?v=v2&amp;amp;px=999" role="button" title="LPPS - topic.PNG.png" alt="LPPS - topic.PNG.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Figure 1:&amp;nbsp; LPPS Flow Diagram&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="LPPS  timing- topic.PNG.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46410i21FF8B07DB36C669/image-size/large?v=v2&amp;amp;px=999" role="button" title="LPPS  timing- topic.PNG.png" alt="LPPS  timing- topic.PNG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="text-align: center;"&gt;Figure 2:&amp;nbsp; LPPS Timing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: left;"&gt;More infomation about the LPPS feature can be found in the MKW2x device reference manual located at : &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KW2x&amp;amp;tid=redKW20" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KW2x&amp;amp;tid=redKW20"&gt;KW2x |Kinetis KW2x 2.4 GHz RF MCUs|Freescale&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Oct 2014 21:17:09 GMT</pubDate>
    <dc:creator>franklatona-r49</dc:creator>
    <dc:date>2014-10-03T21:17:09Z</dc:date>
    <item>
      <title>Using the KW2x series devices Low Power Preamble Search (LPPS) feature to save current.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Using-the-KW2x-series-devices-Low-Power-Preamble-Search-LPPS/m-p/367548#M206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The MKW2x IEEE 802.15.4 series devices have a unique feature for that saves power during the receive sequence of the transceiver.&amp;nbsp; The feature is called Low Power Preamble Search (LPPS).&amp;nbsp; When the LPPS feature is enabled, the demodulator section of the receiver is duty cycled during part of the preamble search phase of packet reception.&amp;nbsp; During the LPPS phase of the preamble, the receiver looks for one symbol 0 match.&amp;nbsp; Once this criterion for LPPS is met the receiver goes into normal preamble search followed by packet processing.&amp;nbsp; The hardware sequence manager handles the timing and is not adjustable by the user.&amp;nbsp; During LPPS mode, the receiver current consumption is reduced approximately 4mA.&amp;nbsp; In addition, there is no added cost of using the LPPS feature since no extra components are required.&amp;nbsp; In fact, enabling LPPS mode all the time has little system design impact and the current savings is 20%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;LPPS Flow and timing diagram:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The following figures show the MKW2x LPPS flow diagram and timing associated with the feature.&amp;nbsp; Although not adjustable by the user, it figures show the hardware sequence of the feature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: center;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="LPPS - topic.PNG.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46409iEC89881372DA83ED/image-size/large?v=v2&amp;amp;px=999" role="button" title="LPPS - topic.PNG.png" alt="LPPS - topic.PNG.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Figure 1:&amp;nbsp; LPPS Flow Diagram&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="LPPS  timing- topic.PNG.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46410i21FF8B07DB36C669/image-size/large?v=v2&amp;amp;px=999" role="button" title="LPPS  timing- topic.PNG.png" alt="LPPS  timing- topic.PNG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="text-align: center;"&gt;Figure 2:&amp;nbsp; LPPS Timing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="text-align: left;"&gt;More infomation about the LPPS feature can be found in the MKW2x device reference manual located at : &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KW2x&amp;amp;tid=redKW20" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KW2x&amp;amp;tid=redKW20"&gt;KW2x |Kinetis KW2x 2.4 GHz RF MCUs|Freescale&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Oct 2014 21:17:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Using-the-KW2x-series-devices-Low-Power-Preamble-Search-LPPS/m-p/367548#M206</guid>
      <dc:creator>franklatona-r49</dc:creator>
      <dc:date>2014-10-03T21:17:09Z</dc:date>
    </item>
  </channel>
</rss>