<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM-MCXW72: AN14889 Sensitivity test in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW72-AN14889-Sensitivity-test/m-p/2418737#M20502</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am following the steps in the&amp;nbsp;AN14889 to run sensitivity tests on &lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;LI-PRODUCT title="FRDM-MCXW72" id="FRDM-MCXW72"&gt;&lt;/LI-PRODUCT&gt;&lt;SPAN&gt;&amp;nbsp;but without success&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I use the following sequence to run the test on channel 0 (2402 MHz).&lt;BR /&gt;Could you check it?&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Connectivity Test Interface short cuts&lt;BR /&gt;------------------------------------------&lt;BR /&gt;-Press [t] for Tx operation&lt;BR /&gt;-Press [r] for Rx operation&lt;BR /&gt;-Press [z] to increase mode (GENFSK, BLE) and rate&lt;BR /&gt;-Press [x] to decrease mode (GENFSK, BLE) and rate&lt;BR /&gt;-Press [c] to toggle between fixed or per channel whitening (for BLE only)&lt;BR /&gt;-Press [q] for channel up&lt;BR /&gt;-Press [w] for channel down&lt;BR /&gt;-Press [a] for Power up&lt;BR /&gt;-Press [s] for Power down&lt;BR /&gt;-Press [n] to increase the Payload&lt;BR /&gt;-Press [m] to decrease the Payload&lt;BR /&gt;-Press [d] to increase the XTAL Trim value&lt;BR /&gt;-Press [f] to decrease the XTAL Trim value&lt;BR /&gt;These keys can be used all over the application to change&lt;BR /&gt;the test parameters&lt;BR /&gt;________________________________&lt;BR /&gt;| |&lt;BR /&gt;| Select the Test to perform |&lt;BR /&gt;|________________________________|&lt;BR /&gt;-Press [1] Continuous tests&lt;BR /&gt;-Press [2] Packet Error Rate test&lt;BR /&gt;-Press [3] Range test&lt;BR /&gt;-Press [4] Adjust RTC XTAL&lt;BR /&gt;-Press [5] Adjust PLL numerator offset&lt;BR /&gt;-Press [!] Reset MCU&lt;/P&gt;&lt;P&gt;Mode RX, Rate BLE 1Mbps, Whiten Chan, Channel 42, Power 8, Payload 6, XtalTrim 10&amp;gt;&lt;/P&gt;&lt;P&gt;--------------------------------------------------------------&lt;BR /&gt;[t] Tx [z] Mode/Rate+ [c] Fix/Ch whit. [q] Ch+ [a] Pw+&lt;BR /&gt;[r] Rx [x] Mode/Rate- [w] Ch- [s] Pw-&lt;/P&gt;&lt;P&gt;[n] Pyld+ [d] XtalTrim+&lt;BR /&gt;[m] Pyld- [f] XtalTrim-&lt;BR /&gt;--------------------------------------------------------------&lt;BR /&gt;______________________&lt;BR /&gt;| |&lt;BR /&gt;| PER Rx Test Menu |&lt;BR /&gt;|______________________|&lt;/P&gt;&lt;P&gt;-Press [space bar] to start/stop Receiving Packets&lt;BR /&gt;-Press any push button to stop Receiving Packets&lt;BR /&gt;-Press [p] Previous Menu&lt;/P&gt;&lt;P&gt;Mode RX, Rate BLE 1Mbps, Whiten Chan, Channel 42, Power 8, Payload 6, XtalTrim 10&amp;gt;&lt;/P&gt;&lt;P&gt;PER Test Rx Running&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;PER Test Rx Stopped&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Average Rssi during PER: 0 dBm&lt;BR /&gt;Received 0 of 0 packets transmitted&lt;/P&gt;&lt;P&gt;Press [ENTER] to go back to the Per Rx test menu&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I use a BLE tester to send the standard BLE test packets but the board doesn't receive any packet.&lt;BR /&gt;The application note does not specify any setting for the sensitivity test.&lt;BR /&gt;&lt;BR /&gt;On the other hand if I use hci_bb application and standard HCI commands, the board gets stuck randomly at all PHY only when the tester sends the HCI_LE_RECEIVER_TEST or HCI_LE_ENHANCED_RECEIVER_TEST make it impossible to run the tests.&lt;BR /&gt;The transmitter test command works flawlessly.&lt;BR /&gt;&lt;BR /&gt;Could you give me some advices?&lt;BR /&gt;I am using&amp;nbsp;SDK_26_06_00_FRDM-MCXW72.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Marco&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 06 Oct 2026 10:31:27 GMT</pubDate>
    <dc:creator>Marcon</dc:creator>
    <dc:date>2026-10-06T10:31:27Z</dc:date>
    <item>
      <title>FRDM-MCXW72: AN14889 Sensitivity test</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW72-AN14889-Sensitivity-test/m-p/2418737#M20502</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I am following the steps in the&amp;nbsp;AN14889 to run sensitivity tests on &lt;/SPAN&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;LI-PRODUCT title="FRDM-MCXW72" id="FRDM-MCXW72"&gt;&lt;/LI-PRODUCT&gt;&lt;SPAN&gt;&amp;nbsp;but without success&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I use the following sequence to run the test on channel 0 (2402 MHz).&lt;BR /&gt;Could you check it?&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;Connectivity Test Interface short cuts&lt;BR /&gt;------------------------------------------&lt;BR /&gt;-Press [t] for Tx operation&lt;BR /&gt;-Press [r] for Rx operation&lt;BR /&gt;-Press [z] to increase mode (GENFSK, BLE) and rate&lt;BR /&gt;-Press [x] to decrease mode (GENFSK, BLE) and rate&lt;BR /&gt;-Press [c] to toggle between fixed or per channel whitening (for BLE only)&lt;BR /&gt;-Press [q] for channel up&lt;BR /&gt;-Press [w] for channel down&lt;BR /&gt;-Press [a] for Power up&lt;BR /&gt;-Press [s] for Power down&lt;BR /&gt;-Press [n] to increase the Payload&lt;BR /&gt;-Press [m] to decrease the Payload&lt;BR /&gt;-Press [d] to increase the XTAL Trim value&lt;BR /&gt;-Press [f] to decrease the XTAL Trim value&lt;BR /&gt;These keys can be used all over the application to change&lt;BR /&gt;the test parameters&lt;BR /&gt;________________________________&lt;BR /&gt;| |&lt;BR /&gt;| Select the Test to perform |&lt;BR /&gt;|________________________________|&lt;BR /&gt;-Press [1] Continuous tests&lt;BR /&gt;-Press [2] Packet Error Rate test&lt;BR /&gt;-Press [3] Range test&lt;BR /&gt;-Press [4] Adjust RTC XTAL&lt;BR /&gt;-Press [5] Adjust PLL numerator offset&lt;BR /&gt;-Press [!] Reset MCU&lt;/P&gt;&lt;P&gt;Mode RX, Rate BLE 1Mbps, Whiten Chan, Channel 42, Power 8, Payload 6, XtalTrim 10&amp;gt;&lt;/P&gt;&lt;P&gt;--------------------------------------------------------------&lt;BR /&gt;[t] Tx [z] Mode/Rate+ [c] Fix/Ch whit. [q] Ch+ [a] Pw+&lt;BR /&gt;[r] Rx [x] Mode/Rate- [w] Ch- [s] Pw-&lt;/P&gt;&lt;P&gt;[n] Pyld+ [d] XtalTrim+&lt;BR /&gt;[m] Pyld- [f] XtalTrim-&lt;BR /&gt;--------------------------------------------------------------&lt;BR /&gt;______________________&lt;BR /&gt;| |&lt;BR /&gt;| PER Rx Test Menu |&lt;BR /&gt;|______________________|&lt;/P&gt;&lt;P&gt;-Press [space bar] to start/stop Receiving Packets&lt;BR /&gt;-Press any push button to stop Receiving Packets&lt;BR /&gt;-Press [p] Previous Menu&lt;/P&gt;&lt;P&gt;Mode RX, Rate BLE 1Mbps, Whiten Chan, Channel 42, Power 8, Payload 6, XtalTrim 10&amp;gt;&lt;/P&gt;&lt;P&gt;PER Test Rx Running&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;PER Test Rx Stopped&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Average Rssi during PER: 0 dBm&lt;BR /&gt;Received 0 of 0 packets transmitted&lt;/P&gt;&lt;P&gt;Press [ENTER] to go back to the Per Rx test menu&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I use a BLE tester to send the standard BLE test packets but the board doesn't receive any packet.&lt;BR /&gt;The application note does not specify any setting for the sensitivity test.&lt;BR /&gt;&lt;BR /&gt;On the other hand if I use hci_bb application and standard HCI commands, the board gets stuck randomly at all PHY only when the tester sends the HCI_LE_RECEIVER_TEST or HCI_LE_ENHANCED_RECEIVER_TEST make it impossible to run the tests.&lt;BR /&gt;The transmitter test command works flawlessly.&lt;BR /&gt;&lt;BR /&gt;Could you give me some advices?&lt;BR /&gt;I am using&amp;nbsp;SDK_26_06_00_FRDM-MCXW72.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Marco&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Oct 2026 10:31:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW72-AN14889-Sensitivity-test/m-p/2418737#M20502</guid>
      <dc:creator>Marcon</dc:creator>
      <dc:date>2026-10-06T10:31:27Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MCXW72: AN14889 Sensitivity test</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW72-AN14889-Sensitivity-test/m-p/2420011#M20512</link>
      <description>&lt;P&gt;Hello, hope you are doing well.&lt;/P&gt;
&lt;P&gt;Some features of the Connectivity Test Application like Packet Error Rate or Range Tests require the usage of two devices.&amp;nbsp; One of the platforms must be set in RX mode (by&lt;/P&gt;
&lt;P&gt;pressing “r”) and the other in TX (by pressing “t”).&lt;/P&gt;
&lt;P&gt;Could you please try the PER test with a board to board scenario? One board as the Tx and the other as Rx. This to first validate the Connectivity Test application in a controlled environment , and to identify if the configuration of the Rx was correct.&lt;/P&gt;
&lt;P&gt;You can find more information on steps and packet configuration to perform the PER test here:&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/middleware/wireless/ieee-802.15.4/docs/connectivity_test/CTACLIUG/topics/connectivity_test_cli.html" target="_blank"&gt;Steps to perform a PER test | Connectivity Test CLI — MCUXpresso SDK Documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The RF test flow described in AN14889 does not specify a custom packet or frame format for the sensitivity test, but instead relies on the standard Bluetooth Low Energy specifications.&lt;/P&gt;
&lt;P&gt;BLE RF PHY tests, including sensitivity and PER measurements, can also be performed using Direct Test Mode (DTM), which is defined in the &lt;A href="https://www.bluetooth.com/wp-content/uploads/Files/Specification/HTML/Core-60/out/en/low-energy-controller/direct-test-mode.html" target="_blank"&gt;Bluetooth Core Specification, Vol. 6, Part F.&lt;/A&gt; This section defines the LE Test packets and the standardized test procedures used for RF validation.&lt;/P&gt;
&lt;P&gt;The underlying packet structure itself (preamble, access address, PDU, CRC) is defined in the &lt;A href="https://www.bluetooth.com/wp-content/uploads/Files/Specification/HTML/Core-60/out/en/low-energy-controller/link-layer-specification.html" target="_blank"&gt;Bluetooth Core Specification, Vol. 6, Part B&lt;/A&gt;. The LE Test packets used in DTM follow this same structure, with controlled payload patterns and parameters for testing.&lt;/P&gt;
&lt;P&gt;The specific test conditions and limits for measurements such as sensitivity and PER are also defined in the &lt;A href="https://files.bluetooth.com/wp-content/uploads/dlm_uploads/2026/05/RFPHY.TS.p25.pdf" target="_blank"&gt;Bluetooth RF-PHY Test Suite&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Sofia.&lt;/P&gt;</description>
      <pubDate>Sat, 10 Oct 2026 00:20:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW72-AN14889-Sensitivity-test/m-p/2420011#M20512</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2026-10-10T00:20:13Z</dc:date>
    </item>
  </channel>
</rss>