<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックKW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW45-Intermittent-Wire-ACK-Fault-During-Programming-Debugging/m-p/2411879#M20467</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am currently working with a KW45-based custom board and facing an intermittent issue during programming and debugging the firmware.&lt;/P&gt;&lt;P&gt;I have tested the board with both a SEGGER J-Link and an NXP MCU-Link debug probe, and the issue occurs with both probes.&lt;/P&gt;&lt;P&gt;The custom board has the same boot configuration as the KW45 EVK, and the JTAG/SWD connections have also been checked and appear to be correct.&lt;/P&gt;&lt;P&gt;However, I am seeing the following behaviour:&lt;/P&gt;&lt;P&gt;When I try to dump or program a known-working application:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Sometimes the application is programmed successfully, but after programming or starting a debug session, the device eventually jumps to a fault address.&lt;/LI&gt;&lt;LI&gt;The debugger then halts at that location.&lt;/LI&gt;&lt;LI&gt;During some programming or dumping attempts, I receive a Wire ACK fault.&lt;/LI&gt;&lt;LI&gt;At other times, MCUXpresso reports:&lt;BR /&gt;Error while executing the MI command&lt;/LI&gt;&lt;LI&gt;I also tried to erase the flash from MCUXpresso, but the flash erase operation itself does not complete successfully.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Checks already performed&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;JTAG/SWD connections have been checked and appear to be correct.&lt;/LI&gt;&lt;LI&gt;The issue was tested with both a SEGGER J-Link and an NXP MCU-Link debug probe.&lt;BR /&gt;Boot configuration has been compared with the KW45 EVK.&lt;/LI&gt;&lt;LI&gt;I am using a known-working application for testing.&lt;BR /&gt;The issue is intermittent: programming sometimes succeeds, but at other times a Wire ACK fault or MI command error occurs.&lt;/LI&gt;&lt;LI&gt;Flash erase has also been attempted, but it does not complete successfully.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;My questions&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;What could cause the KW45 to: Intermittently report a Wire ACK fault while dumping or programming code?&lt;/LI&gt;&lt;LI&gt;Report Error while executing the MI command?&lt;/LI&gt;&lt;LI&gt;Jump or halt at an unexpected or invalid memory address after programming?&lt;/LI&gt;&lt;LI&gt;Fail even when attempting a full flash erase?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Since the issue includes intermittent Wire ACK faults and failure during flash erase, I suspect this may be related to the debug interface, SWD/JTAG signal integrity, power-supply stability, reset sequence, flash controller state, device security/configuration, boot configuration, or another hardware-level issue rather than the application itself.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Could you please suggest the recommended procedure to:&lt;/LI&gt;&lt;LI&gt;Recover or erase the KW45 device.&lt;/LI&gt;&lt;LI&gt;Verify that the debug interface is functioning correctly.&lt;/LI&gt;&lt;LI&gt;Check whether the device is secured or in a state that prevents normal programming.&lt;/LI&gt;&lt;LI&gt;Determine whether the Wire ACK fault is caused by the target hardware, debug probe, power/reset behavior, or SWD/JTAG signal integrity.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I can provide the following information if required:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MCUXpresso IDE version: 25.6.1&lt;/LI&gt;&lt;LI&gt;Debug probes tested: SEGGER J-Link and NXP MCU-Link&lt;/LI&gt;&lt;LI&gt;Complete error log, including the Wire ACK fault details&lt;/LI&gt;&lt;LI&gt;Debug console output&lt;/LI&gt;&lt;LI&gt;Schematic of the JTAG/SWD and boot connections&lt;/LI&gt;&lt;LI&gt;SWD/JTAG clock frequency&lt;/LI&gt;&lt;LI&gt;Power-supply and reset configuration&lt;/LI&gt;&lt;LI&gt;Memory/register information from the failed state&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any guidance on the recommended troubleshooting steps would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Tue, 08 Sep 2026 08:07:59 GMT</pubDate>
    <dc:creator>Prashanth1</dc:creator>
    <dc:date>2026-09-08T08:07:59Z</dc:date>
    <item>
      <title>KW45: Intermittent Wire ACK Fault During Programming/Debugging and Flash Erase Failure</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45-Intermittent-Wire-ACK-Fault-During-Programming-Debugging/m-p/2411879#M20467</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am currently working with a KW45-based custom board and facing an intermittent issue during programming and debugging the firmware.&lt;/P&gt;&lt;P&gt;I have tested the board with both a SEGGER J-Link and an NXP MCU-Link debug probe, and the issue occurs with both probes.&lt;/P&gt;&lt;P&gt;The custom board has the same boot configuration as the KW45 EVK, and the JTAG/SWD connections have also been checked and appear to be correct.&lt;/P&gt;&lt;P&gt;However, I am seeing the following behaviour:&lt;/P&gt;&lt;P&gt;When I try to dump or program a known-working application:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Sometimes the application is programmed successfully, but after programming or starting a debug session, the device eventually jumps to a fault address.&lt;/LI&gt;&lt;LI&gt;The debugger then halts at that location.&lt;/LI&gt;&lt;LI&gt;During some programming or dumping attempts, I receive a Wire ACK fault.&lt;/LI&gt;&lt;LI&gt;At other times, MCUXpresso reports:&lt;BR /&gt;Error while executing the MI command&lt;/LI&gt;&lt;LI&gt;I also tried to erase the flash from MCUXpresso, but the flash erase operation itself does not complete successfully.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Checks already performed&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;JTAG/SWD connections have been checked and appear to be correct.&lt;/LI&gt;&lt;LI&gt;The issue was tested with both a SEGGER J-Link and an NXP MCU-Link debug probe.&lt;BR /&gt;Boot configuration has been compared with the KW45 EVK.&lt;/LI&gt;&lt;LI&gt;I am using a known-working application for testing.&lt;BR /&gt;The issue is intermittent: programming sometimes succeeds, but at other times a Wire ACK fault or MI command error occurs.&lt;/LI&gt;&lt;LI&gt;Flash erase has also been attempted, but it does not complete successfully.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;My questions&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;What could cause the KW45 to: Intermittently report a Wire ACK fault while dumping or programming code?&lt;/LI&gt;&lt;LI&gt;Report Error while executing the MI command?&lt;/LI&gt;&lt;LI&gt;Jump or halt at an unexpected or invalid memory address after programming?&lt;/LI&gt;&lt;LI&gt;Fail even when attempting a full flash erase?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Since the issue includes intermittent Wire ACK faults and failure during flash erase, I suspect this may be related to the debug interface, SWD/JTAG signal integrity, power-supply stability, reset sequence, flash controller state, device security/configuration, boot configuration, or another hardware-level issue rather than the application itself.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Could you please suggest the recommended procedure to:&lt;/LI&gt;&lt;LI&gt;Recover or erase the KW45 device.&lt;/LI&gt;&lt;LI&gt;Verify that the debug interface is functioning correctly.&lt;/LI&gt;&lt;LI&gt;Check whether the device is secured or in a state that prevents normal programming.&lt;/LI&gt;&lt;LI&gt;Determine whether the Wire ACK fault is caused by the target hardware, debug probe, power/reset behavior, or SWD/JTAG signal integrity.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;I can provide the following information if required:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MCUXpresso IDE version: 25.6.1&lt;/LI&gt;&lt;LI&gt;Debug probes tested: SEGGER J-Link and NXP MCU-Link&lt;/LI&gt;&lt;LI&gt;Complete error log, including the Wire ACK fault details&lt;/LI&gt;&lt;LI&gt;Debug console output&lt;/LI&gt;&lt;LI&gt;Schematic of the JTAG/SWD and boot connections&lt;/LI&gt;&lt;LI&gt;SWD/JTAG clock frequency&lt;/LI&gt;&lt;LI&gt;Power-supply and reset configuration&lt;/LI&gt;&lt;LI&gt;Memory/register information from the failed state&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Any guidance on the recommended troubleshooting steps would be greatly appreciated.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2026 08:07:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45-Intermittent-Wire-ACK-Fault-During-Programming-Debugging/m-p/2411879#M20467</guid>
      <dc:creator>Prashanth1</dc:creator>
      <dc:date>2026-09-08T08:07:59Z</dc:date>
    </item>
  </channel>
</rss>