<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Qi proprietary packet RX/TX from/to Renesas Qi in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Qi-proprietary-packet-RX-TX-from-to-Renesas-Qi/m-p/2367691#M20369</link>
    <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;We've built our own Qi charger on top of Renesas P9235 wireless charge transmitter (WCT). This WCT is capable of charging our custom, Renesas P9222 wireless charge receiver (WCR) based device. Beyond the 5W charge support, we're also capable of sending/receiving proprietary packets in both directions (with a strong limitation on packet size).&lt;/P&gt;&lt;P&gt;We've also got NXP WCT (WCT-15W) and WCR (WPR1500) devices to experiment with charging and proprietary packet transmission in any direction. As momentarily we are capable of modifying the FW of WCR only, can't determine whether these two NXP ICs can establish a functional prop. packet transmission between each other.&lt;/P&gt;&lt;P&gt;Our goal is to be able to recv/send prop. packets between:&lt;/P&gt;&lt;P&gt;- NXP WCT and NXP WCR;&lt;/P&gt;&lt;P&gt;- Renesas WCT (P9235) and NXP WCR (WPR9516);&lt;/P&gt;&lt;P&gt;- NXP WCT (WCT-15W) and Reneases WCR (P9222);&lt;/P&gt;&lt;P&gt;All of our attemps have failed until this time and there are indications we'll have to struggle with this a lot.&lt;/P&gt;&lt;P&gt;Want to ask you whether you have any experience, hint, technique, document etc which would promote us being able to implement NXP - Renesas Qi proprietary packet exchange? Is it feasible at all in this configuration? The 5W charge is working and most probably we won't need more than that.&lt;/P&gt;&lt;P&gt;thanks, regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 19 May 2026 13:18:47 GMT</pubDate>
    <dc:creator>treefrog</dc:creator>
    <dc:date>2026-05-19T13:18:47Z</dc:date>
    <item>
      <title>Qi proprietary packet RX/TX from/to Renesas Qi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qi-proprietary-packet-RX-TX-from-to-Renesas-Qi/m-p/2367691#M20369</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;We've built our own Qi charger on top of Renesas P9235 wireless charge transmitter (WCT). This WCT is capable of charging our custom, Renesas P9222 wireless charge receiver (WCR) based device. Beyond the 5W charge support, we're also capable of sending/receiving proprietary packets in both directions (with a strong limitation on packet size).&lt;/P&gt;&lt;P&gt;We've also got NXP WCT (WCT-15W) and WCR (WPR1500) devices to experiment with charging and proprietary packet transmission in any direction. As momentarily we are capable of modifying the FW of WCR only, can't determine whether these two NXP ICs can establish a functional prop. packet transmission between each other.&lt;/P&gt;&lt;P&gt;Our goal is to be able to recv/send prop. packets between:&lt;/P&gt;&lt;P&gt;- NXP WCT and NXP WCR;&lt;/P&gt;&lt;P&gt;- Renesas WCT (P9235) and NXP WCR (WPR9516);&lt;/P&gt;&lt;P&gt;- NXP WCT (WCT-15W) and Reneases WCR (P9222);&lt;/P&gt;&lt;P&gt;All of our attemps have failed until this time and there are indications we'll have to struggle with this a lot.&lt;/P&gt;&lt;P&gt;Want to ask you whether you have any experience, hint, technique, document etc which would promote us being able to implement NXP - Renesas Qi proprietary packet exchange? Is it feasible at all in this configuration? The 5W charge is working and most probably we won't need more than that.&lt;/P&gt;&lt;P&gt;thanks, regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 May 2026 13:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qi-proprietary-packet-RX-TX-from-to-Renesas-Qi/m-p/2367691#M20369</guid>
      <dc:creator>treefrog</dc:creator>
      <dc:date>2026-05-19T13:18:47Z</dc:date>
    </item>
    <item>
      <title>Re: Qi proprietary packet RX/TX from/to Renesas Qi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qi-proprietary-packet-RX-TX-from-to-Renesas-Qi/m-p/2367897#M20370</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;While 5 W Qi charging works correctly, proprietary Qi packet communication is not interoperable between Renesas and NXP devices, as these packets are vendor-specific and not defined by the Qi standard. At this time, there are no documents or references that support implementing proprietary packet exchange between NXP and Renesas devices.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;We recommend using TX and RX devices from the same manufacturer or relying only on Qi-standard communication.&lt;/P&gt;
&lt;P&gt;We apologize for any inconvenience this may cause you.&lt;/P&gt;</description>
      <pubDate>Tue, 19 May 2026 21:02:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qi-proprietary-packet-RX-TX-from-to-Renesas-Qi/m-p/2367897#M20370</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2026-05-19T21:02:45Z</dc:date>
    </item>
    <item>
      <title>Re: Qi proprietary packet RX/TX from/to Renesas Qi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Qi-proprietary-packet-RX-TX-from-to-Renesas-Qi/m-p/2368031#M20371</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;proprietary Qi packet communication is not interoperable between Renesas and NXP devices, as these packets are vendor-specific and not defined by the Qi standard.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;SPAN&gt;Well, I've just checked Wireless Power Consortium's 1.2.3 and 1.3.0 Qi specification, and there are proprietary packets defined, among the other ones. E.g. 0x28 is a 2-byte prop.&amp;nbsp; packet that can be sent by the power receiver to the power transmitter. Anyway, this prop. packet communication is seamlessly working between our Reneses devices.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;So, considering these above, it there really no chance that mixed NXP - Renesas Qi prop. packet communication will work? Maybe by some modification of the Qi sample FW provided to NXP Qi power receiver/transmitter?&lt;/P&gt;</description>
      <pubDate>Wed, 20 May 2026 04:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Qi-proprietary-packet-RX-TX-from-to-Renesas-Qi/m-p/2368031#M20371</guid>
      <dc:creator>treefrog</dc:creator>
      <dc:date>2026-05-20T04:15:55Z</dc:date>
    </item>
  </channel>
</rss>