<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: KW45B41Z83 Fuse Program Failed</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2167255#M20022</link>
    <description>Hi Luis&lt;BR /&gt;The RoTKTH and SB3KDK parameters I am using are set to their default values, which have been flashed onto the blank board. I have reviewed the document you mentioned, but found no information specifying the conditions under which the chip would become unresponsive when writing to the FUSE. As for the post-loading method via SWD, it has not been verified yet.&lt;BR /&gt;Currently, my solution is to program the FUSE via UART. Could you let me know which document contains the detailed programming process?&lt;BR /&gt;Best Regards&lt;BR /&gt;Xcj</description>
    <pubDate>Thu, 11 Sep 2025 00:07:09 GMT</pubDate>
    <dc:creator>Xcj</dc:creator>
    <dc:date>2025-09-11T00:07:09Z</dc:date>
    <item>
      <title>KW45B41Z83 Fuse Program Failed</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2166758#M20016</link>
      <description>&lt;P&gt;Hello, NXP Engineer&lt;BR /&gt;I am currently developing a program for burning FUSE and SB3 files via a serial tool. I encountered an issue: when burning FUSE(0x1F and 0x20) through the UART interface, after performing a voltage boost (SetProperty) and waiting for 1 second, I send the FUSE burning command, but the chip does not respond. At this point, the chip status is already abnormal. If I attempt to burn the FUSEs again, it may succeed or fail (the chip returns 0x01). What could be the possible causes of this problem?&lt;BR /&gt;Below is the waveform data when the failure occurs, as shown in the figure:&lt;/P&gt;&lt;P&gt;ALL:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_8-1757513486755.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356300iE46213AF8EABF5A9/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_8-1757513486755.png" title="Xcj_8-1757513486755.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;1.SetProperty:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_11-1757513620809.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356303i05574C40E3400C40/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_11-1757513620809.png" title="Xcj_11-1757513620809.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_10-1757513593324.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356302i6A037D7E72BC8EDB/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_10-1757513593324.png" title="Xcj_10-1757513593324.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_12-1757513674601.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356305iC99B411A979F602B/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_12-1757513674601.png" title="Xcj_12-1757513674601.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;2.Send 0x5A,0xA6:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_13-1757513761260.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356306i9DA51600AB7A9A14/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_13-1757513761260.png" title="Xcj_13-1757513761260.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_14-1757513770074.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356307iD4114EC4DB5389B1/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_14-1757513770074.png" title="Xcj_14-1757513770074.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;3.Write FUSE:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_15-1757513823167.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356309iE637B0583E7B3BF1/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_15-1757513823167.png" title="Xcj_15-1757513823167.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_16-1757513843735.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356310i26175E17D3A5A08E/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_16-1757513843735.png" title="Xcj_16-1757513843735.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_17-1757513873825.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356311i97E85D9C38A6CAA4/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_17-1757513873825.png" title="Xcj_17-1757513873825.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_18-1757513894077.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356312iDFA513027B89F5D8/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_18-1757513894077.png" title="Xcj_18-1757513894077.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_19-1757513940446.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356313i830225DA51BD08C2/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_19-1757513940446.png" title="Xcj_19-1757513940446.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_20-1757513958938.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356314iDE47601A9930D400/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_20-1757513958938.png" title="Xcj_20-1757513958938.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_21-1757514020375.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356315iFC458CFA056D349D/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_21-1757514020375.png" title="Xcj_21-1757514020375.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_22-1757514038652.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356316iE9F3001E481D014F/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_22-1757514038652.png" title="Xcj_22-1757514038652.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_23-1757514080868.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356317i7FCD1C23D6805BDC/image-size/medium?v=v2&amp;amp;px=400" alt="Xcj_23-1757514080868.png" title="Xcj_23-1757514080868.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 10 Sep 2025 14:22:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2166758#M20016</guid>
      <dc:creator>Xcj</dc:creator>
      <dc:date>2025-09-10T14:22:21Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z83 Fuse Program Failed</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2167115#M20021</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;Fuses 0x1F [CUST_PROD_OEMFW_AUTH_PUK] and 0x20 [CUST_PROD_OEMFW_ENC_SK] are encryption keys, also known as RoTKTH and SB3KDK.&lt;/P&gt;
&lt;P&gt;You can find this information in Chapter 15.2.1 and Table 55 in &lt;A href="https://www.nxp.com/webapp/Download?colCode=KW45RM" target="_blank"&gt;KW45 Refence Manual&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;The RoTKTH and SB3KDK fuses play a critical role in securing KW45 devices during the boot process.&lt;/P&gt;
&lt;P&gt;Both fuses are one-time programmable and must be carefully configured during production, as incorrect values can permanently affect device behavior or prevent secure boot.&lt;/P&gt;
&lt;P&gt;For the KW45B41Z-EVK board, NXP provides the default keys, However, for the KW45 chip received from the factory, by default, the SBKDK and RoTKTH keys in the fuse are null.&lt;/P&gt;
&lt;P&gt;In the &lt;A href="https://docs.nxp.com/bundle/AN14158/page/topics/introduction.html" target="_blank"&gt;AN14158: Debug Authentication on KW45/K32W148 | NXP Semiconductors&lt;/A&gt; Chapter 7.2.1 you can see the command to program these fuses for enter OEM secure world closed state.&lt;/P&gt;
&lt;P&gt;If you are trying to fuse KW45 chips from factory; I would strongly recommend following the instructions in &lt;A href="https://docs.nxp.com/bundle/AN14003/page/topics/introduction.html" target="_blank"&gt;AN14003: Programming the KW45 flash for Application and Radio firmware via Serial Wire Debug during mass production | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;A very important question is; The KW45 chips are destined to operate same as the KW45B41Z-EVK? If that’s the case, you can use the default Keys for RoTKTH and SB3KDK described in chapter 5.2.1 [AN14003].&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Wed, 10 Sep 2025 21:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2167115#M20021</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-09-10T21:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z83 Fuse Program Failed</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2167255#M20022</link>
      <description>Hi Luis&lt;BR /&gt;The RoTKTH and SB3KDK parameters I am using are set to their default values, which have been flashed onto the blank board. I have reviewed the document you mentioned, but found no information specifying the conditions under which the chip would become unresponsive when writing to the FUSE. As for the post-loading method via SWD, it has not been verified yet.&lt;BR /&gt;Currently, my solution is to program the FUSE via UART. Could you let me know which document contains the detailed programming process?&lt;BR /&gt;Best Regards&lt;BR /&gt;Xcj</description>
      <pubDate>Thu, 11 Sep 2025 00:07:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2167255#M20022</guid>
      <dc:creator>Xcj</dc:creator>
      <dc:date>2025-09-11T00:07:09Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z83 Fuse Program Failed</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2168576#M20026</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Luis&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Could you first check if there is an issue with the method I am using to enter ISP mode?&lt;BR /&gt;My current procedure for entering ISP mode is as follows:&lt;BR /&gt;1.Supply 3.3V to VCC.&lt;BR /&gt;2.After maintaining power for 200ms, pull the Reset and PTA4 pins of the chip high.&lt;BR /&gt;3.After maintaining this for 5ms, pull the Reset pin low and maintain for 1000ms.&lt;BR /&gt;4.Pull the Reset pin high and maintain for 2000ms.&lt;BR /&gt;5.Use the tool to send 0x5A, 0xA6 three times consecutively. The chip returns correct responses for the latter two attempts.&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230059"&gt;@luis_maravilla&lt;/a&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Xcj_0-1757653438861.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/356636i5B377772B879AB74/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Xcj_0-1757653438861.png" alt="Xcj_0-1757653438861.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Xcj_0-1757653438861.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Xcj&lt;/P&gt;</description>
      <pubDate>Fri, 12 Sep 2025 05:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2168576#M20026</guid>
      <dc:creator>Xcj</dc:creator>
      <dc:date>2025-09-12T05:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z83 Fuse Program Failed</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2173706#M20039</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;In the MCUXpresso SDK documentation indicates that the process for entering ISP mode in KW45 custom board is Short the BOOT_CFG pin[PTA4] to VDD while reset.&lt;/P&gt;
&lt;P&gt;For more information about this please refer to: &lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/boards/Wireless/kw45b41zevk/gettingStarted/topics/how_to_set_the_board_to_bootloader.html" target="_blank"&gt;How to set the board to the Bootloader ISP mode — MCUXpresso SDK Documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Sending the 0x5A, 0xA6 [Also known as ping packet] is a way to confirm the UART transmission; After the bootloader detects the ping packet (0x5A 0xA6) on UARTn_RX, the bootloader firmware executes the autobaud sequence.&lt;/P&gt;
&lt;P&gt;For more information about this please refer to: &lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/middleware/mcu_bootloader/docs/MCU_Bootloader_Reference_Manual/topics/uart_peripheral.html" target="_blank"&gt;UART peripheral — MCUXpresso SDK Documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Mon, 22 Sep 2025 18:26:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z83-Fuse-Program-Failed/m-p/2173706#M20039</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-09-22T18:26:53Z</dc:date>
    </item>
  </channel>
</rss>