<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 write event in eatt example</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/write-event-in-eatt-example/m-p/2166026#M20008</link>
    <description>&lt;P&gt;Hi Nxp team,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want write specific value in ble handle and uuid have write caharacterstic on eatt peripheral example using eatt central using method GattClient_SimpleCharacteristicWrite but event in not trigeer in eatt peripheral what to do to trigger the write event in eatt peripheral.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;using kw45&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SDK : 25.12&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;using SDK eatt peripheral example.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 09 Sep 2025 15:51:15 GMT</pubDate>
    <dc:creator>Chan_17</dc:creator>
    <dc:date>2025-09-09T15:51:15Z</dc:date>
    <item>
      <title>write event in eatt example</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/write-event-in-eatt-example/m-p/2166026#M20008</link>
      <description>&lt;P&gt;Hi Nxp team,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I want write specific value in ble handle and uuid have write caharacterstic on eatt peripheral example using eatt central using method GattClient_SimpleCharacteristicWrite but event in not trigeer in eatt peripheral what to do to trigger the write event in eatt peripheral.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;using kw45&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;SDK : 25.12&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;using SDK eatt peripheral example.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 09 Sep 2025 15:51:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/write-event-in-eatt-example/m-p/2166026#M20008</guid>
      <dc:creator>Chan_17</dc:creator>
      <dc:date>2025-09-09T15:51:15Z</dc:date>
    </item>
    <item>
      <title>Re: write event in eatt example</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/write-event-in-eatt-example/m-p/2166081#M20009</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;GattClient_SimpleCharacteristicWrite&lt;/EM&gt; &amp;nbsp;sends an ATT Write Request if the value length does not exceed the maximum space for an over-the-air packet (ATT_MTU – 3).&lt;/P&gt;
&lt;P&gt;There is a short example to write a 3-byte long Characteristic Value and how the client procedure callback is triggered described in Chapter 5.1.4.4 &lt;STRONG&gt;&lt;EM&gt;Characteristic write procedure&lt;/EM&gt;&lt;/STRONG&gt; in &lt;STRONG&gt;&lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/_static/wireless/Bluetooth/Bluetooth_Low_Energy_Application_Developer's_Guide.pdf" target="_blank"&gt;Bluetooth Low Energy Application Developer’s Guide&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;The latest SDK version for KW45 is 25.06, could you help us confirm if you mean another SDK version? As 24.12?&lt;/P&gt;
&lt;P&gt;Also, could you help us confirm if the KW45 you are using is the KW45B41Z-EVK or a KW45 custom board?&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Tue, 09 Sep 2025 17:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/write-event-in-eatt-example/m-p/2166081#M20009</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-09-09T17:32:17Z</dc:date>
    </item>
  </channel>
</rss>