<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Extend ZCL command timeouts in HA SDK App in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Extend-ZCL-command-timeouts-in-HA-SDK-App/m-p/623309#M1990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have noticed that when using the the HA SDK (JN-SW-4168) on a custom board and using the JN-AN-1223 ZigBee GUI that after a while, that an "APS Fail" starts to come in. Sniffing the channel I can see that the payload does come back eventually, but sometimes its up to 3s afterwards. I am unsure if it is because the Stack starts to hound the router (I can see it sends 8 messages within 1.2s of my sniffers time).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can confirm this plug works very successfully with other ZigBee Coordinators purchased.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Profile: HA 1.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nonetheless, with other stacks in the past I have been able to set custom timeouts on this commands to not issue&amp;nbsp;an error for some time,&amp;nbsp;typically 3-10s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also notice that reading the Neighbour table every 15 minutes that the only device in my network sometimes disappears and has to do a route dicsovery to find it again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following response is what I received from the ZigBee GUI app mentioned above. The support sniffer image is attached with the highlighted payload and all responses following. Note: Only one request was sent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Type: 0x8000 (Status)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Length: 4&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Status: 0x00 (Success)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SQN: 0x06&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Message:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Type: 0x8702 (APS Data Confirm Fail)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SQN: 0xE9&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Status: 0x01&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Source Endpoint: 0x01&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Destination Endpoint: 0x02&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Destination Mode: 0xD3&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Destination Address: 0x01&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Type: 0x8101 (Default Response)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SQN: 0x06&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;EndPoint: 0x01&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Cluster ID: 0x0006 (General: On/Off)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Command: 0x00&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Status: 0x00&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Mar 2017 00:22:04 GMT</pubDate>
    <dc:creator>ryanf</dc:creator>
    <dc:date>2017-03-28T00:22:04Z</dc:date>
    <item>
      <title>Extend ZCL command timeouts in HA SDK App</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Extend-ZCL-command-timeouts-in-HA-SDK-App/m-p/623309#M1990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Guys,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have noticed that when using the the HA SDK (JN-SW-4168) on a custom board and using the JN-AN-1223 ZigBee GUI that after a while, that an "APS Fail" starts to come in. Sniffing the channel I can see that the payload does come back eventually, but sometimes its up to 3s afterwards. I am unsure if it is because the Stack starts to hound the router (I can see it sends 8 messages within 1.2s of my sniffers time).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can confirm this plug works very successfully with other ZigBee Coordinators purchased.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Profile: HA 1.2&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nonetheless, with other stacks in the past I have been able to set custom timeouts on this commands to not issue&amp;nbsp;an error for some time,&amp;nbsp;typically 3-10s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also notice that reading the Neighbour table every 15 minutes that the only device in my network sometimes disappears and has to do a route dicsovery to find it again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following response is what I received from the ZigBee GUI app mentioned above. The support sniffer image is attached with the highlighted payload and all responses following. Note: Only one request was sent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Type: 0x8000 (Status)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Length: 4&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Status: 0x00 (Success)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SQN: 0x06&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Message:&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Type: 0x8702 (APS Data Confirm Fail)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SQN: 0xE9&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Status: 0x01&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Source Endpoint: 0x01&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Destination Endpoint: 0x02&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Destination Mode: 0xD3&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Destination Address: 0x01&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Type: 0x8101 (Default Response)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SQN: 0x06&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;EndPoint: 0x01&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Cluster ID: 0x0006 (General: On/Off)&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Command: 0x00&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Status: 0x00&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Mar 2017 00:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Extend-ZCL-command-timeouts-in-HA-SDK-App/m-p/623309#M1990</guid>
      <dc:creator>ryanf</dc:creator>
      <dc:date>2017-03-28T00:22:04Z</dc:date>
    </item>
    <item>
      <title>Re: Extend ZCL command timeouts in HA SDK App</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Extend-ZCL-command-timeouts-in-HA-SDK-App/m-p/623310#M1991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ryan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please confirm what is the AN that you are referring?&lt;/P&gt;&lt;P&gt;Also you are join routers and end devices, what is the example for this devices?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You don't have this issue with other devices, in other words, did you use a USB dongle, a JN module and create the network successfully?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Mario&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2017 22:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Extend-ZCL-command-timeouts-in-HA-SDK-App/m-p/623310#M1991</guid>
      <dc:creator>mario_castaneda</dc:creator>
      <dc:date>2017-06-01T22:31:41Z</dc:date>
    </item>
  </channel>
</rss>